STM32 MPU OpenSTLinux release note - v4.1.0

Revision as of 19:16, 13 November 2023 by Registered User (→‎v4.1.1)
Applicable for STM32MP13x lines, STM32MP15x lines

This article describes the content of OpenSTLinux distribution software release version openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23, which is part of the STM32 MPU ecosystem release note - v4.1.0.

1. Intended audience[edit source]

The targeted audience is STM32MP13x lines More info.png and STM32MP15x lines More info.png customers or partners.

2. Delivery scope and purpose[edit source]

The OpenSTLinux distribution is a Linux® distribution based on the OpenEmbedded build Framework. It runs on the Arm® Cortex®-A7 processors, and is a fundamental part of the STM32MPU Embedded Software distribution. This delivery of OpenSTLinux distribution is part of STM32 MPU Ecosystem v4.1.0 (see the STM32 MPU ecosystem release note - v4.1.0).

3. Licensing[edit source]

This software package is licensed under a LIMITED LICENSE AGREEMENT FOR ST MATERIALS EVALUATION (LLA). Customers may not use this package except in compliance with the software license agreement (SLA).

All packages use the same source components. All components and their respective licenses are listed here.

4. Supported hardware[edit source]

This software delivery is compatible with the following boards:

STM32MP13 boards
Boards PCBs list Main features Ordering
STM32MP135x-DK.png
STM32MP135F-DK Discovery kit
  • MB1635 (motherboard)
  • MB1897 (camera module board)
  • STM32MP135FAF7[1] Rev.Y
    • Arm®-based Cortex®-A7 1 GHz
    • Secure boot and cryptography
    • 4-Gbit DDR3L, 16 bits, 533 MHz
  • ST PMIC STPMIC1
  • 4.3" TFT 480x272 pixels with LED backlight, and capacitive touch panel
  • 2-megapixel dual lane CSI-2 camera module with 15-pin FFC connector
  • Wi-Fi® 802.11b/g/n
  • Bluetooth® Low Energy 4.1

Discovery kit with STM32MP135F MPU

STM32MP15 boards
Boards PCBs list Main features Ordering
STM32MP157D-DK1.jpg
STM32MP157D-DK1 Discovery kit
  • MB1272C (motherboard)
  • STM32MP157DAC1[2] Rev.Z
    • Arm®-based dual Cortex®-A7 800 MHz
    • Basic security
    • 4-Gbit DDR3L, 16 bits, 533 MHz
  • ST PMIC STPMIC1APQR cut2.0

Discovery kit with STM32MP157D MPU

STM32MP157F-DK2.jpg
STM32MP157F-DK2 Discovery kit
  • MB1272C (motherboard)
  • MB1407B (daughterboard DSI display)
  • STM32MP157FAC1[2] Rev.Z
    • Arm®-based dual Cortex®-A7 800 MHz
    • Secure boot and cryptography
    • 4-Gbit DDR3L, 16 bits, 533 MHz
  • ST PMIC STPMIC1APQR cut2.0
  • 4" TFT 480×800 pixels with LED backlight, and capacitive touch panel
  • Wi-Fi® 802.11b/g/n
  • Bluetooth® Low Energy 4.1

Discovery kit with STM32MP157F MPU

STM32MP157D or F-EV1.jpg
STM32MP157D-EV1 Evaluation board
  • MB1262C (motherboard)
  • MB1263C (daughterboard)
  • MB1230C (daughterboard DSI display)
  • MB1379A (camera)
  • STM32MP157DAA1[2] Rev.Z
    • Arm®-based dual Cortex®-A7 800 MHz
    • Basic security
    • 2 × 4-Gbit DDR3L, 16 bits, 533 MHz
  • PMIC STPMIC1APQR cut2.0
  • 5.5" TFT 720×1280 pixels with LED backlight, and capacitive touch panel
  • 5-megapixel, 8-bit camera

Evaluation board with STM32MP157D MPU

STM32MP157D or F-EV1.jpg
STM32MP157F-EV1 Evaluation board
  • MB1262C (motherboard)
  • MB1263C (daughterboard)
  • MB1230C (daughterboard DSI display)
  • MB1379A (camera)
  • STM32MP157FAA1[2] Rev.Z
    • Arm®-based dual Cortex®-A7 800 MHz
    • Secure boot and cryptography
    • 2 × 4-Gbit DDR3L, 16 bits, 533 MHz
  • PMIC STPMIC1APQR cut2.0
  • 5.5" TFT 720×1280 pixels with LED backlight, and capacitive touch panel
  • 5-megapixel, 8-bit camera

Evaluation board with STM32MP157F MPU

STM32MP157A-DK1.jpg
STM32MP157A-DK1 Discovery kit
  • MB1272C (motherboard)
  • STM32MP157AAC3[2] Rev.B
    • Arm®-based dual Cortex®-A7 650 MHz
    • Basic security
    • 4-Gbit DDR3L, 16 bits, 533 MHz
  • ST PMIC STPMIC1APQR cut1.2

Out of production

STM32MP157C-DK2.jpg
STM32MP157C-DK2 Discovery kit
  • MB1272C (motherboard)
  • MB1407B (daughterboard DSI display)
  • STM32MP157CAC3[2] Rev.B
    • Arm®-based dual Cortex®-A7 650 MHz
    • Secure boot and cryptography
    • 4-Gbit DDR3L, 16 bits, 533 MHz
  • ST PMIC STPMIC1APQR cut1.2
  • 4" TFT 480×800 pixels with LED backlight, and capacitive touch panel
  • Wi-Fi® 802.11b/g/n
  • Bluetooth® Low Energy 4.1

Out of production

STM32MP157A or C-EV1.jpg
STM32MP157A-EV1 Evaluation board
  • MB1262C (motherboard)
  • MB1263C (daughterboard)
  • MB1230C (daughterboard DSI display)
  • MB1379A (camera)
  • STM32MP157AAA3[2] Rev.B
    • Arm®-based dual Cortex®-A7 650 MHz
    • Basic security
    • 2 × 4-Gbit DDR3L, 16 bits, 533 MHz
  • PMIC STPMIC1APQR cut1.2
  • 5.5" TFT 720×1280 pixels with LED backlight, and capacitive touch panel
  • 5-megapixel, 8-bit camera

Out of production

STM32MP157A or C-EV1.jpg
STM32MP157C-EV1 Evaluation board
  • MB1262C (motherboard)
  • MB1263C (daughterboard)
  • MB1230C (daughterboard DSI display)
  • MB1379A (camera)
  • STM32MP157CAA3[2] Rev.B
    • Arm®-based dual Cortex®-A7 650 MHz
    • Secure boot and cryptography
    • 2 × 4-Gbit DDR3L, 16 bits, 533 MHz
  • PMIC STPMIC1APQR cut1.2
  • 5.5" TFT 720×1280 pixels with LED backlight, and capacitive touch panel
  • 5-megapixel, 8-bit camera

Out of production


5. Release content[edit source]

5.1. Main software components[edit source]

  • Build process
    • OpenEmbedded v4.0.4 (Kirkstone) - Updated
    • GCC version v11.3.0 - Updated
  • Embedded software components
    • Linux kernel v5.15-stm32mp-r2 (v5.15.67) - Updated
    • TF-A v2.6-stm32mp-r2 - Updated
    • U-Boot v2021.10-stm32mp-r2 - Updated
    • OP-TEE 3.16.0-stm32mp-r2 - Updated
    • OpenOCD version v0.11.0
  • Applicative components
    • Weston version v10.0.2 - Updated
    • Wayland version 1.20.0
    • GStreamer version v1.20.3 - Updated
    • GCnano version v6.4.9 - Updated

5.2. Changes[edit source]

5.2.1. OpenSTLinux layers[edit source]

Changes are:‎

  • Rebase on Yocto LTS Release 4.0.4 (Kirkstone)
  • Add support of Firmware Update feature for NAND memory
  • Add Arm® Cortex®-A7 and Arm® Cortex®-M4 examples in Starter Package for STM32MP157D-DK1 More info green.png
  • Move Arm® Cortex®-A7 and Arm® Cortex®-M4 examples from STM32MP157C-DK2 Warning.png to STM32MP157F-DK2 More info green.png
  • Increase default rootfs ext4 partition size: 3GB for eMMC and 4GB for Micro SD Card
  • Minor fixes
Info white.png Information
From prevous major release OpenSTLinux v4.0.0, FIP configuration is the only packaging format supported for boot loaders (more about FIP here) :
  • Only TF-A BL2 requires the stm32 header for a ROM code authentication. Others bootloader binaries are embedded in a FIP container.
  • A dedicated fip-utils-stm32mp.bbclass class is provided on meta-st-stm32mp layer side to manage the FIP image configuration, build and update.

5.2.2. Linux® kernel[edit source]

New component release tag 5.15-stm32mp-r2 is available, rebased on official Linux® kernel v5.15.67.

Changes are:‎

  • Real Time ready drivers (RT-Linux)
  • SPI slave support
  • ADC oversampling support
  • SPI master driver with dual-qspi mode support
  • DMA support for CRYP IP (Crypto performance improvement)
  • STM32MP13x lines More info.png:
    • New wake up sources
      • USB OTG wake up via STM32G0
      • Ethernet PHY Wakeup on LAN
  • Minor fixes

5.2.3. U-Boot[edit source]

New component release tag 2021.10-stm32mp-r2 is available, rebased on official U-Boot v2021.10.

Changes are:

  • Fix support of STM32MP13x Rev.Y
  • Device tree alignment with Linux Kernel v5.15-stm32mp-r2
  • Remove tests on CONFIG_DM_REGULATOR
  • Fix invalid clock name references in SCMI driver
  • Make usage of clock/reset bulk() API in USB EHCI driver
  • Fix the display of protected GPIO in gpio and pinmux command
  • Display label for gpio in alternate mode in gpio status command
  • Fixes for stm32prog command:
  • Correctly handle OTP when SMC is not supported
  • Support empty flashlayout
  • Several fixes for STM32MP13 clock
  • Use correct compatible string to add MTD partitions int ft_board_setup()
  • Check fdtcontroladdr in label_boot for pxe command parsing, used on extlinux.conf for GENERIC DISTRO support
  • Use RGB565 for BMP blitting, as panel configuration
  • Several STM32 I2C corrections
  • Other minor updates
Info white.png Information
The U-Boot defconfig to use for ecosystem release ≥ v4.0.0 More info.png changed to stm32mp15_defconfig.
Warning white.png Warning
SPL and STM32Image is not supported anymore in OpenSTLinux U-Boot. Migrate to TF-A with FIP support instead.

5.2.4. TF-A[edit source]

New component release tag 2.6-stm32mp-r2 is available, rebased on official TF-A v2.6.

Changes are:

  • Firmware update on NAND devices
  • Improve FIP management on NAND devices
  • Add GPIO regulators driver
  • Use FCONF to manage the Chain of Trust
  • Allow support of non-paged OP-TEE
  • Skip boot devices initialization when returning from Standby (only with OP-TEE)
  • Minor fixes

5.2.5. OP-TEE[edit source]

New component release tag 3.16.0-stm32mp-r2 is available, rebased on official OP_TEE OS 3.16.0.

Changes are:

  • ADC driver implementation
  • IRQ forwarding
  • Update regulator IO management
  • Hardware unique key (HUK) implementation:
  • using secured OTP through BSEC driver mapping on STM32MP15
  • through SAES on STM32MP13
  • Minor Fixes

6. Release change notification[edit source]

OpenSTLinux attention points to switch from ecosystem release v4.0.0 More info.png to ecosystem release v4.1.0 More info.png are documented in STM32 MPU OpenSTLinux release changes notification – v4.1.0 article.

7. Recommendations for use[edit source]

7.1. Safe use[edit source]

  • Flash programming and boot from all supported flash devices: SDCard, eMMC, ONFI NAND and NOR flash memories.
  • Develop Linux® applications, libraries, kernel modules based on OpenSTLinux delivery.
  • Develop coprocessor Cube applications based on STM32CubeMP1 delivery.
  • Develop boards based on STM32MP1 Series.
  • Prototype applications based on ST boards.

7.2. Non-recommended use[edit source]

  • None

8. Restrictions[edit source]

  • If Firmware Update is not enabled, and the flashlayout partition is not needed anymore, but the storage mapping is hardcoded in U-Boot; either the flashlayout keeps the partitions for Firmware Update feature or U-Boot needs to be updated.
Warning white.png Warning
On an Ubuntu 18.04 (with a host gcc version prior to 8.0), U-Boot cannot be built by using the STM32MP1_Developer_Package because the option : -fmacro-prefix-map , used in U-Boot is not supported by Ubuntu 18.04

9. Minor release updates[edit source]

STMicroelectronics regularly delivers corrections through github® components which are U-Boot, OP-TEE, TF-A, Linux kernel.
The corrections can be incorporated into the Developer Package (refer to STM32MP1 Developer Package) or Distribution Package (see below).

Two possibilities exist to update a Distribution Package:

  • Update your existing Distribution Package:
Switch your Distribution Package to # github® mode .
  1. Use the devtool modify <recipe name> command to set up an environment. It fetches and unpacks the source code.
  2. In the extracted source code, use a git command such as git checkout -b WORK <github® TAG> to point to a new revision of the component.
More rarely STMicroelectronics also delivers fixes on layers through github®. These changes can be integrated (via git commands: git checkout -b WORK <github® commit SHA1>) into the local STM32MP1 Distribution Package environment. See below the github® links of the quoted layers :
  • Get a new Distribution Package:
Refer to Installing_the_OpenSTLinux_distribution page for install instructions, and use the repo command given for the minor version below, if it exists.

9.1. v4.1.1[edit source]

  • Update to Yocto Project 4.0.11 (2022-04.11-kirkstone)
  • Update to Linux Kernel 5.15.118
  • BSP maturation with an amount of 49 fixes delivered BSP components (TF-A, u-Boot, OP-TEE and Linux Kernel)
  • BSP update:
Layer name github® commit SHA1 reference
meta-st-stm32mp ef4a6a785d17b4370cd20402b351a17ed34cd74d
meta-st-openstlinux 03daeb62ccffa2e29c20ee97154dc18dda4fbd60
  • Component update:
Component Recipe name new github® release
tf-a tf-a-stm32mp v2.6-stm32mp-r2.1
u-boot u-boot-stm32mp v2021.10-stm32mp-r2.1
kernel linux-stm32mp v5.15-stm32mp-r2.1
optee-os optee-os-stm32mp 3.16.0-stm32mp-r2.1"
  • New manifest tag available to get the release: openstlinux-5.15-yocto-kirkstone-mp1-v23.07.26
repo init -u https://github.com/STMicroelectronics/oe-manifest -b refs/tags/openstlinux-5.15-yocto-kirkstone-mp1-v23.07.26
repo sync

10. How to get started with openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23[edit source]

Refer to How to download the software and start with this release?

11. Associated tools[edit source]

Refer to the Referenced tools release notes .

12. Yocto features enabled in the delivery[edit source]

OpenEmbedded[3] build framework engine is named OE-Core.
OpenSTLinux distribution is based on the build framework OpenEmbedded, and can be configured thanks to a mechanism named "features" (machine features, distribution features, ...).

Depending on the features enabled, the resulting distribution can have more capabilities or software embedded.
For example, if the wifi is enabled then the wifi software and drivers are present on the filesystem and the wifi can be used.

12.1. Machine features[edit source]

The variable MACHINE_FEATURES specifies the list of hardware features the machine is capable of supporting.
These features (MACHINE_FEATURES) are defined inside the machine configuration .

Machine feature Purpose
alsa Include ALSA support (OSS compatibility kernel modules installed if available).
autoresize Add support of autoresize through InitRD
bluetooth Add Broadcom43430 (Bluetooth) firmware to the filesystem
(STM32MP135x-DK Discovery kit More info green.png and STM32MP157x-DKx Discovery kit More info green.png)
ext2 Add Second Extended File System support
fip Enable Firmware In Package (FIP) packaging format
fw-update Enable Firmware update feature
gpu Add GPU support (if EULA is accepted) (STM32MP157 line More info.png only)
initrd Enable Intial ramdisk building
m4copro Add m4projects to userfs (STM32MP15x lines More info.png only)
optee Add OP-TEE Secure part
pci Add Peripheral Component Interconnect peripheral support
rtc Add Real Time Clock peripheral support
screen Add display screen peripheral support
splashscreen Add splashscreen to U-Boot
tpm2 Add Trusted Platform Module peripheral support
usbg0 Add G0 Firmware for USB support
usbgadget Enable USB Gadget feature
usbhost Enable USB Host feature
watchdog Add watchdog support and binaries
wifi Add Broadcom43430 (wifi) firmware to the filesystem
(STM32MP135x-DK Discovery kit More info green.png and STM32MP157x-DKx Discovery kit More info green.png)

12.2. Distribution features[edit source]

The variable DISTRO_FEATURES specifies the list of software features present in the distribution.
These features (DISTRO_FEATURES) are defined inside the distribution configuration .

Distribution feature Purpose
alsa Include ALSA support (OSS compatibility kernel modules installed if available).
argp
autoresize Add support of userfs auto resize feature in OpenSTLinux
bluetooth Include Bluetooth support
bluez5 Add Bluetooth stack
efi Add userland EFI tools
ext2 Add Second Extended File System support
ext4 Add Fourth Extended File System support
gobject-introspection-data Enable GObject Introspection, project for providing machine readable introspection data of the API of C libraries.
gplv3 Add gplv3 binaries in OpenSTLinux
gstreamer Add gstreamer tools in filesystem
initrd Add ramdisk
ipv4 Add ipv4 support
ipv6 Add ipv6 support
kde Add several tools (e.g. cups, fontconfig, ...) to the filesystem
largefile Enable large file support
ldconfig Include support for ldconfig and ld.so.conf on the target
multiarch Enable 64 bits BFD (Binary File Descriptor)
nfs Include NFS client support (for mounting NFS exports on device).
opengl Include the Open Graphics Library
optee Install tee service on the filesystem
pam Enable Pluggable Authentication Module
pci Add pci support
polkit Enable PolicyKit for controlling system-wide privileges
pulseaudio Network-capable sound server program
splashscreen Add U-Boot splashscreen
systemd Use systemd as init service
usbgadget USB Gadget Device support (for USB networking/serial/storage)
usbhost USB Host support (allows to connect external keyboard, mouse, storage, network etc)
wayland Add Wayland support
wifi WiFi support
xattr Add "Extended Attributes" support for filesystem
zeroconf Add zeroconf package to set up a ad-hoc network

12.3. Bootscheme labels[edit source]

The variable BOOTSCHEME_LABELS defines which kind of boot is supported on the board.
These settings (BOOTSCHEME_LABELS) are defined inside the machine configuration .

Bootscheme label Purpose
optee Add optee in bootscheme
trusted Add trusted in bootscheme

12.4. Bootdevice labels[edit source]

The variable BOOTDEVICE_LABELS defines which kind of mass storage OpenSTLinux can programmed.
These settings (BOOTDEVICE_LABELS ) are defined inside the machine configuration .

Bootdevice label Purpose
emmc Add boot on emmc device
nand-4-256 Add boot on NAND device
nor-sdcard Add boot stage on NOR device and the filesystem on SD-Card
sdcard Add boot on SD-Card