X-LINUX-RT OpenSTLinux Expansion Package

Revision as of 11:34, 16 February 2023 by Registered User (→‎Install X-LINUX-RT environment)


Applicable for STM32MP13x lines, STM32MP15x lines

X-LINUX-RT is an STM32 MPU OpenSTLinux Expansion Package that targets real-time (RT) feature in the Linux kernel.
A RT system is a system which responds to a request in a time laps and not as fast as possible​:

  • determinism​
  • LATENCY but not SPEED

To have a better understanding about RT Linux, you can refer to the Linux RT foundation website[1].

RT Expansion Package In STM32MPU Embedded Software.png

1. X-LINUX-RT[edit source]

Info white.png Information
This version is compatible with Yocto Project® build system Kirkstone and has been validated against the OpenSTLinux ecosystem release v4.1.0 More info.png and validated on:
  • STM32MP157D-DK1 More info green.png
  • STM32MP157C-DK2 Warning.png and STM32MP157F-DK2 More info green.png
  • STM32MP157C-EV1 Warning.png , STM32MP157D-EV1 More info green.png and STM32MP157F-EV1 More info green.png
  • STM32MP135F-DK More info green.png

1.1. Main software modification[edit source]

Moving on a Linux-RT impacts kernel configuration:​

  • Power management is not "compliant" with a real time context as it changes system behavior. There is no more frequency scaling ; it's a fixed frequency.
    • 900MHZ for STM32MP13x lines More info.png
    • 650MHz for STM32MP15x lines More info.png
  • High Resolution timers and periodic ticks should be used in order to have a precise tick.

2. Distribution package: re-generate X-LINUX-RT OpenSTLinux distribution[edit source]

With the following procedure, the complete distribution can be re-generated by enabling the X-LINUX-RT expansion package.

2.1. Download the STM32MP1 Distribution Package[edit source]

For ecosystem release v4.1.0 More info.png :
Install the STM32MP1 Distribution Package v4.1.0.

2.2. Install X-LINUX-RT environment[edit source]

  • Clone the meta-st-x-linux-rt git repositories
 cd <Distribution Package installation directory>/layers/meta-st
 git clone https://github.com/STMicroelectronics/meta-st-x-linux-rt.git
 cd ../..
  • Source the build environment with the correct board and layer.

For STM32MP13x lines More info.png:

 DISTRO=openstlinux-weston MACHINE=stm32mp13-rt source layers/meta-st/scripts/envsetup.sh

For STM32MP15x lines More info.png:

 DISTRO=openstlinux-weston MACHINE=stm32mp15-rt source layers/meta-st/scripts/envsetup.sh

2.3. Build the image[edit source]

 bitbake st-image-weston
Info white.png Information
Note that building the image could take long time depending on the host computer performance.

2.4. Program the built image into the Flash memory[edit source]

Follow this link to see how to program the built image.


3. Developer package: build RT BSP with the SDK[edit source]

Linux RT can be built with sources provided in the OpenSTLinux BSP packages in addition with patches and device tree files provided in X-LINUX-RT meta layer.

3.1. Install the OpenSTLinux SDK[edit source]

The OpenSTLinux SDK contains all the basis needed for the X-LINUX-RT Expansion package, so it needs to be downloaded and installed: see OpenSTLinux SDK installation guide. Once done, a directory is present on your machine containing the OpenSTLinux SDK.


3.2. Download the Developer package[edit source]

The STM32MP1 Developer Package, containing all the BSP source code, must be downloaded and extracted. To do this, follow only the STM32MP1_Developer_Package#Installing_the_OpenSTLinux_BSP_packages (and not the sub-chapters ).


Two BSP components (OP-TEE OS and Linux kernel) must be modified for RT feature.


3.3. Download X-LINUX-RT meta layer[edit source]

  • Clone the meta-st-x-linux-rt git repository
cd <Developer Package installation directory>/stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23/sources/arm-ostl-linux-gnueabi/
git clone https://github.com/STMicroelectronics/meta-st-x-linux-rt.git

3.4. Modify the BSP[edit source]

As written above, to enable the RT feature, two BSP components must be modified.

3.4.1. Modify the Linux kernel[edit source]

Follow now the sub-chapter STM32MP1_Developer_Package#Building_and_deploying_the_Linux_kernel_for_the_first_time to prepare the Linux kernel.
Patches found in <Developer Package installation directory>/stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23/sources/arm-ostl-linux-gnueabi/meta-st-x-linux-rt/recipes-kernel/linux/5.15/5.15.67 must also be applied.

Enter in the directory containing Linux kernel sources, then apply patches:

for p in `ls -1 <Developer Package installation directory>/stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23/sources/arm-ostl-linux-gnueabi/meta-st-x-linux-rt/recipes-kernel/linux/5.15/5.15.67/*.patch`; do patch -p1 < $p; done

Once patches are applied, new fragments are present inside the Linux kernel source. Apply fragments as it is explain in the README.HOW_TO.txt helper file.


Then add also the following fragments:

For STM32MP13x lines More info.png:

* arch/arm/configs/fragment-07-rt.config
* arch/arm/configs/fragment-07-rt-sysvinit.config
* arch/arm/configs/fragment-08-rt-mp13.config

For STM32MP15x lines More info.png:

* arch/arm/configs/fragment-07-rt.config
* arch/arm/configs/fragment-07-rt-sysvinit.config

The Linux kernel can now be built and deployed.


3.4.2. Modify the OP-TEE OS[edit source]

Follow now the sub-chapter STM32MP1_Developer_Package#Building_and_deploying_the_OP-TEE_for_the_first_time to prepare the OP-TEE OS.
Patches found in <Developer Package installation directory>/stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23/sources/arm-ostl-linux-gnueabi/meta-st-x-linux-rt/recipes-security/optee/optee-os must also be applied.
Enter in the directory containing OP-TEE OS sources, then apply patches

for p in `ls -1 <Developer Package installation directory>/stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23/sources/arm-ostl-linux-gnueabi/meta-st-x-linux-rt/recipes-security/optee/optee-os/*.patch`; do patch -p1 < $p; done

OP-TEE OS can now be built and deployed.


4. To go further[edit source]

To check that RT feature is enabled and functional, following commands can be executed.

4.1. Check Linux kernel version[edit source]

 uname -s -r -v
Without RT feature With RT feature
Linux 5.15.67 #1 SMP PREEMPT Thu Sep 8 10:32:54 UTC 2022
Linux 5.15.67-rt49 #1 SMP PREEMPT_RT Thu Sep 8 10:32:54 UTC 2022

4.2. Cyclictest[edit source]

Cyclictest accurately and repeatedly measures the difference between a thread's intended wake-up time and the time at which it actually wakes up.
For a better understanding on cyclictest, refer to the cyclictest webpage in Linux RT foundation website[2].

For example, following command can be used:

 cyclictest --mlockall -t -a --priority=99 --interval=200 --distance=0 -l 1000
Without RT feature With RT feature
policy: fifo: loadavg: 0.03 0.08 0.08 1/173 8476          

T: 0 ( 8475) P:99 I:200 C:   1000 Min:     15 Act:   71 Avg:   32 Max:     100
T: 1 ( 8476) P:99 I:200 C:    853 Min:     15 Act:   48 Avg:   31 Max:      65
policy: fifo: loadavg: 0.29 0.32 0.24 1/211 3815          

T: 0 ( 3814) P:99 I:200 C:   1000 Min:     15 Act:   21 Avg:   23 Max:      60
T: 1 ( 3815) P:99 I:200 C:    795 Min:     16 Act:   32 Avg:   20 Max:      59

5. References[edit source]