How to transfer files to Discovery kit using Tera Term on Windows PC

Revision as of 16:00, 23 November 2022 by Registered User

{{ArticleToRename | How to transfer files to Discovery kit using Tera Term on Windows PC | Balance the verb complements better |

Warning white.png Warning
This section has not been yet updated/tested for/with the STM32 MPU ecosystem-v4.
Information provided in this section may not be fully applicable for v4 and you may need to proceed to some adaptations.
We apologize for this inconvenient.

The article is written as an extension to the articles X-NUCLEO-NFC05A1 expansion board and X-NUCLEO-NFC06A1 expansion board. The purpose of this article is to specifically help users with steps to transfer any file from a Windows® PC to the STM32MP157F-DK2 Discovery kit More info green.png using "Tera Term"[1]. Download and install Tera Term on your Windows® PC and follow the steps listed below.


  • Plug the power cable to power-up the STM32MP157F-DK2 More info green.png.
  • Connect the STM32MP157F-DK2 Discovery kit More info green.png to your PC via a USB Micro-B cable through CN11.
  • Check the Virtual COM port number visible in the device manager. For example, in the snapshot below, the COM port number is 14.

VCOM Port Enumeration On DevManager.png


  • Open Tera Term on your PC and select the COM port (as found in step 3 above). The baud rate must be 115200 bauds. The virtual terminal (remote access) is displayed as shown in the snapshot below.

Snapshot Terminal TeraTerm.png


  • To transfer a file from the host PC to STM32MP157F-DK2 More info green.png,click on the File menu in the top-left corner of the Tera Term window and go to [File]>[Transfer]>[ZMODEM]>[Send...]. Refer to the snapshot below.

Snapshot TeraTerm ZMODEM Send.png


  • Select the file to be transferred from the pop-up window (see an example in the snapshot below) and click on the Open tab.

Snapshot TeraTermOpenFile.png

  • A progress bar shows the file transfer status as shown in the snapshot below

Snapshot FileTransferProgressBarTeraTerm.png


  • The transferred file is then available at /home/root on the STM32MP157F-DK2 More info green.png.

1. Reference[edit source]