This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Purpose[edit source]
This article gives an example of a driver that controls GPIOs from kernel space.
Sample source files are provided as examples: kernel module (driver), device tree and Makefile.
This example is available for or
2. Code[edit source]
2.1. Objective[edit source]
Sample gpiolib usage code that makes an LED blink for 20 seconds.
2.2. Device tree[edit source]
dummy_device { compatible = "st,dummy"; status = "okay"; greenled-gpios = <&gpioa 14 (GPIO_ACTIVE_HIGH | GPIO_PULL_UP)>; };
See GPIO_device_tree_configuration for more details of GPIO use in a device tree.
2.3. Kernel module code[edit source]
#include <linux/module.h>
#include <linux/of_device.h>
#include <linux/kernel.h>
#include <linux/delay.h>
#include <linux/gpio/consumer.h>
#include <linux/platform_device.h>
struct gpio_desc *red, *green;
static int gpio_init_probe(struct platform_device *pdev)
{
int i = 0;
printk("GPIO example init\n");
/* "greenled" label is matching the device tree declaration. OUT_LOW is the value at init */
green = devm_gpiod_get(&pdev->dev, "greenled", GPIOD_OUT_LOW);
/* blink of the green led */
while (i < 10)
{
ssleep(1);
gpiod_set_value(green, 1);
ssleep(1);
gpiod_set_value(green, 0);
i++;
}
return(0);
}
static int gpio_exit_remove(struct platform_device *pdev)
{
printk("GPIO example exit\n");
return(0);
}
/* this structure does the matching with the device tree */
/* if it does not match the compatible field of DT, nothing happens */
static struct of_device_id dummy_match[] = {
{.compatible = "st,dummy"},
{/* end node */}
};
static struct platform_driver dummy_driver = {
.probe = gpio_init_probe,
.remove = gpio_exit_remove,
.driver = {
.name = "dummy_driver",
.owner = THIS_MODULE,
.of_match_table = dummy_match,
}
};
module_platform_driver(dummy_driver);
MODULE_AUTHOR("Bernard Puel");
MODULE_DESCRIPTION("Gpio example");
MODULE_LICENSE("GPL");
MODULE_ALIAS("platform:dummy_driver");
2.4. Kernel module build[edit source]
See Adding_external_out-of-tree_Linux_kernel_modules for further information on module compilation.
2.5. Kernel module use[edit source]
scp dummy_driver.ko root@<board ip address>:/lib/modules/
- Update dependency descriptions for loadable kernel modules, and synchronize the data on disk with memory
/sbin/depmod -a sync
- Insert the kernel module example into the Linux kernel
modprobe dummy_driver [18167.821725] dummy_driver: GPIO example init