X-LINUX-AI - image classification using ONNX Python runtime

Revision as of 09:41, 18 October 2022 by Registered User
Applicable for STM32MP13x lines, STM32MP15x lines

This article explains how to experiment with ONNX Runtime [1] applications for image classification based on the MobileNet v1 model using ONNX Python runtime.

Info white.png Information
Python applications are good for prototyping but are less efficient than C/C++ application

1. Description[edit source]

The image classification neural network model allows identification of the subject represented by an image. It classifies an image into various classes.

Python ONNX runtime image classification application


The application enables three main features :

  • A camera streaming preview implemented using Gstreamer
  • A NN inference based on the camera (or test data pictures) inputs is being ran by the ONNX Runtime [1] interpreter
  • A user interface implemented using Python GTK.

The performances depend on the number of CPUs available. The camera preview is limited to one CPU core where the ONNX runtime[1] interpreter is configured to use the maximum of the available resources.

The model used with this application is the MobileNet v1 downloaded from the Tensorflow Lite Hub[2] and convert to ONNX opset 16 format using tf2onnx.

1.1. Convert a Tensorflow Lite model to ONNX using tf2onnx[edit source]

To convert a .tflite model to ONNX format, ONNX provide a tool named tf2onnx [3] which is very simple to use.

The first step is to install Tensorflow on the host computer, for test purposes it could be useful to install also ONNX Runtime. Tool tf2onnx will use the already installed versions of Tensorflow and ONNX runtime, if it does not find any it will install the most recent versions.

The second step is to install tf2onnx :

- Install from pypi :

 pip install -U tf2onnx

or

- Install latest from github :

 pip install git+https://github.com/onnx/tensorflow-onnx

After the installation, you are able to convert the tflite model directly using the following command line :

  python -m tf2onnx.convert --opset 16 --tflite path/to/tflite/model.tflite --output path/to/onnx/model/model.onnx

Native ONNX models are also available in the ONNX Model Zoo [4]

2. Installation[edit source]

2.1. Install from the OpenSTLinux AI package repository[edit source]

Warning white.png Warning
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here.

After having configured the AI OpenSTLinux package you can install the X-LINUX-AI components for this application:

 apt-get install onnx-cv-apps-image-classification-python

And restart the demo launcher:

- For OpenSTLinux distribution with a version lower than 4.0 use

 systemctl restart weston@root

- For other OpenSTLinux distribution use :

 systemctl restart weston-launch

2.2. Source code location[edit source]

The label_onnx.py Python script is available:

  • in the Openembedded OpenSTLinux Distribution with X-LINUX-AI Expansion Package:
<Distribution Package installation directory>/layers/meta-st/meta-st-stm32mpu-ai/recipes-samples/onnxrt-cv-apps/files/image-classification/python/label_onnx.py
  • on the target:
/usr/local/demo-ai/computer-vision/onnx-image-classification/python/label_onnx.py
  • on GitHub:
https://github.com/STMicroelectronics/meta-st-stm32mpu-ai/tree/v2.2.0/recipes-samples/onnxrt-cv-apps/files/image-classification/python/label_onnx.py

3. How to use the application[edit source]

3.1. Launching via the demo launcher[edit source]

Demo launcher

3.2. Executing with the command line[edit source]

The Python script label_onnx.py application is located in the userfs partition:

/usr/local/demo-ai/computer-vision/onnx-image-classification/python/label_onnx.py

It accepts the following input parameters:

usage: label_onnx.py [-h] [-i IMAGE] [-v VIDEO_DEVICE] [--frame_width FRAME_WIDTH] [--frame_height FRAME_HEIGHT] [--framerate FRAMERATE]
                     [-m MODEL_FILE] [-l LABEL_FILE] [--input_mean INPUT_MEAN] [--input_std INPUT_STD] [--validation]
                     [--num_threads NUM_THREADS]

options:
  -h, --help            show this help message and exit
  -i IMAGE, --image IMAGE
                        image directory with image to be classified
  -v VIDEO_DEVICE, --video_device VIDEO_DEVICE
                        video device (default /dev/video0)
  --frame_width FRAME_WIDTH
                        width of the camera frame (default is 640)
  --frame_height FRAME_HEIGHT
                        height of the camera frame (default is 480)
  --framerate FRAMERATE
                        framerate of the camera (default is 15fps)
  -m MODEL_FILE, --model_file MODEL_FILE
                        .onnx model to be executed
  -l LABEL_FILE, --label_file LABEL_FILE
                        name of file containing labels
  --input_mean INPUT_MEAN
                        input mean
  --input_std INPUT_STD
                        input standard deviation
  --validation          enable the validation mode
  --num_threads NUM_THREADS
                        Select the number of threads used by ONNX interpreter to run inference

3.3. Testing with MobileNet V1[edit source]

The model used for test is the mobilenet_v1_0.5_128_quant.onnx downloaded from Tensorflow Lite Hub[2] and converted to ONNX format.

Info white.png Information
The different objects the neural network is able to classify are listed in the labels_onnx.txt file located in the target:

/usr/local/demo-ai/computer-vision/models/mobilenet/labels_onnx.txt

To ease launching of the Python script, two shell scripts are available:

  • launch image classification based on camera frame inputs
 /usr/local/demo-ai/computer-vision/onnx-image-classification/python/launch_python_label_onnx_mobilenet.sh
  • launch image classification based on the pictures located in /usr/local/demo-ai/computer-vision/models/mobilenet/testdata directory:
 /usr/local/demo-ai/computer-vision/onnx-image-classification/python/launch_python_label_onnx_mobilenet_testdata.sh
Info white.png Information
Note that you need to populate the testdata directory with your own data sets.

The pictures are then randomly read from the testdata directory

4. References[edit source]