How to develop an X-Linux Expansion Package

Revision as of 16:45, 2 November 2022 by Registered User
Applicable for STM32MP13x lines, STM32MP15x lines


OpenSTLinux ExPackages H.jpg

On this page, learn how to create your own STM32MPU Expansion package to extend the limit of the ecosystem.

1. Design of a STM32MPU Expansion for OpenSTLinux Distribution Package[edit source]

A STM32MPU Expansion package for OpenSTLinux Yocto distribution is a solution proposed to extend a Distribution Package by providing new features, examples or demonstrations.

STM32MPU_Expansion_Package


Three possible profile types are defined to covered different user needs and following the required changes on the OpenSTLinux distribution:

  1. OpenSTLinux tools add-on: in case of making changes only at Linux user space level, without any changes on boot chain or Linux OS.
  2. OpenSTLinux embedded software add-ons: in case of modifying Linux kernel part (configuration, device tree update), or/and adding user space application(s)/framework(s) needed to demonstrate Cortex-A processor functionality
  3. Coprocessor and OpenSTLinux embedded software add-ons: in case of profile type 2 and/or need to modify STM32CubeMPU part and/or to include new firmware source code example to demonstrate Cortex-M coprocessor functionality

2. Check for OpenSTLinux compability version[edit source]

For ecosystem release ≥ v3.1.0 :

In order to ensure the adherence with a given OpenSTLinux version, the dependency is managed with a dedicated ST_OSTL_COMPATIBILITY_VERSION_<layer_name> variable to set in the I-PACK Yocto meta layer (layer.conf file).
This information is verified at compilation phase.

To get the version to set, please refer to the variable value given in meta-st-openstlinux/conf/layer.conf , for example:

ST_OSTL_COMPATIBILITY_VERSION_st-openstlinux = "3.1"
Warning white.png Warning
As soon as a new OpenSTlinux release version or major revision is published, if you want to indicate the I-Pack is compliant (it means "validated with") with it, you need to update the corresponding compatibility version variable ST_OSTL_COMPATIBILITY_VERSION accordingly in the I-Pack expansion package; otherwise a build error is generated


For ecosystem release ≤ v3.0.0 :

Typo issue was present: ST_OSTL_COMPATIBILTY_VERSION instead of ST_OSTL_COMPATIBILITY_VERSION

In order to ensure the adherence with a given OpenSTLinux version, the dependency is managed with a dedicated ST_OSTL_COMPATIBILTY_VERSION_<layer_name> variable to set in the I-PACK Yocto meta layer (layer.conf file).
This information is verified at compilation phase.

To get the version to set, please refer to the variable value given in meta-st-openstlinux/conf/layer.conf , for example:

ST_OSTL_COMPATIBILTY_VERSION_st-openstlinux = "3.0"
Warning white.png Warning
As soon as a new OpenSTlinux release version or major revision is published, if you want to indicate the I-Pack is compliant (it means "validated with") with it, you need to update the corresponding compatibility version variable ST_OSTL_COMPATIBILTY_VERSION accordingly in the I-Pack expansion package; otherwise a build error is generated

3. STM32MPU Expansion cases[edit source]

3.1. OpenSTLinux tools add-on[edit source]

This profile type covers the case when only changes/additions are done at Linux user space level for application(s), tool(s) or script(s) on the root file system.

Two possible approaches:

  • Add a Standard Yocto layer on the OpenSTLinux distribution: please refer to existing skeleton example[1] in yocto project
  • Deploy a Debian package on the target: in case all dependencies are already managed on Embedded software on the target, this is possible to install the new application(s) by using a standard Debian package

3.2. OpenSTLinux embedded software add-ons[edit source]

This profile type covers previous one and is recommended when some additional changes are required at Linux kernel level (configuration and/or device tree update), and/or adding user space application(s)/framework(s) needed to demonstrate Cortex-A processor functionalities.

For this case, the OpenSTLinux distribution must be updated, and the proposed solution is to add a new add-on meta layer to provide the services described below. A meta layer template is proposed as reference to help modifying BSP components: meta-st-stm32mp-addons[2].

Otherwise, if only user space applications and image need to be updated, please refer to existing skeleton example[1] in Yocto project for a standard Yocto layer.

3.2.1. New image creation with additional Linux user space packages[edit source]

Refer to the How_to_create_your_own_image wiki page.

As example, please have a look the the X-LINUX-AI expansion package image recipe: https://github.com/STMicroelectronics/meta-st-stm32mpu-ai/blob/master/recipes-st/images/st-image-ai.bb

3.2.2. TF-A, OP-TEE, U-Boot, Kernel device tree(s) update[edit source]

Two possible approaches, which depend of the way the top device tree source file is written for the given reference board:

  • The dts file contain the complete device tree settings and is generated by using CubeMx (see STM32CubeMX_generated_device_tree)
  • A new device tree source file (.dts) inherit from an existing DT file of a ST board and is used to modify/add DT node Overload the device tree (i.e. minor changes compared to existing boards)

For both approaches, the way to declare it in the I-Pack meta layer is the same, and is done in the machine file (conf/machine directory). For example please see conf/machine/stm32mp13-mx.conf (STM32MP13x lines More info.png) or conf/machine/stm32mp15-mx.conf (STM32MP15x lines More info.png).

  • Force the new device tree source file usage: ENABLE_CUBEMX_DTB ?= "1"
  • Define the dtb binary name to be generated, which is the same as the dts file you want to use: CUBEMX_DTB = "<your_dtb_file_name>"
  • Define the path for the device tree files: CUBEMX_PROJECT = "'<your_dt_file_path>"

Ensure the corresponding device tree source files that have to be taken into account must be present in the path given by variable CUBEMX_PROJECT previously defined.

Then, as the examples provided in meta-st-stm32mp-addons[2], this is possible for each BSP components to define the device tree source file to be used by an update of the corresponding recipes.

Component Yocto recipe append example for BSP components
TF-A tf-a-stm32mp_%.bbappend
OP-TEE optee-os-stm32mp_%.bbappend
U-Boot u-boot-stm32mp_%.bbappend
Linux Kernel linux-stm32mp_%.bbappend

3.2.3. Linux kernel configuration change[edit source]

Two possible approaches:

  • Make defconfig changes by using a configuration fragment file (recommended)
  • Provide a full defconfig file
3.2.3.1. Change defconfig with a configuration fragment file[edit source]

A simple way to update the Linux kernel configuration is to use a fragment file. You can refer to the Yocto Project web article Creating Configuration Fragments for information.

The config fragment file must be added in the path meta-st-stm32mp-addons/recipes-kernel/linux/linux-stm32mp/<config_fragment_file_name>.

The linux-stm32mp recipe file must be appended in order to update the build setup. It is done through the file meta-st-stm32mp-addons/recipes-kernel/linux/linux-stm32mp_%.bbappend.

In this file, the new config fragment file must be added to the variable KERNEL_CONFIG_FRAGMENTS and listed in the SRC_URI variable as given below:

FILESEXTRAPATHS_prepend := "${THISDIR}/${PN}:"
SRC_URI += "file://<config_fragment_file_name>"
KERNEL_CONFIG_FRAGMENTS += "<config_fragment_file_name>"
3.2.3.2. Use new full defconfig file[edit source]

This is also possible to provide a full defconfig file for the Linux kernel configuration building.
For creating a defconfig file, please refer to the Yocto Project web article Creating a defconfig File.

The file must be present in the path meta-st-stm32mp-addons/recipes-kernel/linux/linux-stm32mp/<defconfig_file_name>.

The linux-stm32mp recipe file must be appended in order to update the build setup. It is done through the file meta-st-stm32mp-addons/recipes-kernel/linux/linux-stm32mp_%.bbappend.

In this file, the variable KERNEL_DEFCONFIG has to be cleaned, the new variable KERNEL_EXTERNAL_DEFCONFIG must be defined and the path of the <defconfig_file_name> listed in the SRC_URI variable as given below:

FILESEXTRAPATHS_prepend := "${THISDIR}/${PN}:"
SRC_URI += "file://<defconfig_file_name>"
KERNEL_DEFCONFIG = ""
KERNEL_EXTERNAL_DEFCONFIG = "<defconfig_file_name>"

3.2.4. Addition of source code / binary files for new applications[edit source]

Refer to How_to_add_a_customer_application wiki article.

Two other wiki pages are also proposed to help for meta-st-stm32mp-addons usage:

3.3. Coprocessor and OpenSTLinux embedded software add-ons[edit source]

Under construction.png Coming soon

This profile type inherit from OpenSTLinux embedded software add-ons and is recommended when some changes are required at STM32CubeMPU part and/or to include new firmware source code example to demonstrate Cortex-M coprocessor functionality (including hardware resources reallocations).


4. I-Pack expansion package example[edit source]

X-LINUX-AI_OpenSTLinux_Expansion_Package

5. References[edit source]