How to adjust USBPHYC settings using USB Eye Diagram

Revision as of 11:03, 25 October 2022 by Registered User
Applicable for STM32MP13x lines, STM32MP15x lines

The purpose of this article is to describe the basic steps required to tune or troubleshoot the USB High-Speed PHYs from hardware and software perspectives.

1. General recommendations[edit source]

The eye diagram is characterized with a specific reference resistor on board, between the STM32 MPU device USB_RREF pin and ground.

Verify first that USB_RREF resistor is correctly connected and has proper value and precision (3 kΩ 1%)

2. Eye Diagram[edit source]

Common modeJitterLevel attenuationRising edgeRippleSignal-to-NoiseFalling edgeCommon modeJitterLevel attenuationRising edgeRippleSignal-to-NoiseFalling edgeUSB Eye diagram.png

2.1. Common mode troubleshooting[edit source]

Hardware root causes to investigate
  • Mismatch between D+ and D- (in terms of length and/or parallelism)
  • Check layout and add common mode filter (e.g. ECMF02-2AMX6[1])
Info white.png Information
It is not possible to solve common mode issue with software.

2.2. Jitter troubleshooting[edit source]

Hardware root causes to investigate
  • Too much capacitance (component or PCB) on D+/D- lines
  • USB Power/GND instability
Check decoupling / Check grounding
Fine tuning may be performed by using USBPHYC device tree configuration [2]

High jitter has an HW root cause in most cases.

  • USBPHYC_TUNEx.HSDRVRFRED
0: increase rising edge but add jitter (i.e. remove st,enable-hs-rftime-reduction;[3])
  • USBPHYC_TUNEx.INCURREN/.INCURRINT
Tune current increase with .INCURREN or .INCURRINT (i.e. remove st,current-boost-microamp= <n>;[3] or set it to 1000µA or 2000µA)
  • USBPHYC_TUNEx.HSDRVCHKITRM
Reduce the increase of the main level (i.e. reduce value of st,trim-hs-current = <n>;[3])

2.3. Level attenuation or Signal-to-Noise troubleshooting[edit source]

Hardware root causes to investigate
  • too much serial resistance and capacitance (component or PCB) on D+/D- lines
  • USB Power/GND instability
Check decoupling / Check grounding
Software potential tuning
  • USBPHYC_TUNEx.HSDRVCHKITRM
Higher the value, higher will be the level of signal (i.e. increase value of st,trim-hs-current = <n>;[3]).
But noise and ripple can appear
  • USBPHYC_TUNEx.HSDRVCURINCR/.HSDRVDCLEV
Higher the value, higher will be the margin for the level (i.e. increase value of st,hs-dc-level = <n>;[3]).
But jitter in the rising edge and noise can appear

2.4. Rising edge or Falling edge troubleshooting[edit source]

Hardware root causes to investigate
  • too much serial resistance and capacitance (component or PCB) on D+/D- lines
  • Impedance mismatch : check characteristic impedance of lines, stubs…
Software potential tuning
  • USBPHYC_TUNEx.HSDRVRFRED
0: improve rising edge (i.e. remove st,enable-hs-rftime-reduction;[3])
1: slow-down rising edge (i.e. add st,enable-hs-rftime-reduction;)
Potential impact on jitter
  • USBPHYC_TUNEx.HSDRVCHKITRM
Depending on level, slope is increased/decreased (i.e. adjust value of st,trim-hs-current = <n>;[3])
  • USBPHYC_TUNEx.HSDRVSLEW
0: normal rising edge (i.e. remove st,decrease-hs-slew-rate;[3])
1: reduce rising edge (i.e. add st,decrease-hs-slew-rate;)
Useful to reduce a hill shape ripple on top of rising/falling edge
  • USBPHYC_TUNEx.HSDRVCURINCR/.HSDRVDCLEV
Improve slope speed (i.e. increase value of st,hs-dc-level = <n>;[3]).
But jitter in the rising edge and noise can appear

2.5. Ripple troubleshooting[edit source]

Hardware root causes to investigate
  • Impedance mismatch : check characteristic impedance of lines, stubs…
Software potential tuning
  • USBPHYC_TUNEx.HSDRVCHKZTRM[1:0]
00: Usually open the eye but can create some jitter and ripple (i.e. st,trim-hs-impedance = <0>;[3])
11: Close the eye but can reduce jitter and ripple (i.e. st,trim-hs-impedance = <3>;)
  • USBPHYC_TUNEx.HSDRVSLEW
0: normal rising edge (i.e. remove st,decrease-hs-slew-rate;[3])
1: reduce rising edge (i.e. add st,decrease-hs-slew-rate;)
Useful to reduce a hill shape ripple on top of rising/falling edge

3. Link between Register values and Device Tree description[edit source]

Only few bitfields should be adjusted in the scope of Eye Diagram tuning. It is recommended to keep other as described in default Device Tree examples. See also USBPHYC device tree bindings[3]

Device Tree item details USBPHYC_TUNEx field
st,current-boost-microamp <1000> current boosting of 1mA .INCURREN=1/.INCURRINT=0
<2000> current boosting of 2mA .INCURREN=1/.INCURRINT=1
st,no-lsfs-fb-cap disables the LS/FS feedback capacitor .LFSCAPEN=1
st,decrease-hs-slew-rate slows the HS driver slew rate by 10% .HSDRVSLEW=1
st,hs-dc-level <0> normal level .HSDRVCURINCR=0/.HSDRVDCCUR=0
<1> increases the HS driver DC level by 5 to 7mV .HSDRVCURINCR=1/.HSDRVDCLEV=0
<2> increases the HS driver DC level by 10 to 14mV .HSDRVCURINCR=1/.HSDRVDCLEV=1
<3> decreases the HS driver DC level by 5 to 7mV .HSDRVDCCUR=1
st,enable-fs-rftime-tuning enables the FS rise/fall tuning option .FSDRVRFADJ=1
st,enable-hs-rftime-reduction enables the HS rise/fall reduction feature .HSDRVRFRED=1
st,trim-hs-current controls HS driver current trimming for choke .HSDRVCHKITRM=n [0:15]
st,trim-hs-impedance controls HS driver impedance tuning for choke .HSDRVCHKZTRM=n [0:3]
st,tune-squelch-level adjusts the squelch DC threshold value .SQLCHCTL=n [0:3]
st,enable-hs-rx-gain-eq enables the HS Rx gain equalizer .HDRXGNEQEN
st,tune-hs-rx-offset adjusts the HS Rx offset .HSRXOFF=n [0:3]
st,no-hs-ftime-ctrl disables the HS fall time control of single ended signals during pre-emphasis .HSFALLPREEM=1
st,no-lsfs-sc disables the short circuit protection in LS/FS driver .SHTCCTCTLPROT
st,enable-hs-tx-staggering enables the basic staggering in HS Tx mode .STAGSEL

4. Software configuration to enter test modes[edit source]

This section describes how to

4.1. Device tree configuration[edit source]

The Target Peripheral List (TPL) is used to identify targeted devices during Embedded Host compliance testing. The user can add "tpl-support" in the board device tree file to enable it.

# Enable Target Peripheral List on USBH, on both EHCI and OHCI controllers:
&usbh_ehci {
+	tpl-support;
};

&usbh_ohci {
+	tpl-support;
};
# Enable Target Peripheral List on OTG:
&usbotg_hs {
+	tpl-support;
};

5. References[edit source]