This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.
Das U-Boot ("the Universal Boot Loader" or U-Boot) is an open-source bootloader that can be used on STMicroelectronics boards to initialize the platform and load the Linux® kernel.
See U-Boot overview for generic information.
Information about U-Boot depends on the microprocessor device.
Several articles have been created to manage STM32 MPU diversity and provide the relevant level of information. Browse the one corresponding to the STM32 MPU you use.
STM32 MPU devices | Associated articles |
---|---|
STM32MP13x lines ![]() |
STM32MP13 U-Boot |
STM32MP15x lines ![]() |
STM32MP15 U-Boot |