OP-TEE OTP overview

Revision as of 10:55, 27 June 2022 by Registered User (→‎System overview)
Applicable for STM32MP13x lines, STM32MP15x lines

This article gives information about the OTP framework in OP-TEE and the associated interfaces.

1. Framework purpose[edit source]

The OP-TEE OTP PTA provides a generic interface for the device non-volatile OTP (one-time programmable) fuses.

It offers interfaces to read and/or write OTP data and status at Trusted Applications (TA) in secure world and at non-secure applications.

2. System overview[edit source]

Under construction.png Coming soon

2.1. Component description[edit source]

  • NVMEM framework (kernel space)

The NVMEM framework in Linux® kernel provides sysfs interface and NVMEM API.

  • NVMEM drivers (kernel space)

Provider drivers such as BSEC Linux® driver that exposes OTP data to the core.

  • TEE framework (kernel space)

The TEE framework provides TEE client API to communicate with secure services, as the services provided by the OP-TEE Linux® driver.

  • OP-TEE (Secure)

The OP-TEE secure OS is running on the Cortex-A in secure mode and exposes secure service with Trusted Applications (TA), as BSEC PTA and NVMEM PTA.

Under construction.png Coming soon

2.2. API description[edit source]

The OTP interface is provided by two trusted applications (TA) in OP-TEE, accessible from the normal world with the GlobalPlatform API:

3. References[edit source]

Please refer to the following links for additional information: