STM32 MPU OpenSTLinux release note - v4.0.0

Revision as of 08:31, 28 June 2022 by Registered User
Applicable for STM32MP13x lines, STM32MP15x lines

This article describes the content of OpenSTLinux distribution software release version openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15, which is part of STM32 MPU ecosystem release note - v4.0.0.

1. Intended audience[edit source]

The targeted audience is STM32MP13x lines More info.png and STM32MP15x lines More info.png customers or partners.

2. Delivery scope and purpose[edit source]

The OpenSTLinux distribution is a Linux® distribution based on the OpenEmbedded build Framework. It runs on the Arm® Cortex®-A7 processors, and is a fundamental part of the STM32MPU Embedded Software distribution.

This delivery of OpenSTLinux distribution is part of STM32 MPU Ecosystem v4.0.0 (see the STM32 MPU ecosystem release note - v4.0.0).

3. Licensing[edit source]

This software package is licensed under a LIMITED LICENSE AGREEMENT FOR ST MATERIALS EVALUATION (LLA). Customers may not use this package except in compliance with the software license agreement (SLA).

All of the packages use the same source components. All components and their respective licenses are listed here.

4. Supported hardware[edit source]

This software delivery is compatible with the following boards:

  • STM32MP135D-DK unknown board type identifier and STM32MP135F-DK More info green.png Discovery kits of STM32MP13x lines More info.png.
  • STM32MP157A-EV1 Warning.png(obsolete), STM32MP157C-EV1 Warning.png(obsolete), STM32MP157D-EV1 More info green.png and STM32MP157F-EV1 More info green.png Evaluation boards of STM32MP15x lines More info.png.
  • STM32MP157A-DK1 Warning.png(obsolete), STM32MP157C-DK2 Warning.png(obsolete), STM32MP157D-DK1 More info green.png and STM32MP157F-DK2 More info green.png Discovery kits of STM32MP15x lines More info.png.

5. Delivered features[edit source]

5.1. Main software components[edit source]

  • Linux kernel v5.15-stm32mp-r1 (v5.15.24)
  • TF-A v2.6-stm32mp-r1
  • U-Boot v2021.10-stm32mp-r1
  • OP-TEE 3.16.0-stm32mp-r1
  • STM32CubeMP1 Package v1.6.0
  • OpenEmbedded v4.0.1 (Kirkstone)
  • Weston version v10.0.0
  • Wayland version 1.20.0
  • GStreamer version v1.20.1
  • GCC version v11.2
  • OpenOCD version v0.11.0
  • GCnano version v6.4.7

5.2. Detailed features[edit source]

5.2.1. OpenSTLinux layers part[edit source]

  • Rebase on Yocto LTS Release 4.0.1 (Kirkstone)
  • Many impacts in recipes
  • Graphic frameworks user change for security reasons (change from Weston community)
  • Machine:
  • New stm32mp13-disco for STM32MP135D-DK unknown board type identifier and STM32MP135F-DK Discovery kit More info green.png
  • Add support of Firmware Update feature
  • Minor fixes
Info white.png Information
From this release OpenSTLinux v4.0.0, FIP configuration is the only packaging format supported for boot loaders (more about FIP here) :
  • 0nly TF-A BL2 requires the stm32 header for a ROM code authentication. Others bootloader binaries are embedded in a FIP container.
  • A dedicated fip-utils-stm32mp.bbclass class is provided on meta-st-stm32mp layer side to manage the FIP image configuration, build and update.

5.2.2. Linux® kernel part[edit source]

New component release tag v5.15-stm32mp-r1 rebased on official Linux® kernel v5.15.24.

Main updates for STMP32MP1:

  • CONFIG: STM32MP13x lines More info.png and STM32MP15x lines More info.png support
  • DT: New boards STM32MP135F-DK Discovery kit More info green.png and STM32MP135D-DK unknown board type identifier support
  • FMC nand driver Write Protect(WP) function support
  • RTC ALARM TOGGLE
  • Minor fixes


STM32MP15x lines More info.png:

  • LCD Rocktech RK055MHD042A0-CTG support

5.2.3. U-boot part[edit source]

New component release tag v2021.10-stm32mp-r1 rebased on official U-Boot v2021.10

Main updates for STMP32MP1:

  • Device tree alignment with Linux kernel v5.15-stm32mp-r1
  • Add STM32MP13x family support
  • DDR tuning support removed
  • Activate CONFIG_OF_LIVE
  • Activate CONFIG_LOG
  • Deactivate IPCC driver
  • Add Uclass USB typeC and driver for UCSI
  • Add USB phy tuning support
  • Add NAND Write Protect support
  • Add ADC calibration support
  • Add TF-A firmware update support
  • Update SCMI support for OP-TEE transport
  • Add BSEC and stm32prog support with OP-TEE and TA
  • ADC calibration in U-Boot
  • Other minor updates
Info white.png Information
The U-Boot defconfig to use for ecosystem release ≥ v4.0.0 change to stm32mp15_defconfig.
Warning white.png Warning
SPL and STM32Image is no more supported in OpenSTLinux U-Boot. Migrate to TF-A with FIP support instead.

5.2.4. TF-A part[edit source]

New component release tag v2.6-stm32mp-r1 rebased on official TF-A 2.6

Main updates for STM32MP1:

  • Rebase OpenSTLinux delivery on official TF-A tag v2.6
  • Introduction of STM32MP13 platform
  • FIP encryption for STM32MP13
  • Firmware Update (FWU) support
  • Early console management
  • Configurable baudrate for UART
  • Serial boot (USB/UART): flashlayout is no more loaded by BL2
  • BL2 always boots at 650MHz
  • Removal of STM32IMAGE legacy boot
  • Minor fixes


5.2.5. OP-TEE part[edit source]

New component release tag 3.16.0-stm32mp-r1 rebased on official OP_TEE OS 3.16.0

Main updates for STMP32MP1:

  • Introduction of STM32MP13 platform
  • OP-TEE Updated driver model based on DT
  • New driver probing model based on device tree
  • Support IRQ threads
  • Fix GIC low-power sequence
  • Pinctrl, I2C and clocks are now providers
  • Rework HSI/LSI clocks calibration as a PTA
  • OTP PTA interface for OTP management
  • TA NVMEM for OTP provisionning support
  • CRYP/HASH/BSEC/TAMP driver update
  • TZC400 full configuration
  • RNG connection to HW RNG PTA -> RNG secure by default
  • Firewall bus management update
  • Backup battery charging
  • Replace Python wand with a new supported library
  • Support Secured display
  • Minor Fixes
  • Documentation: Add device tree bindings documentation
  • STM32MP15x lines More info.png:
  • Probe non secure IP management

6. Recommendations for use[edit source]

6.1. Safe use[edit source]

  • Flash programming and boot from all supported flash devices: SDCard, eMMC, ONFI NAND and NOR flash memories
  • Develop Linux® applications, libraries, kernel modules based on OpenSTLinux delivery
  • Develop coprocessor Cube applications based on STM32CubeMP1 delivery
  • Develop boards based on STM32MP1 Series
  • Prototype applications based on ST boards

6.2. Non-recommended use[edit source]

  • None

7. Main restrictions list[edit source]

  • Sysprof issue when making a record
  • If Firmware Update is not enable, flashlayout partition no more needed, but storage mapping hardcoded in U-Boot; so either flashlayout keep partitions for Firmware Update feature or U-Boot needs to be updated.
Warning white.png Warning
On an Ubuntu 18.04 (with a host gcc version prior to 8.0), U-Boot cannot be built by using the STM32MP1_Developer_Package because of the usage of an unsupported option : -fmacro-prefix-map .

8. Minor release updates[edit source]

STMicroelectronics regularly delivers corrections through github® components which are U-Boot, OP-TEE, TF-A, Linux kernel.
The corrections can be incorporated into the Developer Package (refer to STM32MP1 Developer Package) or Distribution Package (see below).

Two possibilities exist to update a Distribution Package:

  • Update your existing Distribution Package:
Switch your Distribution Package to # github® mode .
  1. Use the devtool modify <recipe name> command to set up an environment. It will fetch and unpack the source code.
  2. In the extracted source code, use a git command such as git checkout -b WORK <github® TAG> to point to a new revision of the component.
More rarely STMicroelectronics also delivers fixes on layers through github®. These changes can be integrated (via git commands: git checkout -b WORK <github® commit SHA1>) into the local STM32MP1 Distribution Package environment. See below the github® links of the quoted layers :
  • Get a new Distribution Package:
Refer to Installing_the_OpenSTLinux_distribution page for install instructions, and use the repo command given for the minor version below, if it exists.

9. How to get started with openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15[edit source]

Refer to How to download the software and start with this release?

10. Associated tools[edit source]

Refer to the Referenced tools release notes .

11. Features enabled in the delivery[edit source]

OpenEmbedded[1] build framework engine is named OE-Core.
OpenSTLinux distribution is based on the build framework OpenEmbedded, and can be configured thanks to a mechanism named "features" (machine features, distribution features, ...).

Depending on features enabled, the resulting distribution can have more capabilities or software embedded.
For example, if wifi is enabled then wifi software and drivers will be present on the filesystem and wifi can be used.

11.1. Machine features[edit source]

The variable MACHINE_FEATURES specifies the list of hardware features the machine is capable of supporting.
These features (MACHINE_FEATURES) are defined inside the machine configuration .

Machine feature Purpose
alsa Include ALSA support (OSS compatibility kernel modules installed if available).
autoresize Add support of autoresize through InitRD
bluetooth Add Broadcom43430 (Bluetooth) firmware to the filesystem
(STM32MP135x-DK Discovery kit More info green.png and STM32MP157x-DKx Discovery kit More info green.png)
ext2 Add Second Extended File System support
fip Enable Firmware In Package (FIP) packaging format
fw-update Enable Firmware update feature
gpu Add GPU support (if EULA is accepted) (STM32MP157 line More info.png only)
initrd Enable Intial ramdisk building
m4copro Add m4projects to userfs (STM32MP15x lines More info.png only)
optee Add OP-TEE Secure part
pci Add Peripheral Component Interconnect peripheral support
rtc Add Real Time Clock peripheral support
screen Add display screen peripheral support
splashscreen Add splashscreen to U-Boot
tpm2 Add Trusted Platform Module peripheral support
usbg0 Add G0 Firmware for USB support
usbgadget Enable USB Gadget feature
usbhost Enable USB Host feature
watchdog Add watchdog support and binaries
wifi Add Broadcom43430 (wifi) firmware to the filesystem
(STM32MP135x-DK Discovery kit More info green.png and STM32MP157x-DKx Discovery kit More info green.png)

11.2. Distribution features[edit source]

The variable DISTRO_FEATURES specifies the list of software features present in the distribution.
These features (DISTRO_FEATURES) are defined inside the distribution configuration .

Distribution feature Purpose
alsa Include ALSA support (OSS compatibility kernel modules installed if available).
argp
autoresize Add support of userfs auto resize feature in OpenSTLinux
bluetooth Include Bluetooth support
bluez5 Add Bluetooth stack
efi Add userland EFI tools
ext2 Add Second Extended File System support
ext4 Add Fourth Extended File System support
gobject-introspection-data Enable GObject Introspection, project for providing machine readable introspection data of the API of C libraries.
gplv3 Add gplv3 binaries in OpenSTLinux
gstreamer Add gstreamer tools in filesystem
initrd Add ramdisk
ipv4 Add ipv4 support
ipv6 Add ipv6 support
kde Add several tools (e.g. cups, fontconfig, ...) to the filesystem
largefile Enable large file support
ldconfig Include support for ldconfig and ld.so.conf on the target
multiarch Enable 64 bits BFD (Binary File Descriptor)
nfs Include NFS client support (for mounting NFS exports on device).
opengl Include the Open Graphics Library
optee Install tee service on the filesystem
pam Enable Pluggable Authentication Module
pci Add pci support
polkit Enable PolicyKit for controlling system-wide privileges
pulseaudio Network-capable sound server program
splashscreen Add U-Boot splashscreen
systemd Use systemd as init service
usbgadget USB Gadget Device support (for USB networking/serial/storage)
usbhost USB Host support (allows to connect external keyboard, mouse, storage, network etc)
wayland Add Wayland support
wifi WiFi support
xattr Add "Extended Attributes" support for filesystem
zeroconf Add zeroconf package to set up a ad-hoc network

11.3. Bootscheme labels[edit source]

The variable BOOTSCHEME_LABELS defines which kind of boot is supported on the board.
These settings (BOOTSCHEME_LABELS) are defined inside the machine configuration .

Bootscheme label Purpose
optee Add optee in bootscheme
trusted Add trusted in bootscheme

11.4. Bootdevice labels[edit source]

The variable BOOTDEVICE_LABELS defines which kind of mass storage OpenSTLinux can programmed.
These settings (BOOTDEVICE_LABELS ) are defined inside the machine configuration .

Bootdevice label Purpose
emmc Add boot on emmc device
nand-4-256 Add boot on NAND device
nor-sdcard Add boot stage on NOR device and the filesystem on SD-Card
sdcard Add boot on SD-Card