OP-TEE Calibration PTA overview

Revision as of 17:57, 22 June 2022 by Registered User

This article gives information about the OP-TEE OS Calibration PTA.

1. PTA Calibration purpose[edit source]

The purpose of this article is to explain to access to the HSI and CSI oscillators calibration service.

These internal oscillators are initially calibrated at chip production level. But, they can be affected by temperature and voltage variations and it is important to provide a mechanism to compensate the effects of these variations to achieve a good frequency accuracy.

The service provides a way to calibrate the oscillator based on timer comparison between oscillator and a refence clock derived from the HSE clock that is considered as always accurate.

Refer to STM32MP13 reference manuals or STM32MP15 reference manuals for detailed information on the timer channels that can be used for HSI or CSI calibration input.

2. System overview[edit source]

OP-TEE calibration overview

2.1. Components description[edit source]

Non secure world:

  • Calibration Timer (User Space): User space service (systemd based) that call the calibration binary at every choosen timer expiration.
  • Calibration (User Space): User space client application that connects to the calibration PTA to request the calibration execution.
  • TEE Core API Lib (User Space): Library called by the client application to access to the kernel space.
  • OP-TEE driver (Kernel Space): Generic driver that send the message to the OP-TEE OS.

Secure World:

  • Calibration PTA (Kernel Space): Interface that expose the calibration specific services.
  • Calibration driver (Kernel Space): Specific calibration driver that control and calculate the calibration values.
  • TIM driver (Kernel Space): Timer driver using the OP-TEE counter framework.
  • STM32 peripherals (Hardware): Access to hardware specific peripherals (RCC, TIM) under firewall access control.

2.2. API description[edit source]

The calibration PTA offers a single interface to request a calibration. The calibration is started on HSI and/or CSI depending the calibration driver initialization defined using the Calibration_device_tree_configuration.

3. Configuration[edit source]

3.1. OP-TEE_OS configuration[edit source]

Activate Calibration PTA in OP-TEE configuration core/arch/arm/plat-stm32mp1/conf.mk :

CFG_STM32_CLKCALIB ?=y

3.2. Device tree configuration[edit source]

Detailed DT configuration for STM32 internal peripherals:

4. How to use the framework[edit source]

A default calibration application is released in the OpenSTLinux ecosystem to give a reference implementation for the calibration service.

5. References[edit source]