STM32 MPU Flash mapping

Revision as of 15:06, 17 June 2022 by Registered User (→‎Flash partitions)
Applicable for STM32MP13x lines, STM32MP15x lines


1. Supported Flash memory technologies[edit source]

STM32MP1 Series support the following types of Flash memory and the sub-bullets below show which interfaces are supported on STMicroelectronics boards:

  • SD card on the SDMMC interface
  • eMMC on the SDMMC interface
  • Serial NOR Flash memory on the Dual QSPI interface
  • NAND Flash memory on the FMC interface

The next section lists all partitions used on STM32MP1 boards (size, name, and content), and the following sections show how they are mapped on the different types of Flash memory.

2. Flash partitions[edit source]

The tables below list the partitions defined for STMP32MP1 boards.

Size Component Comment
Remaining area userfs The user file system contains user data and examples
768 Mbytes rootfs Linux root file system contains all user space binaries (executable, libraries, and so on), and kernel modules
16 Mbytes vendorfs This partition is preferred to the rootfs for third-party proprietary binaries, and ensures that they are not contaminated by any open source licence, such as GPL v3
64 Mbytes bootfs
or
boot (NAND)
The boot file system contains:
  • (option) the init RAM file system, which can be copied to the external RAM and used by Linux before mounting a fatter rootfs
  • Linux kernel device tree (can be in a Flattened Image Tree - FIT)
  • Linux kernel U-Boot image (can be in a Flattened Image Tree - FIT)
  • For all flashes except for NOR: the boot loader splash screen image, displayed by U-Boot
  • U-Boot distro config file extlinux.conf
2 * 256 Kbytes (*) env
or uboot_config / uboot_config_r (NAND)
This partition is used to store the U-Boot environment.
uboot_config_r is used for redundancy management with uboot_config, in NAND Flash.
4 Mbytes fip The TF-A firmware image package (FIP) is a binary file that encapsulates several binaries, and their certificates (optionally, for authentication), that will be loaded by TF-A]].

OpenSTLinux FIP contains:

  • the second stage boot loader (SSBL):
    • U-Boot binary
    • U-Boot device tree blob
  • the OP-TEE
256 Kbytes to 512 Kbytes (*) fsbl The first stage boot loader is Arm Trusted Firmware (TF-A). At least two copies are embedded.

Note: the FSBL payload is limited to 128 Kbytes on STM32MP13 and 247 Kbytes on STM32MP15.

(*): The partition size depends on the Flash technology, to be aligned to the block erase size of the Flash memory present on the board: NOR (256 Kbytes) / NAND (512 Kbytes).

Info white.png Information
Some boards can be equipped with multiple Flash devices, like the STM32MP15 EVAL board, where all of the Flash devices can be programmed with STM32CubeProgrammer. However, caution must be taken for the serial NOR/NAND and SLC NAND because a static bootable MTD partitioning is defined in U-Boot default config (see MTD configuration for details), with the consequence that up to 6 Mbytes of space is lost at the beginning of each such device, even those which are not bootable.

3. SD card memory mapping[edit source]

The SD card has to be partitioned with GPT format in order to be recognized by the STM32MP1. The easiest way to achieve this is to use STM32CubeProgrammer.
The ROM code looks for the GPT entries whose name begins with "fsbl": fsbl1 and fsbl2 for example.
Note: The SD card can be unplugged from the board and inserted into a Linux host computer for direct partitioning with Linux utilities and access to the bootfs, rootfs and userfs partitions. The file system is Linux EXT4.

SD card mapping.png


4. eMMC memory mapping[edit source]

The eMMC embeds four physical partitions:

  • Boot area partition 1: one copy of the FSBL
  • Boot area partition 2: one copy of the FSBL
  • User data area: formatted with GPT partitioning and used to store all remaining partitions
  • Replay Protected Memory Block (RPMB): not shown in the figure below, since not involved in the current boot chain.

STM32CubeProgrammer has to be used to prepare the eMMC with the layout shown below, and to populate each partition.

Info white.png Information
The boot area partition used by the eMMC boot sequence is selected via the EXT_CSD[179] register in the eMMC. The STM32CubeProgrammer execution is concluded with the selection of the last written partition from the flashlayout file, typically partition 2. The other copy is never used as long as the user does not explicitly change the eMMC EXT_CSD[179] register to select it.
EMMC mapping.png

5. NOR memory mapping[edit source]

As NOR Flash memory is expensive, its size is usually limited to the minimum needed to store only the bootloaders. The system files (bootfs, rootfs and userfs) are usually stored in another Flash memory, such as the SD card in OpenSTLinux distribution.
STM32CubeProgrammer must be used to prepare the NOR Flash and the SD card with the layout shown below, and to populate each partition.

It is possible to use an eMMC card or NAND as second-level Flash memory, rather than an SD card. This requires the following aspects to be changed:

  • The Flash memory layout, using STM32CubeProgrammer in order to write the rootfs and userfs to the targeted Flash memory
  • The Linux kernel parameters, using U-Boot, in order to indicate where the rootfs and userfs have to be mounted.
NOR mapping.png

6. NAND memory mapping[edit source]

STM32CubeProgrammer has to be used to prepare the NAND Flash memory with the layout shown below, and to populate each partition.

NAND mapping.png
Warning white.png Warning
In the RAW/MTD area, the number of copies to embed and the number of blocks to reserve at the end of each partition, for future bad blocks replacement, are a critical part of NAND based product dimensioning !

The strategy has to take into account many parameters such as:

  • the binaries sizes,
  • the read accesses to those partitions during product life, that may generate read disturb effect,
  • the capability of the product to refresh the partitions content when erroneous bits are detected,
  • the number of software updates estimated on this partition,
  • the selected NAND flash characteristics

ST set foundations in the STM32MP1 device in order to allow the integration of NAND flash memories but the product definition remains the customer responsibility. Please, contact your memory provider for further advice.