This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This page is a candidate for renaming (move). The requested new name is: How to configure wireless gateway . The supplied reason is: configure of configuration... . -- Registered User (-) 14:55, 16 May 2022 (CEST). Wiki maintainers: remember to update the pages that link this page before renaming (moving) it. |
1. How to configure a wireless gateway[edit source]
A wireless gateway routes packets from a wireless LAN to wired network (Ethernet)
For this example of configuration, the setup is :
- wlan0: wireless interface connected to SSID_NETWORK with DHCP
- eth0: ethernet interface with static IP which also have a DHCPserver on it
- forward of packet are activated between the two network interfaces.
1.1. Configure wireless interface[edit source]
cat /lib/systemd/network/wlan0.network
[Match]
Name=wlan0
[Network]
DHCP=ipv4
IPForward=ipv4
- IPForward
- permit to forward all network packet from wireless network to other network.
Configure wireless interface for SSID_NETWORK network:
mkdir -p /etc/wpa_supplicant/ echo "ctrl_interface=/var/run/wpa_supplicant" > /etc/wpa_supplicant/wpa_supplicant-wlan0.conf echo "eapol_version=1" >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf echo "ap_scan=1" >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf echo "fast_reauth=1" >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf echo "" >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf wpa_passphrase SSID_NETWORK PASSWORD_NETWORK >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf or wpa_passphrase SSID_NETWORK >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf
Where SSID_NETWORK PASSWORD_NETWORK correspond to the SSID and password of wireless network.
Enable the wireless configuration (to be take into account after reboot):
systemctl enable wpa_supplicant@wlan0.service systemctl restart systemd-networkd.service systemctl restart wpa_supplicant@wlan0.service