This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This article gives information about the OTP framework in OP-TEE and the associated interfaces.
1. Framework purpose[edit source]
Coming soon |
2. System overview[edit source]
Coming soon |
2.1. Component description[edit source]
Coming soon |
2.2. API description[edit source]
The OTP interface is provided by the 2 trusted applications (TA) in OP-TEE, accessible from the normal world with the GlobalPlatform API:
- BSEC PTA: used to export OTP to other TA or to normal world (individual access)
- NVMEM TA: used to export OTP to STM32cubeProgrammer (global access)
3. References[edit source]
Please refer to the following links for additional information: