This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Article purpose[edit source]
The purpose of this article is to explain how to configure the SAES internal peripheral using the device tree mechanism.
2. DT bindings documentation[edit source]
The following binding-related documentation explains how to write device tree files for SAES:
- OP-TEE STM32 SAES device tree bindings: documentation/devicetree/bindings/crypto/st,stm32-saes.yaml[1].
3. DT configuration[edit source]
This hardware description is a combination of STM32 microprocessor and board device tree files. See Device tree for explanations on device tree file split.
3.1. DT configuration (STM32 level)[edit source]
The SAES node is located in the STM32 MPU device tree.
3.2. DT configuration (board level)[edit source]
Board level device tree is used to enable the SAES.
4. References[edit source]
Please refer to the following links for additional information: