This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.![]() |
This page is a candidate for renaming (move). The requested new name is: STM32 MPU ROM trace analyzer . The supplied reason is: extended to MP13 . -- Registered User (-) 11:34, 19 January 2022 (CET). Wiki maintainers: remember to update the pages that link this page before renaming (moving) it. |
1. ROM trace analysis procedure[edit source]
When the device is in OPEN state, it is possible to access to the trace buffer located in a non-secure area of an embedded SRAM, and analyze ROM code execution traces.
To analyze ROM code traces:
- copy the rom_trace_analyzer_py script from chapter #Scripts to analyze traces and paste it into a script file, in this example rom_trace_analyzer.py
- connect the debugger and use it to download trace buffer address range in binary format into a file (for example traces.bin). See chapter #Procedure to dump traces
- launch the following command:
python3 rom_trace_analyzer.py traces.bin
2. Procedure to dump traces[edit source]
2.1. On STM32MP13x lines
[edit source]
- Traces are stored in SRAM1 at address ranges [0x30001638-0x30002638]
openocd -f board/stm32mp13x_dk2.cfg -c 'init;cortex_a smp off;halt;dump_image traces.bin 0x30001638 4096;resume;shutdown'
2.2. On STM32MP15x lines
[edit source]
- Traces are stored in SYSRAM at address ranges [0x2ffc1c00-0x2ffC2400]
- The command below gives an example of how to this with "openocd" tool on a DK2 board.
openocd -f board/stm32mp15x_dk2.cfg -c 'init;cortex_a smp off;halt;dump_image traces.bin 0x2ffc1c00 2048;resume;shutdown'
3. Scripts to analyze traces[edit source]
3.1. On STM32MP13x lines
[edit source]
#
# rom_trace_analyzer_py : script to analyze STM32MP13 ROM code traces
#
import os
import sys
import struct
import argparse
levels = (
'INFO',
'WARN',
'ERR ',
'DEBUG',
)
def level2str(level):
try:
return levels[level]
except IndexError:
return "UNKNOWN"
tags = {
0x90000001 : "NAND_DetectionFailed",
0x90000002 : "NAND_InitFailed",
0x90000003 : "NAND_NotInitialized",
0x90000004 : "NAND_NotOnfiOrNotDetected",
0x90000005 : "NAND_TransferFailed",
0x90000006 : "NAND_ImageTooBig",
0x90000007 : "NAND_OnlyBadBlocks",
0x90000008 : "NAND_UncorrectableEccErr",
0x90000009 : "NAND_NotGPTFound",
0x9000000A : "NAND_TryingSECBL1",
0x9000000B : "NAND_TryingSECBL2",
0x9000000C : "NAND_SecblFirstValidBlock",
0x9000000E : "NAND_EccErrorsDetected",
0x9000000F : "NAND_EccErrorCorrected",
0x90000010 : "NAND_EccErrorNotInDataArea",
0x90000011 : "NAND_SecblsFoundInGPT",
0x90000012 : "NAND_ReadColAddr",
0x90000013 : "NAND_ResetFailed",
0x90000014 : "NAND_NoOnfiParameterPage",
0x90000015 : "NAND_GetParamFromOtp",
0x90000016 : "NAND_EccBitsNbForcedByOtp",
0x90000017 : "NAND_NoValidBlockFound",
0x90000018 : "NAND_GptFound",
0x90000019 : "NAND_DirectFsblFound",
0x9000001A : "NAND_TryingDirectFSBL",
0x9000001B : "NAND_WrongFsblOffsetsInGPT",
0x9000001C : "NAND_EndOfNandReached",
0x90000101 : "NANDCORE_DetectionFailed",
0x90000102 : "NANDCORE_InitFailed",
0x90000103 : "NANDCORE_NotInitialized",
0x90000104 : "NANDCORE_NotOnfiOrNotDetected",
0x90000105 : "NANDCORE_TransferFailed",
0x90000106 : "NANDCORE_ImageTooBig",
0x90000107 : "NANDCORE_OnlyBadBlocks",
0x90000108 : "NANDCORE_UncorrectableEccErr",
0x90000109 : "NANDCORE_NotGPTFound",
0x9000010A : "NANDCORE_TryingSECBL1",
0x9000010B : "NANDCORE_TryingSECBL2",
0x9000010E : "NANDCORE_EccErrorsDetected",
0x9000010F : "NANDCORE_EccErrorCorrected",
0x90000110 : "NANDCORE_EccErrorNotInDataArea",
0x9000010C : "NANDCORE_SecblFirstValidBlock",
0x90000111 : "NANDCORE_SecblsFoundInGPT",
0x90000112 : "NANDCORE_ReadColAddr",
0x90000113 : "NANDCORE_ResetFailed",
0x90000114 : "NANDCORE_NoOnfiParameterPage",
0x90000115 : "NANDCORE_GetParamFromOtp",
0x90000116 : "NANDCORE_EccBitsNbForcedByOtp",
0x90000117 : "NANDCORE_NoValidBlockFound",
0x90000118 : "NANDCORE_GptFound",
0x90000119 : "NANDCORE_DirectFsblFound",
0x9000011A : "NANDCORE_TryingDirectFSBL",
0x9000011B : "NANDCORE_WrongFsblOffsetsInGPT",
0x9000011C : "NANDCORE_EndOfNandReached",
0x9000020E : "FMC_NAND_LL_EccErrorsDetected",
0x9000020F : "FMC_NAND_LL_EccErrorCorrected",
0x90000210 : "FMC_NAND_LL_EccErrorNotInDataArea",
0x90000251 : "QSPI_NAND_LL_NoEccErrorOrCorrected",
0x90000252 : "QSPI_NAND_LL_UncorrectableEccErr",
0x40000001 : "MMC_AcknowledgeErr",
0x40000002 : "MMC_AcknowledgeTimeout",
0x40000003 : "MMC_CardNotDetected",
0x40000004 : "MMC_DataCrcErr",
0x40000005 : "MMC_DataTimeout",
0x40000007 : "MMC_DmaTransferErr",
0x40000008 : "MMC_CmdTimeoutErr",
0x40000009 : "MMC_CmdCrcErr",
0x4000000A : "MMC_AddAlignErr",
0x4000000B : "MMC_NotEnoughBootDataRxErr",
0x4000000C : "MMC_ImageCopiedIsNotComplete",
0x4000000D : "MMC_ImageCopiedHeaderSizeZero",
0x4000000E : "MMC_AttemptBootDespiteErrors",
0x4000000F : "MMC_GotDataEndFlagWithNoErrors",
0x40000010 : "MMC_NbBytesCopiedInRam",
0x40000011 : "MMC_ImageCopiedHeaderNotFound",
0x40000012 : "MMC_VDDSD1RDYNotAsserted",
0x40000013 : "MMC_VDDSD2RDYNotAsserted",
0xCC000001 : "HASHDRV_Timeout",
0xCC000002 : "HASHDRV_BadState",
0xCC000003 : "HASHDRV_AccumulateSizeNotMultOf4",
0xCC000040 : "HASHDRV_TestPass",
0xCC000041 : "HASHDRV_TestAccumulateError",
0xCC000042 : "HASHDRV_TestComputeError",
0xCC000043 : "HASHDRV_TestFinishError",
0xCC000044 : "HASHDRV_TestCompareError",
0x80000001 : "QSPI_TryingSECBL1",
0x80000002 : "QSPI_TryingSECBL2",
0x80000003 : "QSPI_TryingSingleMode",
0x80000004 : "QSPI_TryingDualMode",
0x80000005 : "QSPI_FoundGpt",
0x80000006 : "QSPI_FoundMagicAtDefaultLocation",
0x80000007 : "QSPI_UseOffsets",
0x80000008 : "QSPI_WrongImageLen",
0x80000009 : "QSPI_Timeout",
0x0000000A : "BOOTCORE_HwResetPOR",
0x0000000B : "BOOTCORE_HwResetBOR",
0x0000000C : "BOOTCORE_HwResetPadNrst",
0x0000000D : "BOOTCORE_HwResetHcssRst",
0x0000000E : "BOOTCORE_HwResetVCore",
0x0000000F : "BOOTCORE_HwResetMpSysRst",
0x00000010 : "BOOTCORE_HwResetIwdg1",
0x00000011 : "BOOTCORE_HwResetIwdg2",
0x00000012 : "BOOTCORE_HwResetStdby",
0x00000013 : "BOOTCORE_HwResetMpup0Rst",
0x0000001B : "BOOTCORE_LogicalResetRmaReq",
0x0000001C : "BOOTCORE_LogicalResetLocalMpuCore0Reset",
0x0000001D : "BOOTCORE_LogicalResetStdbyExit",
0x0000001E : "BOOTCORE_LogicalResetSystem",
0x00000025 : "BOOTCORE_ChipModeSecOpen",
0x00000026 : "BOOTCORE_ChipModeSecOpenEngiBoot",
0x00000027 : "BOOTCORE_ChipModeSecClosed",
0x00000028 : "BOOTCORE_ChipModeSecClosedRmaOngoing",
0x0000002F : "BOOTCORE_OtpModeOtpSecured",
0x00000035 : "BOOTCORE_BootActionLocalMpuCore0ResetProcess",
0x00000038 : "BOOTCORE_BootActionRmaReqProcess",
0x00000039 : "BOOTCORE_BootActionRmaProcess",
0x0000003A : "BOOTCORE_BootActionSecureBootProcess",
0x0000003B : "BOOTCORE_BootActionWakeupStdby",
0x0000003D : "BOOTCORE_BootActionEngiBoot",
0x00000043 : "BOOTCORE_DebugCfgExitValue",
0x00000044 : "BOOTCORE_BsecJtagInValue",
0x00000045 : "BOOTCORE_BootCfgOtpWordValue",
0x00000046 : "BOOTCORE_BootCfgAfmuxOtpWord1Value",
0x00000047 : "BOOTCORE_BootCfgAfmuxOtpWord2Value",
0x00000048 : "BOOTCORE_BootCfgAfmuxOtpWord3Value",
0x00000049 : "BOOTCORE_BootCfgHseValue",
0x00000051 : "BOOTCORE_NoUsbDpPullupOtpBitValue",
0x00000052 : "BOOTCORE_NoCpuPllOtpBitValue",
0x00000057 : "BOOTCORE_BootCfgFsblDecryptPrio",
0x00000061 : "BOOTCORE_ReOpenDebugValue",
0x00000062 : "BOOTCORE_ReOpenSecNSecDebugValue",
0x00000063 : "BOOTCORE_ReOpenSecOnlyDebugValue",
0x00000064 : "BOOTCORE_ReOpenDbgSwEnableAndHdp",
0x00000065 : "BOOTCORE_DebugCloseAllButDbgenAndDeviceen",
0x0000006E : "BOOTCORE_RmaRequestValue",
0x0000006F : "BOOTCORE_RmaStatusValue",
0x00000074 : "BOOTCORE_NoDataCacheBitValue",
0x00000075 : "BOOTCORE_WakeupFromCSTANDBY",
0x00000076 : "BOOTCORE_WakeupFromSTANDBY",
0x00000079 : "BOOTCORE_WkUpActiveFlags",
0x00000091 : "BOOTCORE_MpuCpuPowerStateHasBeenInCStandby",
0x00000092 : "BOOTCORE_SystemPowerStateHasBeenInStandby",
0x00000093 : "BOOTCORE_BootModeNOBOOTENGIBOOT",
0x00000094 : "BOOTCORE_BootModeNOBOOTNOTENGIBOOTREQBYBOOTPINS",
0x00000095 : "BOOTCORE_BootModeNOBOOT",
0x00000096 : "BOOTCORE_BootModeSECUREBOOT",
0x00000097 : "BOOTCORE_EndBootROMGPIONotification",
0x00000098 : "BOOTCORE_NOBOOTLoop",
0x000000BF : "BOOTCORE_BootTimerSrcSoftCnt",
0x000000C0 : "BOOTCORE_BootTimerSrcGenTimer",
0x000000CF : "BOOTCORE_OtpBootSrcDisableMaskVal",
0x000000D0 : "BOOTCORE_OtpBootUartInstanceDisableMaskVal",
0x000000D1 : "BOOTCORE_EnabledSrcMaskVal",
0x000000E8 : "BOOTCORE_SafMemPwrUp",
0x000000E9 : "BOOTCORE_SafMemPwrDown",
0x000000EC : "BOOTCORE_EndBootGPIOEngiTesterStarted",
0x000000ED : "BOOTCORE_BootFAILED",
0x00000100 : "BOOTCORE_ARM_EXCEPTION_UNDEF",
0x00000101 : "BOOTCORE_ARM_EXCEPTION_PREFETCH_ABORT",
0x00000102 : "BOOTCORE_ARM_EXCEPTION_DATA_ABORT",
0x00000103 : "BOOTCORE_ARM_EXCEPTION_HYP",
0x00000104 : "BOOTCORE_ARM_EXCEPTION_IRQ",
0x00000105 : "BOOTCORE_ARM_EXCEPTION_FIQ",
0x00000106 : "BOOTCORE_ARM_EXCEPTION_SVC",
0x00000107 : "BOOTCORE_ARM_EXCEPTION_SMC_FROM_SECURE_WORLD_ERROR",
0x00000120 : "BOOTCORE_UartTraceEntryOnHwInstance",
0x00000130 : "BOOTCORE_Pll12StartBegin",
0x00000131 : "BOOTCORE_Pll12StartEnd",
0x00000132 : "BOOTCORE_Pll12StartDisabledByOtpBit",
0x00000133 : "BOOTCORE_Pll12StartNotDisabledByOtpBit",
0x00000134 : "BOOTCORE_Pll1Started",
0x00000135 : "BOOTCORE_Pll1Locked",
0x00000136 : "BOOTCORE_Pll1LockTimeout",
0x00000137 : "BOOTCORE_CkMpuSsSwitchedOnPll1",
0x00000138 : "BOOTCORE_Pll2Started",
0x00000139 : "BOOTCORE_Pll2Locked",
0x0000013A : "BOOTCORE_Pll2LockTimeout",
0x0000013B : "BOOTCORE_CkAxiSsSwitchedOnPll2",
0x0000013C : "BOOTCORE_Pll12StartReqStatusPllNotStarted",
0x0000013D : "BOOTCORE_Pll12StartReqStatusPllStarted",
0x0000013E : "BOOTCORE_Pll12StartDisabledByCompilationDirective",
0x00000140 : "BOOTCORE_BootSrcPeriphLoadLoopDisabled",
0x0000014E : "BOOTCORE_Pll4Started",
0x0000014F : "BOOTCORE_Pll4Locked",
0x00000150 : "BOOTCORE_Pll4LockTimeout",
0x00000151 : "BOOTCORE_HseNotReady",
0x00000152 : "BOOTCORE_StartupWaitTime",
0x00000153 : "BOOTCORE_PllUsbLocked",
0x00000154 : "BOOTCORE_PllUsbLockTimeout",
0x00000155 : "BOOTCORE_BootRomVer",
0x00000156 : "BOOTCORE_BootRomChipVer",
0x00000157 : "BOOTCORE_BootRomCutVer",
0x00000158 : "BOOTCORE_BootRomForRtlVer",
0x00000159 : "BOOTCORE_BootRomTargetPlatform",
0x0000015A : "BOOTCORE_BootRomMaskVer",
0x0000015D : "BOOTCORE_McuSecPerimeterRccTzenValue",
0x00000160 : "BOOTCORE_BootModeNOBOOTWithSignalingFromNsec",
0x00000161 : "BOOTCORE_NoBootTogglePa13Nsec",
0x000001C0 : "BOOTCORE_OtpEcdsaKeyCounterMonotonicVal",
0x000001C1 : "BOOTCORE_EcdsaKeyCounterVal",
0x000001C2 : "BOOTCORE_EcdsaKeyCounterNewProgVal",
0x000001D0 : "BOOTCORE_ImageVersionCounterNewProgVal",
0x000001D1 : "BOOTCORE_ImageVersionTooBig",
0x00000200 : "BOOTCORE_ConfigureSRAMsForBlockingFailure",
0x00000201 : "BOOTCORE_ConfigureSRAMsForDownload",
0x00000202 : "BOOTCORE_ConfigureSRAMsSecure",
0x00000203 : "BOOTCORE_ClearDownloadAreas",
0x00001000 : "BOOTCORE_BootPinsFirstSelNone",
0x00001001 : "BOOTCORE_BootPinsFirstSelSerial",
0x00001002 : "BOOTCORE_BootPinsFirstSelQspiNor",
0x00001003 : "BOOTCORE_BootPinsFirstSelSd",
0x00001004 : "BOOTCORE_BootPinsFirstSelEmmc",
0x00001005 : "BOOTCORE_BootPinsFirstSelFmc",
0x00001006 : "BOOTCORE_BootPinsFirstSelEngiBoot",
0x00001007 : "BOOTCORE_BootPinsFirstSelUnknown",
0x00001008 : "BOOTCORE_BootPinsOverridesOtp",
0x00001017 : "BOOTCORE_BootPinsFirstSelQspiNand",
0x00001009 : "BOOTCORE_OtpPrimarySrcForceFmc",
0x0000100A : "BOOTCORE_OtpPrimarySrcForceQspiNor",
0x0000100B : "BOOTCORE_OtpPrimarySrcForceEmmc",
0x0000100C : "BOOTCORE_OtpPrimarySrcForceSd",
0x0000100D : "BOOTCORE_OtpPrimarySrcForceQspiNand",
0x0000100E : "BOOTCORE_OtpPrimarySrcForceNothing",
0x0000100F : "BOOTCORE_OtpPrimarySrcForceUnknown",
0x00001010 : "BOOTCORE_OtpSecondarySrcForceFmc",
0x00001011 : "BOOTCORE_OtpSecondarySrcForceQspiNand",
0x00001012 : "BOOTCORE_OtpSecondarySrcForceQspiNor",
0x00001013 : "BOOTCORE_OtpSecondarySrcForceEmmc",
0x00001014 : "BOOTCORE_OtpSecondarySrcForceSd",
0x00001015 : "BOOTCORE_OtpSecondarySrcForceNothing",
0x00001016 : "BOOTCORE_OtpSecondarySrcForceUnknown",
0x00001020 : "BOOTCORE_TampForceSerialBoot",
0x00001030 : "BOOTCORE_BootPinsValueRead",
0x00002001 : "BOOTCORE_AuthWrongImageVersion",
0x00002002 : "BOOTCORE_AuthHashAreaStartAdd",
0x00002003 : "BOOTCORE_AuthImageLength",
0x00002004 : "BOOTCORE_AuthImageSizeToHash",
0x00002005 : "BOOTCORE_AuthImageEntryPoint",
0x00002006 : "BOOTCORE_AuthEccAlgoP256NIST",
0x00002007 : "BOOTCORE_AuthEccAlgoBrainPool256",
0x00002008 : "BOOTCORE_AuthEccAlgoUnknown",
0x00002009 : "BOOTCORE_AuthSignCheckValue",
0x0000200A : "BOOTCORE_AuthEntryPointOutOfRange",
0x0000200B : "BOOTCORE_AuthPubKHashFailStart",
0x0000200C : "BOOTCORE_AuthPubKHashFailFinish",
0x0000200D : "BOOTCORE_AuthPubKHashCompareError",
0x0000200E : "BOOTCORE_AuthPubKHashCompareOk",
0x0000200F : "BOOTCORE_AuthImageHashFailStart",
0x00002010 : "BOOTCORE_AuthImageHashFailFinish",
0x00002011 : "BOOTCORE_AuthImageSignatureFromHeaderECCDecryptStarted",
0x00002012 : "BOOTCORE_AuthImageSignatureKo",
0x00002013 : "BOOTCORE_AuthImageSignatureOk",
0x00002014 : "BOOTCORE_AuthDecisionIsJumpToImage",
0x00002015 : "BOOTCORE_AuthWrongImageHeaderVersion",
0x00002016 : "BOOTCORE_AuthWrongMagicNumber",
0x00002017 : "BOOTCORE_AuthImageLengthTooSmall",
0x00002018 : "BOOTCORE_AuthImageLengthTooBig",
0x00002019 : "BOOTCORE_AuthWrongImageChecksum",
0x0000201A : "BOOTCORE_AuthIsAuthenticationMandatory",
0x0000201B : "BOOTCORE_AuthIsAuthenticationSkipRequestedAndAllowed",
0x00002020 : "BOOTCORE_AuthImageEncrypted",
0x00002021 : "BOOTCORE_AuthImageNotEncrypted",
0x00002022 : "BOOTCORE_AuthImageDecryptionSucceed",
0x00002023 : "BOOTCORE_AuthImageDecryptionFailed",
0x00002024 : "BOOTCORE_AuthCryptoDisabledError",
0x00002025 : "BOOTCORE_AuthenticationExtensionHeaderMissing",
0x00002026 : "BOOTCORE_AuthMemoryVerifError",
0x00002040 : "BOOTCORE_AuthAuthenticationHeaderNotFound",
0x00002041 : "BOOTCORE_AuthPubKHashTableNotEqualToRef",
0x00002042 : "BOOTCORE_AuthPubKHashTableCheckSpecialSspStage3",
0x00002043 : "BOOTCORE_AuthInvalidKeyIndex",
0x00002044 : "BOOTCORE_AuthPublicKeyIsRevoked",
0x00002045 : "BOOTCORE_AuthPublicKeyNotRevoked",
0x00002046 : "BOOTCORE_AuthPublicKeyHashVerificationError",
0x00002047 : "BOOTCORE_AuthPubKeyVerifFailed",
0x00002048 : "BOOTCORE_AuthPubKeyVerifOk",
0x00002060 : "BOOTCORE_AuthFuseEcdsaKeyCounterRequired",
0x00002061 : "BOOTCORE_AuthFuseEcdsaKeyCounterNotRequired",
0x00002062 : "BOOTCORE_VerifyErrorWhileProgrammingEcdsaKeyCounter",
0x00002063 : "BOOTCORE_AuthNewEcdsaKeyCounterProgSuccess",
0x00002064 : "BOOTCORE_AuthMaxEcdsaKeyCounterReachedRevokNotPossible",
0x00002080 : "BOOTCORE_DecryptOptionHeaderNotFound",
0x00002081 : "BOOTCORE_DecryptWrongKeySize",
0x00002082 : "BOOTCORE_DecryptDerivKeyCalcError",
0x00002083 : "BOOTCORE_DecryptImageDecryptError",
0x00002084 : "BOOTCORE_DecryptHashIntegrityError",
0x00002085 : "BOOTCORE_DecryptOtpSecretKeyReadError",
0x00002086 : "BOOTCORE_DecryptUsingCrypDriver",
0x00002087 : "BOOTCORE_DecryptUsingSaesDriver",
0x00002088 : "BOOTCORE_DecryptOtpAesDriverError",
0x00002089 : "BOOTCORE_DerivKey128UsingSaesDriver",
0x0000208A : "BOOTCORE_DerivKey256UsingSaesDriver",
0x0000208B : "BOOTCORE_DerivKey128UsingCrypDriver",
0x0000208C : "BOOTCORE_DerivKey256UsingCrypDriver",
0x00002400 : "BOOTCORE_HseFrequencyDetected",
0x00002401 : "BOOTCORE_HseDigBypassDetected",
0x00002402 : "BOOTCORE_HseAnalogBypassDetected",
0x00002403 : "BOOTCORE_HseNoBypass",
0x00002404 : "BOOTCORE_HseFreqDetectDisabled",
0x00002405 : "BOOTCORE_HseBypassDetectDisabled",
0x00002406 : "BOOTCORE_eMmcUseSingle128KBytesBootPartition",
0x00002410 : "BOOTCORE_WkAroundEXTIResetValues",
0x00002503 : "BOOTCORE_FingerPrintOverflow",
0x00002504 : "BOOTCORE_FingerPrintValue",
0x00002505 : "BOOTCORE_FingerPrintCoef",
0x50000000 : "USB_Init",
0x50000001 : "USB_Loop",
0x50000002 : "USB_Selection",
0x50000003 : "USB_CallingAuthAndGo",
0x50000004 : "USB_DFU_DownloadComplete",
0x50000005 : "USB_DFU_GetStatus",
0x50000006 : "USB_DFU_GetStatus_GoTo_Idle",
0x50000007 : "USB_DFU_END_OF_DNLOAD",
0x50000008 : "USB_DFU_DNLOAD",
0x50000009 : "USB_DFU_UPLOAD",
0x5000000A : "USB_DFU_GETSTATUS",
0x5000000B : "USB_DFU_CLRSTATUS",
0x5000000C : "USB_DFU_GETSTATE",
0x5000000D : "USB_DFU_ABORT",
0x5000000E : "USB_DFU_DETACH",
0x5000000F : "USB_DFU_LEAVE",
0x50000010 : "USB_DFU_DataOut",
0x50000011 : "USB_DFU_GetStatusMedia",
0x50000012 : "USB_DFU_SRAMWrite",
0x50000013 : "USB_DFU_SRAMWrite_CRC",
0x50000014 : "USB_DFU_SRAMWrite_imgL",
0x50000015 : "USB_DFU_Init",
0x50000016 : "USB_DFU_SET_INTERFACE",
0x50000017 : "USB_DFU_SET_INTERFACE_ERR",
0x50000018 : "USB_DFU_Get_INTERFACE",
0x50000019 : "USB_DFU_LEAVE_EP0_TxReady",
0x50000020 : "USB_ClockTree_Failed",
0x50000021 : "USB_WrongDataTransfer",
0x50000022 : "USB_DataTransfered",
0x50000030 : "USB_DFU_DetachComplete",
0x60000001 : "UART_Selection",
0x60000002 : "UART_PeripheralSerialBootLoopStart",
0x60000003 : "UART_PacketNumber",
0x60000004 : "UART_PacketSize",
0x60000005 : "UART_PacketXor",
0x60000006 : "UART_ImageLength",
0x60000007 : "UART_Cursor",
0x60000008 : "UART_NACK",
0x60000009 : "UART_Abort",
0x6000000A : "UART_ActivityDetected",
0x6000000B : "UART_ActivityDetecting",
0x6000000C : "UART_ReceivedByte",
0x6000000D : "UART_DownloadFinished",
0x6000000E : "UART_Start",
0x30000001 : "SD_InitFailed",
0x30000002 : "SD_TransferFailed",
0x30000003 : "SD_CardDetected",
0x30000004 : "SD_NoCardResponse",
0x30000005 : "SD_TrySecBL1",
0x30000006 : "SD_FailedSecBL1TrySecBL2",
0x30000007 : "SD_InitDetailedErrorDesc",
0x30000008 : "SD_ImageTooBig",
0x30000009 : "SD_ImageLengthZero",
0x3000000A : "SD_StdCapacityCardV11",
0x3000000B : "SD_StdCapacityCardV20",
0x3000000C : "SD_HighCapacityCardSDHCOrSDXC",
0x3000000D : "SD_UnknownCapacityCard",
0x3000000E : "SD_OverallRetryCnt",
0x3000000F : "SD_ImageHeaderNotFound",
0x30000010 : "SD_NotGPTFound",
0x30000011 : "SD_FsblsFound",
0x30000012 : "SD_GPTFound",
0x30000013 : "SD_NotFSBLFound",
0x30000014 : "SD_RamCopyAddr",
0x30000015 : "SD_BufLen",
0x30000016 : "SD_ReadAddrInCard",
0x30000017 : "SD_NbFullBlocks",
0x30000018 : "SD_BytesRemainingInLastBlock",
0x30000019 : "SD_InFullBlocksRead",
0x3000001A : "SD_InLastIncompleteBlockRead",
0x30000020 : "SD_VDDSD1RDYNotAsserted",
0x30000021 : "SD_VDDSD2RDYNotAsserted",
0xC4000002 : "DWNLDMGR_WrongMagicNumber",
0xC4000003 : "DWNLDMGR_ImageLengthTooSmall",
0xC4000004 : "DWNLDMGR_ImageLengthTooBig",
0xC4000005 : "DWNLDMGR_EntryPointOutOfRange",
0xC4000006 : "DWNLDMGR_WrongImageChecksum",
0xC4000007 : "DWNLDMGR_WrongHeaderVersion",
0xC4000008 : "DWNLDMGR_UnknownExtensionHeader",
0xC4000009 : "DWNLDMGR_FoundFsblDecryptionHeader",
0xC400000A : "DWNLDMGR_FoundPkhAuthenticationHeader",
0xC400000B : "DWNLDMGR_WrongExtensionHeaderLength",
0xC400000C : "DWNLDMGR_WrongCipherKeySize",
0xC400000D : "DWNLDMGR_ExtensionFlagsMismatch",
0xC400000E : "DWNLDMGR_WrongNumberOfPublicKeyHash",
0xC400000F : "DWNLDMGR_WrongPublicKeyIndex",
0xC4000010 : "DWNLDMGR_FoundPaddingHeader",
}
def tag2str(tag):
try:
return tags[tag]
except KeyError:
return None
class Trace(object):
def __init__(self, timestamp, level, tag, data ):
self.timestamp = timestamp
self.level = level
self.tag = tag
self.data = data
def dump(self):
level_str = level2str(self.level)
tag_str = tag2str(self.tag)
if tag_str:
print( "< @ %08d | [%s] - %s" % (self.timestamp, level_str, tag_str), end='' )
if len(self.data) > 0:
print (" (", end='')
for d in self.data[:-1]:
print (" 0x%08X," % (d), end='')
print (" 0x%08X )" % (self.data[-1]), end='')
print (" >")
class TraceAnalyzer(object):
START_WORD = 0xFFDDBB00
def __init__(self):
pass
def _next_word_(self):
word = self._file.read(4)
if len(word):
return struct.unpack('<L',word)[0]
else:
raise StopIteration('END OF FILE')
def _look_for_start_word_(self):
while True:
if self._next_word_() == self.START_WORD:
return True
def parse(self,file_):
self._file = file_
return iter(self)
def __iter__(self):
return self
def __next__(self):
self._look_for_start_word_()
size = self._next_word_()
timestamp = self._next_word_()
size -= 4
level = self._next_word_()
size -= 4
tag = self._next_word_()
size -= 4
data = []
while size > 0:
data.append(self._next_word_())
size -= 4
return Trace(timestamp, level, tag, data)
if __name__ == '__main__':
parser = argparse.ArgumentParser(description='STM32MPU15 Bootrom trace decoder')
parser.add_argument("trace_file",
action="store",
type=argparse.FileType('rb'),
help="Name of binary trace file",
metavar="FILE.BIN")
args = parser.parse_args()
traces_analyzer = TraceAnalyzer()
traces = traces_analyzer.parse(args.trace_file)
for trace in traces:
trace.dump()
3.2. On STM32MP15x lines
[edit source]
#
# rom_trace_analyzer_py : script to analyze STM32MP15 ROM code traces
#
import os
import sys
import struct
import argparse
levels = (
'INFO',
'WARN',
'ERR ',
'DEBUG',
)
def level2str(level):
try:
return levels[level]
except IndexError:
return "UNKNOWN"
tags = {
0x90000001 : "NAND_DetectionFailed",
0x90000002 : "NAND_InitFailed",
0x90000003 : "NAND_NotInitialized",
0x90000004 : "NAND_NotOnfiOrNotDetected",
0x90000005 : "NAND_TransferFailed",
0x90000006 : "NAND_ImageTooBig",
0x90000007 : "NAND_OnlyBadBlocks",
0x90000008 : "NAND_UncorrectableEccErr",
0x90000009 : "NAND_NotGPTFound",
0x9000000A : "NAND_TryingSECBL1",
0x9000000B : "NAND_TryingSECBL2",
0x9000000C : "NAND_SecblFirstValidBlock",
0x9000000E : "NAND_EccErrorsDetected",
0x9000000F : "NAND_EccErrorCorrected",
0x90000010 : "NAND_EccErrorNotInDataArea",
0x90000011 : "NAND_SecblsFoundInGPT",
0x90000012 : "NAND_ReadColAddr",
0x90000013 : "NAND_ResetFailed",
0x90000014 : "NAND_NoOnfiParameterPage",
0x90000015 : "NAND_GetParamFromOtp",
0x90000016 : "NAND_EccBitsNbForcedByOtp",
0x90000017 : "NAND_NoValidBlockFound",
0x90000018 : "NAND_GptFound",
0x90000019 : "NAND_DirectFsblFound",
0x9000001A : "NAND_TryingDirectFSBL",
0x9000001B : "NAND_WrongFsblOffsetsInGPT",
0x9000001C : "NAND_EndOfNandReached",
0x90000101 : "NANDCORE_DetectionFailed",
0x90000102 : "NANDCORE_InitFailed",
0x90000103 : "NANDCORE_NotInitialized",
0x90000104 : "NANDCORE_NotOnfiOrNotDetected",
0x90000105 : "NANDCORE_TransferFailed",
0x90000106 : "NANDCORE_ImageTooBig",
0x90000107 : "NANDCORE_OnlyBadBlocks",
0x90000108 : "NANDCORE_UncorrectableEccErr",
0x90000109 : "NANDCORE_NotGPTFound",
0x9000010A : "NANDCORE_TryingSECBL1",
0x9000010B : "NANDCORE_TryingSECBL2",
0x9000010E : "NANDCORE_EccErrorsDetected",
0x9000010F : "NANDCORE_EccErrorCorrected",
0x90000110 : "NANDCORE_EccErrorNotInDataArea",
0x9000010C : "NANDCORE_SecblFirstValidBlock",
0x90000111 : "NANDCORE_SecblsFoundInGPT",
0x90000112 : "NANDCORE_ReadColAddr",
0x90000113 : "NANDCORE_ResetFailed",
0x90000114 : "NANDCORE_NoOnfiParameterPage",
0x90000115 : "NANDCORE_GetParamFromOtp",
0x90000116 : "NANDCORE_EccBitsNbForcedByOtp",
0x90000117 : "NANDCORE_NoValidBlockFound",
0x90000118 : "NANDCORE_GptFound",
0x90000119 : "NANDCORE_DirectFsblFound",
0x9000011A : "NANDCORE_TryingDirectFSBL",
0x9000011B : "NANDCORE_WrongFsblOffsetsInGPT",
0x9000011C : "NANDCORE_EndOfNandReached",
0x9000020E : "FMC_NAND_LL_EccErrorsDetected",
0x9000020F : "FMC_NAND_LL_EccErrorCorrected",
0x90000210 : "FMC_NAND_LL_EccErrorNotInDataArea",
0x90000251 : "QSPI_NAND_LL_NoEccErrorNoEccErrorOrCorrected",
0x90000252 : "QSPI_NAND_LL_UncorrectableEccErr",
0x40000001 : "MMC_AcknowledgeErr",
0x40000002 : "MMC_AcknowledgeTimeout",
0x40000003 : "MMC_CardNotDetected",
0x40000004 : "MMC_DataCrcErr",
0x40000005 : "MMC_DataTimeout",
0x40000007 : "MMC_DmaTransferErr",
0x40000008 : "MMC_CmdTimeoutErr",
0x40000009 : "MMC_CmdCrcErr",
0x4000000A : "MMC_AddAlignErr",
0x4000000B : "MMC_NotEnoughBootDataRxErr",
0x4000000C : "MMC_ImageCopiedIsNotComplete",
0x4000000D : "MMC_ImageCopiedHeaderSizeZero",
0x4000000E : "MMC_AttemptBootDespiteErrors",
0x4000000F : "MMC_GotDataEndFlagWithNoErrors",
0x40000010 : "MMC_NbBytesCopiedInSysram",
0x40000011 : "MMC_ImageCopiedHeaderNotFound",
0x80000001 : "QSPI_TryingSECBL1",
0x80000002 : "QSPI_TryingSECBL2",
0x80000003 : "QSPI_TryingSingleMode",
0x80000004 : "QSPI_TryingDualMode",
0x80000005 : "QSPI_FoundGpt",
0x80000006 : "QSPI_FoundMagicAtDefaultLocation",
0x80000007 : "QSPI_UseOffsets",
0x80000008 : "QSPI_WrongImageLen",
0x80000009 : "QSPI_Timeout",
0x0000000A : "BOOTCORE_HwResetPOR",
0x0000000B : "BOOTCORE_HwResetBOR",
0x0000000C : "BOOTCORE_HwResetPadNrst",
0x0000000D : "BOOTCORE_HwResetHcssRst",
0x0000000E : "BOOTCORE_HwResetVCore",
0x0000000F : "BOOTCORE_HwResetMpSysRst",
0x00000010 : "BOOTCORE_HwResetMcSysRst",
0x00000011 : "BOOTCORE_HwResetIwdg1",
0x00000012 : "BOOTCORE_HwResetIwdg2",
0x00000013 : "BOOTCORE_HwResetWwdg1",
0x00000014 : "BOOTCORE_HwResetStdby",
0x00000015 : "BOOTCORE_HwResetCStdby",
0x00000016 : "BOOTCORE_HwResetMpu0Rst",
0x00000017 : "BOOTCORE_HwResetMpu1Rst",
0x00000018 : "BOOTCORE_HwResetInvalid",
0x0000001A : "BOOTCORE_LogicalResetLocalMpuCore0Reset",
0x0000001B : "BOOTCORE_LogicalResetRmaOrRmaRelockReq",
0x0000001C : "BOOTCORE_LogicalResetCStdbyExit",
0x0000001D : "BOOTCORE_LogicalResetStdbyExit",
0x0000001E : "BOOTCORE_LogicalResetSystem",
0x0000001F : "BOOTCORE_LogicalResetInvalid",
0x00000025 : "BOOTCORE_ChipModeSecOpen",
0x00000026 : "BOOTCORE_ChipModeSecOpenEngiBoot",
0x00000027 : "BOOTCORE_ChipModeSecFinalNormal",
0x00000028 : "BOOTCORE_ChipModeSecFinalRmaOngoing",
0x00000029 : "BOOTCORE_ChipModeSecFinalRmaRelocked",
0x0000002B : "BOOTCORE_ChipModeInvalid",
0x00000031 : "BOOTCORE_BootActionLocalMpuCore0ResetProcess",
0x00000037 : "BOOTCORE_BootActionRmaReqProcess",
0x00000038 : "BOOTCORE_BootActionRmaProcess",
0x00000039 : "BOOTCORE_BootActionRmaRelockReqProcess",
0x0000003A : "BOOTCORE_BootActionColdBootProcess",
0x0000003B : "BOOTCORE_BootActionWakeupCStdby",
0x0000003C : "BOOTCORE_BootActionWakeupStdby",
0x0000003D : "BOOTCORE_BootActionInvalid",
0x0000003E : "BOOTCORE_BootActionEngiBoot",
0x00000045 : "BOOTCORE_BootCfgOtpWordValue",
0x00000046 : "BOOTCORE_BootCfgAfmuxOtpWord1Value",
0x00000047 : "BOOTCORE_BootCfgAfmuxOtpWord2Value",
0x00000048 : "BOOTCORE_BootCfgAfmuxOtpWord3Value",
0x00000049 : "BOOTCORE_BootCfgHseValue",
0x00000051 : "BOOTCORE_NoUsbDpPullupOtpBitValue",
0x00000052 : "BOOTCORE_NoCpuPllOtpBitValue",
0x00000061 : "BOOTCORE_ReOpenDebugValue",
0x00000062 : "BOOTCORE_ReOpenSecNSecDebugValue",
0x00000063 : "BOOTCORE_ReOpenSecOnlyDebugValue",
0x00000064 : "BOOTCORE_ReOpenDbgSwEnableAndHdp",
0x00000065 : "BOOTCORE_DebugCloseAllButDbgenAndDeviceen",
0x00000066 : "BOOTCORE_RmaOtpWordValue",
0x00000068 : "BOOTCORE_RmaTrialOver",
0x00000069 : "BOOTCORE_RmaTrialFoundFreeFuseBit",
0x0000006A : "BOOTCORE_FusedNewRmaTrial",
0x0000006B : "BOOTCORE_RmaPasswdMatch",
0x0000006C : "BOOTCORE_RmaPasswdError",
0x0000006D : "BOOTCORE_RmaRequestValue",
0x0000006E : "BOOTCORE_RmaStatusValue",
0x0000006F : "BOOTCORE_RmaRelockTrialOver",
0x00000070 : "BOOTCORE_RmaRelockTrialCurrentNb",
0x00000071 : "BOOTCORE_FusedNewRmaRelockTrial",
0x00000072 : "BOOTCORE_RmaRelockPasswdMatch",
0x00000073 : "BOOTCORE_RmaRelockPasswdError",
0x00000074 : "BOOTCORE_NoDataCacheBitValue",
0x00000075 : "BOOTCORE_WakeupFromCSTANDBY",
0x00000076 : "BOOTCORE_WakeupFromSTANDBY",
0x00000077 : "BOOTCORE_WakeupFromSTANDBYMpuBenMcuBen",
0x00000078 : "BOOTCORE_WakeupFromSTANDBYMcuSecPerimeterRccTzenRccMckProt",
0x00000079 : "BOOTCORE_WkUpActiveFlags",
0x0000007A : "BOOTCORE_McuRestartOk",
0x0000007B : "BOOTCORE_McuRestartKoNoHashWhileMandatory",
0x0000007C : "BOOTCORE_McuRestartKoWrongHash",
0x0000007D : "BOOTCORE_McuMcicOutOfRangeHashReq",
0x0000007E : "BOOTCORE_McuMcicHashDrvCallStart",
0x0000007F : "BOOTCORE_McuRestartKoErrorWhileHashing",
0x00000080 : "BOOTCORE_McuMcicHashFailStart",
0x00000081 : "BOOTCORE_McuMcicHashFailFinish",
0x00000082 : "BOOTCORE_McuCodeHashVerifReq",
0x00000083 : "BOOTCORE_McuNoCodeHashVerifReq",
0x00000084 : "BOOTCORE_McuCodeHashVerifPass",
0x00000085 : "BOOTCORE_McuSecurityPerimeterVerifPass",
0x00000086 : "BOOTCORE_McuSecurityPerimeterVerifFailed",
0x00000087 : "BOOTCORE_McuSecurityPerimeterVerifNotChecked",
0x00000088 : "BOOTCORE_WakeupFromCSTANDBYWithMcuNotRunning",
0x00000089 : "BOOTCORE_WakeupFromCSTANDBYWithMcuRunning",
0x0000008A : "BOOTCORE_WakeupFromCSTANDBYWithMcuSev",
0x0000008B : "BOOTCORE_WakeupFromCSTANDBYWithWwdg1Evt",
0x00000091 : "BOOTCORE_MpuCpuPowerStateHasBeenInCStandby",
0x00000092 : "BOOTCORE_SystemPowerStateHasBeenInStandby",
0x00000093 : "BOOTCORE_BootModeNOBOOTENGIBOOT",
0x00000094 : "BOOTCORE_BootModeNOBOOTNOTENGIBOOTREQBYBOOTPINS",
0x00000095 : "BOOTCORE_BootModeNOBOOT",
0x00000096 : "BOOTCORE_BootModeNOBOOTWITHENGIACCESS",
0x00000097 : "BOOTCORE_BootModeNOBOOTCSTANDBY",
0x00000098 : "BOOTCORE_BootModeCOLDBOOT",
0x00000099 : "BOOTCORE_WakeupFromCSTANDBYMcuSysRstReqEvt",
0x000000BF : "BOOTCORE_BootTimerSrcSoftCnt",
0x000000C0 : "BOOTCORE_BootTimerSrcGenTimer",
0x000000CF : "BOOTCORE_OtpBootSrcDisableMaskVal",
0x000000D0 : "BOOTCORE_OtpBootUartInstanceDisableMaskVal",
0x000000D1 : "BOOTCORE_EnabledSrcMaskVal",
0x000000E0 : "BOOTCORE_CSISwitchON",
0x000000E8 : "BOOTCORE_SafMemPwrUp",
0x000000E9 : "BOOTCORE_SafMemPwrDown",
0x000000EA : "BOOTCORE_FreezeIWDG12Clocks",
0x000000EB : "BOOTCORE_UnFreezeIWDG12Clocks",
0x000000ED : "BOOTCORE_BootFAILED",
0x00000120 : "BOOTCORE_UartTraceEntryOnHwInstance",
0x00000132 : "BOOTCORE_Pll12StartDisabledByOtpBit",
0x00000133 : "BOOTCORE_Pll12StartNotDisabledByOtpBit",
0x00000134 : "BOOTCORE_Pll1Started",
0x00000135 : "BOOTCORE_Pll1Locked",
0x00000136 : "BOOTCORE_Pll1LockTimeout",
0x00000137 : "BOOTCORE_CkMpuSsSwitchedOnPll1",
0x00000138 : "BOOTCORE_Pll2Started",
0x00000139 : "BOOTCORE_Pll2Locked",
0x0000013A : "BOOTCORE_Pll2LockTimeout",
0x0000013B : "BOOTCORE_CkAxiSsSwitchedOnPll2",
0x0000013C : "BOOTCORE_Pll12StartReqStatusPllNotStarted",
0x0000013D : "BOOTCORE_Pll12StartReqStatusPllStarted",
0x00000140 : "BOOTCORE_BootSrcPeriphLoadLoopDisabled",
0x0000014E : "BOOTCORE_Pll4Started",
0x0000014F : "BOOTCORE_Pll4Locked",
0x00000150 : "BOOTCORE_Pll4LockTimeout",
0x00000151 : "BOOTCORE_HseNotReady",
0x00000152 : "BOOTCORE_StartupWaitTime",
0x00000153 : "BOOTCORE_PllUsbLocked",
0x00000154 : "BOOTCORE_PllUsbLockTimeout",
0x00000155 : "BOOTCORE_BootRomVer",
0x00000156 : "BOOTCORE_BootRomChipVer",
0x00000157 : "BOOTCORE_BootRomCutVer",
0x00000158 : "BOOTCORE_BootRomForRtlVer",
0x00000159 : "BOOTCORE_BootRomTargetPlatform",
0x0000015A : "BOOTCORE_BootRomMaskVer",
0x0000015D : "BOOTCORE_McuSecPerimeterRccTzenValue",
0x0000015E : "BOOTCORE_McuSecPerimeterMckprotValue",
0x0000015F : "BOOTCORE_McuSecPerimeterExtiTzenr1Value",
0x00000160 : "BOOTCORE_McuSecPerimeterExtiTzenr2Value",
0x00000161 : "BOOTCORE_McuSecPerimeterExtiTzenr3Value",
0x00000162 : "BOOTCORE_McuMcicReadInTampOffsetInBytesOfCodeToHashInRETRAM",
0x00000163 : "BOOTCORE_McuMcicReadInTampSizeInBytesToHash",
0x00000164 : "BOOTCORE_McuMcicReadInTampSignatureWord",
0x00000165 : "BOOTCORE_McuSecPerimeterReadWriteSecureOnlyLastBackupIdx",
0x00000166 : "BOOTCORE_McuSecPerimeterWriteSecureOnlyLastBackupIdx",
0x00000167 : "BOOTCORE_BootModeNOBOOTWithSignalingFromNsec",
0x00000168 : "BOOTCORE_NoBootTogglePa13Nsec",
0x00000169 : "BOOTCORE_McuSecPerimeterTampSmcrVal",
0x0000017D : "BOOTCORE_BootModeENGIBOOTSysRamAllNsecInTZMA1",
0x00001000 : "BOOTCORE_BootPinsFirstSelNone",
0x00001001 : "BOOTCORE_BootPinsFirstSelSerial",
0x00001002 : "BOOTCORE_BootPinsFirstSelQspiNor",
0x00001003 : "BOOTCORE_BootPinsFirstSelSd",
0x00001004 : "BOOTCORE_BootPinsFirstSelEmmc",
0x00001005 : "BOOTCORE_BootPinsFirstSelFmc",
0x00001006 : "BOOTCORE_BootPinsFirstSelEngiBoot",
0x00001007 : "BOOTCORE_BootPinsFirstSelUnknown",
0x00001008 : "BOOTCORE_BootPinsOverridesOtp",
0x00001017 : "BOOTCORE_BootPinsFirstSelQspiNand",
0x00001009 : "BOOTCORE_OtpPrimarySrcForceFmc",
0x0000100A : "BOOTCORE_OtpPrimarySrcForceQspiNor",
0x0000100B : "BOOTCORE_OtpPrimarySrcForceEmmc",
0x0000100C : "BOOTCORE_OtpPrimarySrcForceSd",
0x0000100D : "BOOTCORE_OtpPrimarySrcForceQspiNand",
0x0000100E : "BOOTCORE_OtpPrimarySrcForceNothing",
0x0000100F : "BOOTCORE_OtpPrimarySrcForceUnknown",
0x00001010 : "BOOTCORE_OtpSecondarySrcForceFmc",
0x00001011 : "BOOTCORE_OtpSecondarySrcForceQspiNand",
0x00001012 : "BOOTCORE_OtpSecondarySrcForceQspiNor",
0x00001013 : "BOOTCORE_OtpSecondarySrcForceEmmc",
0x00001014 : "BOOTCORE_OtpSecondarySrcForceSd",
0x00001015 : "BOOTCORE_OtpSecondarySrcForceNothing",
0x00001016 : "BOOTCORE_OtpSecondarySrcForceUnknown",
0x00001020 : "BOOTCORE_TampForceSerialBoot",
0x00002001 : "BOOTCORE_AuthWrongImageVersion",
0x00002002 : "BOOTCORE_AuthHashAreaStartAdd",
0x00002003 : "BOOTCORE_AuthImageLength",
0x00002004 : "BOOTCORE_AuthImageSizeToHash",
0x00002005 : "BOOTCORE_AuthImageEntryPoint",
0x00002006 : "BOOTCORE_AuthEccAlgoP256NIST",
0x00002007 : "BOOTCORE_AuthEccAlgoBrainPool256",
0x00002008 : "BOOTCORE_AuthEccAlgoUnknown",
0x00002009 : "BOOTCORE_AuthNoSigCheckValue",
0x0000200A : "BOOTCORE_AuthEntryPointOutOfRange",
0x0000200B : "BOOTCORE_AuthPubKHashFailStart",
0x0000200C : "BOOTCORE_AuthPubKHashFailFinish",
0x0000200D : "BOOTCORE_AuthPubKHashCompareError",
0x0000200E : "BOOTCORE_AuthPubKHashCompareOk",
0x0000200F : "BOOTCORE_AuthImageHashFailStart",
0x00002010 : "BOOTCORE_AuthImageHashFailFinish",
0x00002011 : "BOOTCORE_AuthImageSignatureFromHeaderECCDecryptStarted",
0x00002012 : "BOOTCORE_AuthImageSignatureKo",
0x00002013 : "BOOTCORE_AuthImageSignatureOk",
0x00002014 : "BOOTCORE_AuthDecisionIsJumpToImage",
0x00002015 : "BOOTCORE_AuthWrongImageHeaderVersion",
0x00002016 : "BOOTCORE_AuthWrongMagicNumber",
0x00002017 : "BOOTCORE_AuthImageLengthTooSmall",
0x00002018 : "BOOTCORE_AuthImageLengthTooBig",
0x00002019 : "BOOTCORE_AuthWrongImageChecksum",
0x0000201A : "BOOTCORE_AuthIsAuthenticationMandatory",
0x0000201B : "BOOTCORE_AuthIsAuthenticationSkipRequestedAndAllowed",
0x00002400 : "BOOTCORE_HseFrequencyDetected",
0x00002401 : "BOOTCORE_HseDigBypassDetected",
0x00002402 : "BOOTCORE_HseAnalogBypassDetected",
0x00002403 : "BOOTCORE_HseNoBypass",
0x00002404 : "BOOTCORE_HseFreqDetectDisabled",
0x00002405 : "BOOTCORE_HseBypassDetectDisabled",
0x00002406 : "BOOTCORE_eMmcUseSingle128KBytesBootPartition",
0x50000000 : "USB_Init",
0x50000001 : "USB_Loop",
0x50000002 : "USB_Selection",
0x50000003 : "USB_CallingAuthAndGo",
0x50000004 : "USB_DFU_OperationComplete",
0x50000005 : "USB_DFU_GetStatus",
0x50000006 : "USB_DFU_GetStatus_GoTo_Idle",
0x50000007 : "USB_DFU_END_OF_DNLOAD",
0x50000008 : "USB_DFU_DNLOAD",
0x50000009 : "USB_DFU_UPLOAD",
0x5000000A : "USB_DFU_GETSTATUS",
0x5000000B : "USB_DFU_CLRSTATUS",
0x5000000C : "USB_DFU_GETSTATE",
0x5000000D : "USB_DFU_ABORT",
0x5000000E : "USB_DFU_DETACH",
0x5000000F : "USB_DFU_LEAVE",
0x50000010 : "USB_DFU_DataOut",
0x50000011 : "USB_DFU_GetStatusMedia",
0x50000012 : "USB_DFU_SRAMWrite",
0x50000013 : "USB_DFU_SRAMWrite_CRC",
0x50000014 : "USB_DFU_SRAMWrite_imgL",
0x50000015 : "USB_DFU_Init",
0x50000016 : "USB_DFU_SET_INTERFACE",
0x50000017 : "USB_DFU_SET_INTERFACE_ERR",
0x50000018 : "USB_DFU_Get_INTERFACE",
0x50000019 : "USB_DFU_LEAVE_EP0_TxReady",
0x50000020 : "USB_ClockTree_Failed",
0x50000021 : "USB_WrongDataTransfer",
0x50000022 : "USB_DataTransfered",
0x60000001 : "UART_Selection",
0x60000002 : "UART_PeripheralSerialBootLoopStart",
0x60000003 : "UART_PacketNumber",
0x60000004 : "UART_PacketSize",
0x60000005 : "UART_PacketXor",
0x60000006 : "UART_ImageLength",
0x60000008 : "UART_NACK",
0x60000009 : "UART_ABORT",
0x6000000A : "UART_ActivityDetected",
0x6000000B : "UART_ActivityDetecting",
0x30000001 : "SD_InitFailed",
0x30000002 : "SD_TransferFailedDuringSecBlHeaderRead",
0x30000003 : "SD_TransferFailedDuringSecBlPayloadRead",
0x30000004 : "SD_CardDetected",
0x30000005 : "SD_NoCardResponse",
0x30000006 : "SD_TrySecBL1",
0x30000007 : "SD_FailedSecBL1TrySecBL2",
0x30000008 : "SD_InitDetailedErrorDesc",
0x30000009 : "SD_ImageTooBig",
0x3000000A : "SD_ImageLengthZero",
0x3000000B : "SD_StdCapacityCardV11",
0x3000000C : "SD_StdCapacityCardV20",
0x3000000D : "SD_HighCapacityCardSDHCOrSDXC",
0x3000000E : "SD_UnknownCapacityCard",
0x3000000F : "SD_OverallRetryCnt",
0x30000010 : "SD_ImageHeaderNotFound",
0x30000011 : "SD_NotGPTFound",
0x30000012 : "SD_FsblsFound",
0x30000013 : "SD_GPTFound",
0x30000014 : "SD_NotFSBLFound",
}
def tag2str(tag):
try:
return tags[tag]
except KeyError:
return None
class Trace(object):
def __init__(self, timestamp, level, tag, data ):
self.timestamp = timestamp
self.level = level
self.tag = tag
self.data = data
def dump(self):
level_str = level2str(self.level)
tag_str = tag2str(self.tag)
if tag_str:
print( "< @ %08d | [%s] - %s" % (self.timestamp, level_str, tag_str), end='' )
if len(self.data) > 0:
print (" (", end='')
for d in self.data[:-1]:
print (" 0x%08X," % (d), end='')
print (" 0x%08X )" % (self.data[-1]), end='')
print (" >")
class TraceAnalyzer(object):
START_WORD = 0xFFDDBB00
def __init__(self):
pass
def _next_word_(self):
word = self._file.read(4)
if len(word):
return struct.unpack('<L',word)[0]
else:
raise StopIteration('END OF FILE')
def _look_for_start_word_(self):
while True:
if self._next_word_() == self.START_WORD:
return True
def parse(self,file_):
self._file = file_
return iter(self)
def __iter__(self):
return self
def __next__(self):
self._look_for_start_word_()
size = self._next_word_()
timestamp = self._next_word_()
size -= 4
level = self._next_word_()
size -= 4
tag = self._next_word_()
size -= 4
data = []
while size > 0:
data.append(self._next_word_())
size -= 4
return Trace(timestamp, level, tag, data)
if __name__ == '__main__':
parser = argparse.ArgumentParser(description='STM32MPU15 Bootrom trace decoder')
parser.add_argument("trace_file",
action="store",
type=argparse.FileType('rb'),
help="Name of binary trace file",
metavar="FILE.BIN")
args = parser.parse_args()
traces_analyzer = TraceAnalyzer()
traces = traces_analyzer.parse(args.trace_file)
for trace in traces:
trace.dump()