This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.
The OpenSTLinux distribution does not provide flashlayout files to use UART as serial boot device.
Refer to Using_STM32Programmer_over_UART article to know how to modify a flashlayout file to use UART as serial boot device.
You can use the modified flashlayout as described in STM32CubeProgrammer#How to flash with STM32CubeProgrammer article.
For example, if the provided file FlashLayout_sdcard_stm32mp157c-dk2-optee.tsv can be used on USB with the command:
STM32_Programmer_CLI -c port=usb1 -w FlashLayout_sdcard_stm32mp157c-dk2-optee.tsv
then you can replace tf-a-stm32mp157f-dk2-usb.stm32 by tf-a-stm32mp157f-dk2-uart.stm32 in this tsv file and the resulting file FlashLayout_sdcard_stm32mp157c-dk2-optee_uart.tsv can be used on UART port /dev/ttyACM1 with the command:
STM32_Programmer_CLI -c port=/dev/ttyACM1 -w FlashLayout_sdcard_stm32mp157c-dk2-optee_uart.tsv