DDRCTRL and DDRPHYC internal peripherals

Revision as of 15:36, 26 October 2021 by Registered User (→‎Overview)

1. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the DDRCTRL and DDRPHYC peripherals and their main features
  • indicate the level of security supported by those hardware blocks
  • explain how they can be allocated to the three runtime contexts and linked to the corresponding software components
  • explain, when necessary, how to configure the DDRCTRL and DDRPHYC peripherals.

2. Peripheral overview[edit source]

DDRCTRL and DDRPHYC peripherals are used to configure the physical interface to the external DDR memory.

2.1. Features[edit source]

Refer to STM32MP13 reference manuals or STM32MP15 reference manuals for the complete features list, and to the software components, introduced below, to see which features are actually implemented.

2.2. Security support[edit source]

DDRCTRL and DDRPHYC are secure aware (under ETZPC control).

Access to the DDR memory can be filtered via the TZC controller: for instance, on STM32MP15 reference manuals, it is possible to forbid access from the Cortex®-M4 to the DDR region used by the Cortex®-A7.

3. Peripheral usage and associated software[edit source]

3.1. Boot time[edit source]

DDRCTRL and DDRPHYC are kept secure and used by the FSBL to initialize the access to the DDR where it loads the SSBL (U-Boot) for execution.
STMicroelectronics wishes to make the DDR memory configuration as easy as possible, for this reason a dedicated application note[1] has been published and a DDR tuning function is available in STM32CubeMX tool in order to generate the device tree configuration that is given to the FSBL to perform this initialization.

3.2. Runtime[edit source]

3.2.1. Overview[edit source]

DDRCTRL and DDRPHYC are accessed at runtime by the secure monitor (from the FSBL or OP-TEE) to put the DDR in self-refresh state before going into Stop or Standby low power mode.
On Standby exit, the ROM code loads the FSBL that again configures the DDRCTRL and DDRPHYC before proceeding with the wake-up procedure.
The TZC controller is configured by TF-A to split the DDR in two regions:

  • the first region, the largest one, is reserved for Linux (Cortex-A7 non-secure context)
  • the second region, 32 Mbytes wide, is dedicated for OP-TEE (Cortex-A7 secure context). This area is used by its pager as a cache area from which it can load trusted applications that are authenticated in the SYSRAM internal memory before execution.

This split is visible in the overall memory mapping.

3.2.2. Software frameworks[edit source]

Internal peripherals software table template

| Core/RAM
| DDR via DDRCTRL
| Memory mapping
| Memory mapping
| 
|
|-
|}

3.2.3. Peripheral configuration[edit source]

The DDRCTRL and DDRPHYC device tree configuration is generated via STM32CubeMX tool, according to the DDR characteristics (type, size, frequency, speed grade). This configuration is applied during boot time by the FSBL (see Boot chain overview): TF-A or U-Boot SPL.

3.2.4. Peripheral assignment[edit source]

Internal peripherals assignment table template

| rowspan="1" | Core/RAM
| rowspan="1" | DDR via DDRCTRL
| DDR
| 
| 
|
|
|-
|}

4. References[edit source]