How to configure TF-A FIP

Revision as of 15:34, 23 February 2021 by Registered User (Created page with "== Article Purpose == This section details the TF-A FIP binary management for the STM32 MPU bootchain. It will explain the usage in STM32 MPU context and the build/update proc...")
(diff) ← Older revision | Latest revision (diff) | Newer revision → (diff)

1. Article Purpose[edit source]

This section details the TF-A FIP binary management for the STM32 MPU bootchain. It will explain the usage in STM32 MPU context and the build/update process that is required to deploy on your target. The build examples are based on the OpenSTLinux environment:

  • Developer Package
  • Distribution Package

2. Overview[edit source]

As explained in the TF-A Overview, this binary is used by the TF-A BL2 to load and uathenticate the next stage binaries. It can contains:

  • Boot stage binaries
  • Configuration file (Device tree)
  • Certificate (X509.3 based) for authentication

3. Package structure[edit source]

The FIP binary use a specific layout that is parse by the BL2 during the load processing.

The FIP binary start with a ToC that is recognized by the BL2. Each entry is identified with its UUID, offset in the package, size and flags. The end ToC marker is used to define the start of the binary section. All corrsponding binaries are appended corresponding to the defined offset in the ToC entry.

This structure is automatically built using the fiptool command. It will append all the binaries and create the associated ToC.

4. Fiptool command[edit source]

Fiptool is an host tool that must be used to generate the proper FIP binary.

OpenSTLinux SDK will provide the linux fiptool by default. You don't need to regenerate it if you want to update (or create) a FIP binary.

Fiptool provides a set of useful commands to manage the FIP binary. All options can be listed using:

   fiptool help
  • info : The fiptool info will provide information on a generated FIP binary
   fiptool info fip.bin 
    Secure Payload BL32 (Trusted OS): offset=0x100, size=0x1347C, cmdline="--tos-fw"
    Non-Trusted Firmware BL33: offset=0x1357C, size=0xEDDE2, cmdline="--nt-fw"
    FW_CONFIG: offset=0x10135E, size=0x226, cmdline="--fw-config"
    HW_CONFIG: offset=0x101584, size=0x1E412, cmdline="--hw-config"
    TOS_FW_CONFIG: offset=0x11F996, size=0x45AC, cmdline="--tos-fw-config"
  • update : Update allow to replace one or more images into an existing FIP package
   fiptool update --tos-fw bl32.bin fip.bin

Optional argument can be used to avoid erasing the initial FIP binary

   fiptool update --tos-fw bl32.bin --out new_fip.bin fip.bin
  • unpack : Extract all binaries from a FIP binary
   fiptool unpack fip.bin
  • remove : Remove a binary from FIP binary
   fiptool remove --tos-fw bl32.bin fip.bin

4.1. Generate the tool[edit source]

The tool is provided within the TF-A sources tools/fiptool . The tool can be build for Linux or Windows platform. A dedicate rule is available to generate the tool:

   make fiptool

It will generate the tool in tools/fiptool/fiptool source path.

4.2. TF-A build[edit source]

In case of a TF-A component complete build process, it is possible to automatically generate the FIP binary. In this case the fiptool will be automatically generated too and the FIP binaries will be part of the output folder.

5. FIP binary creation[edit source]

5.1. STM32MP1[edit source]

OpenSTLinux boot flow requires to load the following stages:

  • BL32: Secure OS and Secure Monitor (Could be SP-MIN or OP-TEE OS)
  • BL33: The non secure firmware (Recommended U-Boot)
  • HW_config: OpenSTLinux uses the hw_config as the non secure device tree
  • FW_config: Firmware configuration file listing the previous image and defining their size and the load address

5.1.1. FIP generation using fiptool command[edit source]

To create the FIP binary for the trusted boot chain (using SP-MIN), it is required to have built all the required binaries:

  • SP-MIN
  • OP-TEE in case of OP-TEE Secure OS usage
  • U-Boot
  • Firmware configuration file related to the loaded binaries

The following command will generate the FIP package that is required by BL2 to boot.

5.1.1.1. Trusted Boot chain[edit source]

You can create the FIP binary using the following command:

   fiptool create --fw-config fw-config.dtb \
              --hw-config u-boot.dtb \
              --tos-fw-config bl32.dtb \
              --tos-fw bl32.bin \ 
              --nt-fw u-boot-nodtb.bin \
               fip.bin
5.1.1.2. OP-TEE Boot chain[edit source]

You can create the FIP binary using the following command:

   fiptool create --fw-config fw-config.dtb \
               --hw-config u-boot.dtb \
               --nt-fw u-boot-nodtb.bin \
               --tos-fw tee-header_v2.bin \
               --tos-fw-extra1 tee-pager_v2.bin \
               --tos-fw-extra2 tee-pageable_v2.bin \
               fip-optee.bin

5.1.2. FIP generation using TF-A sources[edit source]

The FIP binary can be automatically generated using the TF-A official Makefile. If you have access to the TF-A source the following command will generate automatically the FIP binary

Depending the toolchain, you must add the following variables to locate the binaries:

  • BL32 : Path to the BL32 used (OP-TEE or SP_MIN)
  • BL32_EXTRA1 : Mandatory when using OP-TEE OS for the pager_v2.bin part.
  • BL32_EXTRA2 : Mandatory when using OP-TEE OS for the pageable_v2.bin part.
  • FW_CONFIG: Path to the firmware configuration file
  • BL33: Path to the non secure firmware
  • BL33_CFG: Path to the no secure device tree
5.1.2.1. Trusted Boot chain[edit source]
   make -j4 ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 BL33=<u-boot_path>/u-boot-nodtb.bin \
          BL33_CFG=<u-boot_path>/u-boot.dtb BL32=<tfa_path>/bl32.bin FW_CONFIG=<tfa_path>/fw-config.dtb fip

Adding the AARCH32_SP=sp_min will automatically manage the BL32 and FW_CONFIG path:

   make -j4 ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 AARCH32_SP=sp_min \
          BL33=<u-boot_path>/u-boot-nodtb.bin BL33_CFG=<u-boot_path>/u-boot.dtb fip
5.1.2.2. OP-TEE Boot chain[edit source]
   make -j4 ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 \
           BL33=<u-boot_path>/u-boot-nodtb.bin BL33_CFG=<u-boot_path>/u-boot.dtb \
           BL32=<optee_path>/tee_header_v2.bin BL32_EXTRA1=<optee_path>/tee_pager_v2.bin \
           BL32_EXTRA1=<optee_path>/tee_pageable_v2.bin FW_CONFIG=<tfa_path>/fw-config.dtb fip

Adding the AARCH32_SP=optee will automatically manage the FW_CONFIG path:

   make -j4 ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 AARCH32_SP=optee \
       BL32=<optee_path>/tee_header_v2.bin BL32_EXTRA1=<optee_path>/tee_pager_v2.bin \
       BL32_EXTRA1=<optee_path>/tee_pageable_v2.bin fip

5.2. Update FIP binary[edit source]

When modifying a component included in the FIP binary, it is possible to just update part of the binary. In this case the fiptool update command must be used:

5.2.1. Updating TF-A SP-MIN[edit source]

When a modification is made in the SP-MIN binary (or its device tree), the SP-MIN must be update in the FIP binary.

  • Full SP-MIN update
   fiptool update --tos-fw BL32=<tfa_path>/bl32.bin --tos-fw-config <tfa_path>/bl32.dtb fip.bin
  • SP-MIN core binary
   fiptool update --tos-fw BL32=<tfa_path>/bl32.bin fip.bin
  • SP-MIN device tree update
   fiptool update --tos-fw-config <tfa_path>/bl32.dtb fip.bin

5.2.2. Updating U-Boot[edit source]

When a new U-Boot is generated, the FIP must be updated with the following commands:

  • Full U-Boot update
   fiptool update --nt-fw <u-boot_path>/u-boot-nodtb.bin --hw-config u-boot.dtb fip.bin
  • U-Boot core binary
   fiptool update --nt-fw <u-boot_path>/u-boot-nodtb.bin fip.bin
  • U-Boot device tree update
   fiptool update --hw-config u-boot.dtb fip.bin

5.2.3. Updating OP-TEE[edit source]

OP-TEE OS rebuild required to update the FIP package.

Warning white.png Warning
It is recommended to update all OP-TEE OS images rather than trying to just update the required one
   fiptool update --tos-fw <optee_path>/tee-header_v2.bin \
          --tos-fw-extra1 <optee_path>/tee-pager_v2.bin \
          --tos-fw-extra2 <optee_path>/tee-pageable_v2.bin \
          fip-optee.bin

OP-TEE OS build process generate static binary location.
In case of mapping modification, the firmware configuration file must be adapted accordingly

5.2.4. Updating FW_CONFIG[edit source]

In case of change in the firmware configuration file, you must also update the FIP binary:

   fiptool update --fw-config fw-config.dtb fip.bin

6. Update software on board[edit source]

6.1. Partitioning of binaries[edit source]

The FIP build provides a binary named fip.bin (or fip-<board-name>-<bootchain>.bin from official release) that MUST be copied to a dedicated partition named "fip".

6.2. Update via SDCARD[edit source]

If you use an SD card, you can simply update FIP binary the dd command on your host.
Plug your SD card into the computer and copy the binary to the dedicated partition; on an SDCard/USB disk the "fip" partition is partition 3:

 - SDCARD: /dev/mmcblkXp3 (where X is the instance number)
 - SDCARD via USB reader: /dev/sdX3 (where X is the instance number)
  • Linux
   dd if=<fip binary file> of=/dev/<device partition> bs=1M conv=fdatasync
Info white.png Information
To find the partition associated to a specific label, just plug the

SDCARD/USB disk into your PC and call the following command:

   ls -l /dev/disk/by-partlabel/
 total 0
 lrwxrwxrwx 1 root root 10 Jan 17 17:38 bootfs -> ../../mmcblk0p4
 lrwxrwxrwx 1 root root 10 Jan 17 17:38 fsbl1 -> ../../mmcblk0p1          ? FSBL1 (TF-A)
 lrwxrwxrwx 1 root root 10 Jan 17 17:38 fsbl2 -> ../../mmcblk0p2          ? FSBL2 (TF-A backup ? same content as FSBL)
 lrwxrwxrwx 1 root root 10 Jan 17 17:38 rootfs -> ../../mmcblk0p5
 lrwxrwxrwx 1 root root 10 Jan 17 17:38 fip -> ../../mmcblk0p3            ? FIP
 lrwxrwxrwx 1 root root 10 Jan 17 17:38 userfs -> ../../mmcblk0p6


  • Windows

CoreUtils [1] that includes the dd command is available for Windows.

6.3. Update via USB mass storage on U-boot[edit source]

See How to use USB mass storage in U-Boot

Follow the previous section to put FIP binary onto SDCard/USB disk

6.4. Update your boot device via STM32CubeProgrammer[edit source]

Refer to the STM32CubeProgrammer documentation to update your target.