This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This article is a guideline to user space project support, fully integrated in release 1.6.0 of STM32CubeIDE.
It covers executable, static or shared libraries support from project creation to debug.
1. Prerequisites[edit source]
Minimum hardware
- STM32MP15x-based board
- Linux console
- Ethernet (or Ethernet over USB) for connection to Linux® Cortex®-A
Minimum software
- STM32CubeIDE v1.6.0 installed and
- STM32MP15 project created
- Yocto SDK installed thanks to "Setup OpenSTLinux" Cortex-A contextual menu
2. STM32CubeIDE User Space[edit source]
From STM32CubeIDE release 1.6.0 it is possible to enrich an STM32MP15x hierarchical project with User Space type project.
>>>> Figure project tree !
- executable project support
- static library project support
- shared library project support
- GTK library usage example
3. Eclipse CDT support[edit source]
From STM32CubeIDE release 1.6.0 it is also possible to easily create a STM32MP15x user space project from standard CDT Eclipse wizard.
In that case, the user space project is not part of any STM32MP15x hierarchical project and appears as a standalone project in Eclipse project explorer view.
>>>> Figure
- CDT wizard - STM32MP15x user space executable project support