STM internal peripheral

Revision as of 10:55, 7 January 2021 by Registered User

1. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the STM peripheral and its main features
  • indicate the level of security supported by this hardware block
  • explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components
  • explain, when necessary, how to configure the STM peripheral.

2. Peripheral overview[edit source]

The STM peripheral is used to log STM trace into the embedded trace FIFO (ETF). This trace can include hardware events (the list is given in the STM32MP15 reference manuals) or direct 'printf like' log from the Cortex®-A7. Once in the ETF buffer, the trace can directly be dumped from the Cortex®-A7 or to the trace port interface unit (TPIU), connected to an external probe able to decode it.

2.1. Features[edit source]

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to see which features are really implemented.

2.2. Security support[edit source]

The STM is a non secure peripheral.

2.3. Boot time[edit source]

The STM can be used to debug the boot sequence using external probe .

2.4. Runtime[edit source]

2.4.1. Overview[edit source]

The STM can be used to debug the run time application using external probe .

2.4.2. Software frameworks[edit source]

There is no software dedicated to the STM internal peripheral delivered with STM32MPU ecosystem. Nevertheless, the STM trace can be captured using an external probe via the Trace Port Interface Unit (TPIU).

2.4.3. Peripheral configuration[edit source]

Configuration of the STM is done via JTAG scripts. Those scripts must be built by user thanks to STM32MP15 reference manuals .

2.4.4. Peripheral assignment[edit source]

Internal peripherals assignment table template

| rowspan="1" | Trace & Debug
| rowspan="1" | STM
| STM
|
| 
|
| No assignment possible 
|-
|}

3. References[edit source]