TSGEN internal peripheral

Revision as of 17:00, 6 January 2021 by Registered User (→‎Overview)

1. Article purpose

The purpose of this article is to:

  • briefly introduce the TSGEN peripheral and its main features
  • indicate the level of security supported by this hardware block
  • explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components
  • explain, when necessary, how to configure the TSGEN peripheral.

2. Peripheral overview

The TSGEN peripheral generates a universal reference in time, named timestamps, and sends it to the CoreSight™ source peripherals (such as STM and ETM internal peripherals). Source peripherals use then this reference to integrate it in the generated trace. Since multiple trace generators can be implemented in a CoreSight system, timestamp allows to order traces chronologically.

2.1. Features

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to see which features are really implemented.

2.2. Security support

The TSGEN is a non secure peripheral.

3. Peripheral usage and associated software

3.1. Boot time

The TSGEN is not used at boot time.

3.2. Runtime

3.2.1. Overview

There is no dedicated driver to manage this peripheral.

3.2.2. Software frameworks

Internal peripherals software table template

| Trace & Debug
| TSGEN
| 
| 
| 
|
|-
|}

3.2.3. Peripheral configuration

The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the STM32CubeMX tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article.

3.2.4. Peripheral assignment

Internal peripherals assignment table template

| rowspan="1" | Trace & Debug
| rowspan="1" | TSGEN
| TSGEN
|
| 
|
|
|-
|}

4. References