Arm Cortex-A7

Revision as of 19:00, 5 January 2021 by Registered User (→‎Boot time)

1. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the Arm® Cortex®-A7 core and its main features
  • indicate the level of security supported by this processor

2. Peripheral overview[edit source]

The Arm Cortex-A7 can be instanciated several times into a single cluster.

The STM32MP15 main processor is a Cortex-A7 cluster embedding one or two core(s), depending on the selected line.

2.1. Features[edit source]

The Cortex-A7 is a 32 bits processor that belongs to ARMv7-VE architecture family. ARMv7-VE corresponds to the ARMv7-A architecture, with virtual extensions. Among a wide range of features, it includes a memory management unit (MMU), a separate L1 cache and a unified L2 cache in order to efficiently support rich OS such as Linux, with a high level of performance.

Refer to the STM32MP15 reference manuals for the complete list of features.

2.2. Security support[edit source]

The Cortex-A7 supports a non-secure and a secure modes that are defining two hardware execution contexts, so called Cortex-A7 non-secure and Cortex-A7 secure.

3. Peripheral usage and associated software[edit source]

3.1. Boot time[edit source]

As soon as the STM32MP1 is powered up, the Cortex-A7 starts to execute the ROM code, that is the first stage of the boot chain, then it executes the FSBL TF-A in secure mode before jumping to the SSBL U-Boot in non-secure mode.

3.2. Runtime[edit source]

3.2.1. Overview[edit source]

The Cortex-A7 is running Linux, in SMP mode (on the dual core versions, as explained in the above).

3.2.2. Software frameworks[edit source]

Internal peripherals software table template

| Ecosystem
|  Cortex-A7
|  OP-TEE
|  Linux
| 
|
|-
|}

3.2.3. Peripheral configuration[edit source]

The Cortex-A7 configuration is done by the various components running on it, according to build times parameters but also information coming from the device tree.

3.2.4. Peripheral assignment[edit source]

The Cortex-A7 is the main processor, supporting Cortex-A7 secure and Cortex-A7 non-secure contexts, so it cannot be assigned but it is managing all the peripherals assigned to those contexts.

4. How to go further[edit source]

Refer to Arm website[1] for more detailled information on this core.

5. References[edit source]