This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Template:ArticleMainWriter Template:ArticleApprovedVersion
![](/stm32mpu-ecosystem-v4/nsfr_img_auth.php/thumb/3/39/QT_logo.png/300px-QT_logo.png)
Qt logo from the official web site https://www.qt.io/
Qt[1][2][3] is a cross-platform application framework that is used to develop graphical user interfaces (GUIs) and multiplatform applications.
meta-qt5[4] is a Yocto compatible meta layer that provides recipes for Qt modules.
The OpenSTLinux distribution is ready to link with this meta layer.
The OpenSTLinux distribution offers the possibility to use an example of an image based on the QT framework (st-example-image-qt) as a demonstrator, not for developing products. For Qt-based products, the list of STMicroelectronics partners can be found on STMicroelectronics web site.
References:
- ↑ https://www.qt.io/ Qt home page
- ↑ https://www.qt.io/qt-for-device-creation/ Qt for Embedded Devices
- ↑ https://www.qt.io/qt-for-application-development/ Qt for Application Development
- ↑ https://github.com/meta-qt5/meta-qt5/ Qt5 OpenEmbedded/Yocto Project layer