1. Article purpose[edit source]
This article explains how to configure the DDRCTRL and DDRPHYC internal peripheral done by the first stage bootloader.
The configuration is performed using the device tree mechanism that provides a hardware description of the DDR subsystem (DDR controler and DDR PHY peripheral), used by the first stage bootloader to initialize the DDR before to load second stage bootloader.
The DDR settings are only used in the device tree of the boot chain FSBL; so in the TF-A device tree for OpenSTLinux official delivery (or in SPL only for the DDR tuning tool).
Even if the DDR node information is also present in the U-Boot device tree, it is not used during boot by this SSBL.
2. DT bindings documentation[edit source]
The DDR sub system is a memory-controllers device represented by the device tree bindings.
The following binding-related documentation explains how to write device tree files for DDR subsystem:
- TF-A: docs/devicetree/bindings/memory-controllers/st,stm32mp1-ddr.txt"[1]
- U-Boot: doc/device-tree-bindings/memory-controllers/st,stm32mp1-ddr.tx"[2]
3. DT configuration[edit source]
This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device tree file split.
STM32CubeMX can be used to generate this DDR board device tree. Refer to How to configure the DT using STM32CubeMX for more details.
3.1. DT configuration (STM32 level)[edit source]
The STM32MP1 DDR node is located in stm32mp15-ddr.dtsi' '[3] (see Device tree for further explanation).
/ { soc { u-boot,dm-spl; ddr: ddr@0x5A003000{ u-boot,dm-spl; u-boot,dm-pre-reloc; compatible = "st,stm32mp1-ddr"; reg = <0x5A003000 0x550 0x5A004000 0x234>; clocks = <&rcc_clk AXIDCG>, <&rcc_clk DDRC1>, <&rcc_clk DDRC2>, <&rcc_clk DDRPHYC>, <&rcc_clk DDRCAPB>, <&rcc_clk DDRPHYCAPB>; clock-names = "axidcg", "ddrc1", "ddrc2", "ddrphyc", "ddrcapb", "ddrphycapb"; ..... status = "okay"; }; }; };
3.2. DT configuration (board level)[edit source]
The next attributes the DDR settings, the register values used to inialized the DDR controller and the DDR PHY, they are generated by DDR tools included in STM32 Cube MX.
3.2.1. info attributes[edit source]
Just strings to identify the configuraiton:
- st,mem-name: name for DDR configuration, simple string for information
- st,mem-speed: DDR expected speed for the setting in kHz
- st,mem-size: DDR mem size in byte
3.2.2. controllor attributes[edit source]
- st,ctl-reg: controleur values depending of the DDR type (DDR3/LPDDR2/LPDDR3)
- for STM32MP1 Series: 25 values are requested in this order (MSTR MRCTRL0 MRCTRL1 DERATEEN DERATEINT PWRCTL PWRTMG HWLPCTL RFSHCTL0 RFSHCTL3 CRCPARCTL0 ZQCTL0 DFITMG0 DFITMG1 DFILPCFG0 DFIUPD0 DFIUPD1 DFIUPD2 DFIPHYMSTR ODTMAP DBG0 DBG1 DBGCMD POISONCFG PCCFG)
- st,ctl-timing: controleur values depending of frequency and timing parameter of DDR
- st,ctl-map: controleur values depending of address mapping
- st,ctl-perf: controleur values depending of performance and scheduling
3.2.3. phy attributes[edit source]
- st,phy-reg: phy values depending of the DDR type (DDR3/LPDDR2/LPDDR3)
- st,phy-timing : phy values depending of frequency and timing parameter of DDR
- st,phy-cal : phy cal depending of calibration or tuning of DDR
The board configuration defines each needed configuration (DDR_...) and include the STM32 level device tree.
3.3. DT configuration examples[edit source]
/ { st,mem-name = "DDR3 2x4Gb 533MHz"; st,mem-speed = <533000>; st,mem-size = <0x40000000>; st,ctl-reg = < 0x00040401 /*MSTR*/ 0x00000010 /*MRCTRL0*/ 0x00000000 /*MRCTRL1*/ 0x00000000 /*DERATEEN*/ 0x00800000 /*DERATEINT*/ 0x00000000 /*PWRCTL*/ 0x00400010 /*PWRTMG*/ 0x00000000 /*HWLPCTL*/ 0x00210000 /*RFSHCTL0*/ 0x00000000 /*RFSHCTL3*/ 0x00000000 /*CRCPARCTL0*/ 0xC2000040 /*ZQCTL0*/ 0x02050105 /*DFITMG0*/ 0x00000202 /*DFITMG1*/ 0x07000000 /*DFILPCFG0*/ 0xC0400003 /*DFIUPD0*/ 0x00000000 /*DFIUPD1*/ 0x00000000 /*DFIUPD2*/ 0x00000000 /*DFIPHYMSTR*/ 0x00000001 /*ODTMAP*/ 0x00000000 /*DBG0*/ 0x00000000 /*DBG1*/ 0x00000000 /*DBGCMD*/ 0x00000000 /*POISONCFG*/ 0x00000010 /*PCCFG*/ >; st,ctl-timing = < 0x0080008A /*RFSHTMG*/ 0x121B2414 /*DRAMTMG0*/ 0x000D041B /*DRAMTMG1*/ 0x0607080E /*DRAMTMG2*/ 0x0050400C /*DRAMTMG3*/ 0x07040407 /*DRAMTMG4*/ 0x06060303 /*DRAMTMG5*/ 0x02020002 /*DRAMTMG6*/ 0x00000202 /*DRAMTMG7*/ 0x00001005 /*DRAMTMG8*/ 0x000D041B /*DRAMTMG14*/ 0x06000600 /*ODTCFG*/ >; st,ctl-map = < 0x00080808 /*ADDRMAP1*/ 0x00000000 /*ADDRMAP2*/ 0x00000000 /*ADDRMAP3*/ 0x00001F1F /*ADDRMAP4*/ 0x07070707 /*ADDRMAP5*/ 0x0F070707 /*ADDRMAP6*/ 0x00000000 /*ADDRMAP9*/ 0x00000000 /*ADDRMAP10*/ 0x00000000 /*ADDRMAP11*/ >; st,ctl-perf = < 0x00001201 /*SCHED*/ 0x00001201 /*SCHED*/1 0x01000001 /*PERFHPR1*/ 0x08000200 /*PERFLPR1*/ 0x08000400 /*PERFWR1*/ 0x00010000 /*PCFGR_0*/ 0x00000000 /*PCFGW_0*/ 0x02100B03 /*PCFGQOS0_0*/ 0x00800100 /*PCFGQOS1_0*/ 0x01100B03 /*PCFGWQOS0_0*/ 0x01000200 /*PCFGWQOS1_0*/ 0x00010000 /*PCFGR_1*/ 0x00000000 /*PCFGW_1*/ 0x02100B03 /*PCFGQOS0_1*/ 0x00800000 /*PCFGQOS1_1*/ 0x01100B03 /*PCFGWQOS0_1*/ 0x01000200 /*PCFGWQOS1_1*/ >; st,phy-reg = < 0x01442E02 /*PGCR*/ 0x10400812 /*ACIOCR*/ 0x00000C40 /*DXCCR*/ 0xF200001F /*DSGCR*/ 0x0000000B /*DCR*/ 0x00010000 /*ODTCR*/ 0x0000007B /*ZQ0CR1*/ 0x0000CE81 /*DX0GCR*/ 0x0000CE81 /*DX1GCR*/ 0x0000CE81 /*DX2GCR*/ 0x0000CE81 /*DX3GCR*/ >; st,phy-timing = < 0x0022A41B /*PTR0*/ 0x047C0740 /*PTR1*/ 0x042D9C80 /*PTR2*/ 0x369477D0 /*DTPR0*/ 0x098A00D8 /*DTPR1*/ 0x10023600 /*DTPR2*/ 0x00000830 /*MR0*/ 0x00000000 /*MR1*/ 0x00000208 /*MR2*/ 0x00000000 /*MR3*/ >; st,phy-cal = < 0x40000000 /*DX0DLLCR*/ 0xFFFFFFFF /*DX0DQTR*/ 0x3DB02000 /*DX0DQSTR*/ 0x40000000 /*DX1DLLCR*/ 0xFFFFFFFF /*DX1DQTR*/ 0x3DB02000 /*DX1DQSTR*/ 0x40000000 /*DX2DLLCR*/ 0xFFFFFFFF /*DX2DQTR*/ 0x3DB02000 /*DX2DQSTR*/ 0x40000000 /*DX3DLLCR*/ 0xFFFFFFFF /*DX3DQTR*/ 0x3DB02000 /*DX3DQSTR*/ >; };
but Cube MX generate the needed values as defines (DDR_...), and the file "stm32mp15-ddr.dtsi"<ref name="stm32mp15-ddr.dtsi"> are preprocessed and used these defines to generate a correct device tree.
For example the file fdts/stm32mp15-ddr3-1x4Gb-1066-binG.dtsi
#define DDR_MEM_NAME "DDR3-1066/888 bin G 1x4Gb 533MHz v1.45" #define DDR_MEM_SPEED 533000 #define DDR_MEM_SIZE 0x20000000 #define DDR_MSTR 0x00041401 #define DDR_MRCTRL0 0x00000010 #define DDR_MRCTRL1 0x00000000 #define DDR_DERATEEN 0x00000000 #define DDR_DERATEINT 0x00800000
.....
#define DDR_DX2DQSTR 0x3DB02000 #define DDR_DX3GCR 0x0000CE80 #define DDR_DX3DLLCR 0x40000000 #define DDR_DX3DQTR 0xFFFFFFFF #define DDR_DX3DQSTR 0x3DB02000 #include "stm32mp15-ddr.dtsi"
4. How to configure the DT using STM32CubeMX[edit source]
The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX support all the defines described in the above DT bindings documentation paragraph. If so, the tool inserts all the needed defines in . Refer to STM32CubeMX user manual for further information.
See also How_to_create_your_board_device_tree#DDR configuration with STM32CubeMX DDR Tuning Tool.
5. References[edit source]
Please refer to the following links for additional information:
- ↑ docs/devicetree/bindings/memory-controllers/st,stm32mp1-ddr.txt TF-A DDR binding information file
- ↑ doc/device-tree-bindings/memory-controllers/st,stm32mp1-ddr.txt U-Boot DDR binding information file
- ↑ fdts/stm32mp15-ddr.dtsi (for TF-A): STM32MP157C device tree files