1. Article purpose[edit source]
This article provides the basic information needed to start using the Linux® kernel tool: ftrace[1].
2. Introduction[edit source]
The following table provides a brief description of the tool, as well as its availability depending on the software packages:
: this tool is either present (ready to use or to be activated), or can be integrated and activated on the software package.
: this tool is not present and cannot be integrated, or it is present but cannot be activated on the software package.
Tool | STM32MPU Embedded Software distribution | STM32MPU Embedded Software distribution for Android™ | ||||||
---|---|---|---|---|---|---|---|---|
Name | Category | Purpose | Starter Package | Developer Package | Distribution Package | Starter Package | Developer Package | Distribution Package |
ftrace | Tracing tools | ftrace[1] (Function Tracer) is a powerful kernel tracing utility that is able, for instance, to trace every kernel function calls and kernel events without adding any extra code in your kernel source code |
Note: Before Linux kernel 4.1, all the ftrace tracing control files were within the debugfs file system, which is typically located at /sys/kernel/debug/tracing. Now, it is located in /sys/kernel/tracing, and independent from debugfs.
For backward compatibility, when mounting the debugfs file system, the tracefs file system is automatically mounted at: /sys/kernel/debug/tracing.
All files located in the tracefs file system are located in that debugfs file system directory as well.
Please note that all functions present in the symbol table are available for ftrace. To know if a function is available in the symbol list, you can use the command "nm vmlinux | grep <function_name>"
3. Installing the trace and debug tool on your target board[edit source]
ftrace is a kernel feature which is not activated by default in the OpenSTLinux distributions as there is an impact on the Linux kernel size (around 1.5% increase of vmlinux), and also an impact on the overall performance, because of an additional treatment done to the trace kernel events and function calls.
In order to use 'Kernel Function Tracer' required for ftrace, the Linux kernel configuration must activate CONFIG_FUNCTION_TRACER and CONFIG_FUNCTION_GRAPH_TRACER using the Linux® kernel menuconfig tool:
Symbol: FUNCTION_TRACER Location: Kernel Hacking ---> Tracers --> [*] Kernel Function Tracer Symbol: FUNCTION_GRAPH_TRACER Location: Kernel Hacking ---> Tracers --> [*] Kernel Function Tracer [*] Kernel Function Graph Tracer
3.1. Using the STM32MPU Embedded Software distribution[edit source]
3.1.1. Developer Package[edit source]
It is not recommended to enable the ftrace kernel configuration by using the Developer Package, as all external modules should be also recompiled (e.g. gcnano driver for GPU STM32MP1), and this is not possible with the Developer Package, which does not necessary provide all the sources.
That is the reason why this is set as not supported for Developer Package.
3.1.2. Distribution Package[edit source]
- Enable the required Linux kernel configuration
- To enable CONFIG_FUNCTION_TRACER and CONFIG_FUNCTION_GRAPH_TRACER in the Linux kernel configuration, please refer to Menuconfig or how to configure kernel article to get instructions for modifying the configuration and recompiling the Linux kernel image in the Distribution Package context.
- You must also recompile the external Linux kernel module(s) (if existing) being not part of the Linux kernel source tree.
- Example for gcnano driver of GPU STM32MP1:
bitbake gcnano-driver-stm32mp
- Re-build the full OpenSTLinux image, in order to recompile all dependencies and have correct rootfs including the external Linux kernel modules
bitbake st-image-weston
3.2. Using the STM32MPU Embedded Software distribution for Android™[edit source]
3.2.1. Distribution Package[edit source]
- Enable the required Linux kernel configuration
- To enable CONFIG_FUNCTION_TRACER and CONFIG_FUNCTION_GRAPH_TRACER in the Linux kernel configuration, please refer to How to customize kernel for Android article to get instructions for modifying the configuration
- Recompile the Linux kernel image and modules in the Distribution Package for Android™ context.
build_kernel vmlinux -i build_kernel modules -i
- You must also recompile the external Linux kernel module(s) (if existing) being not part of the Linux kernel source tree.
- Example for gcnano driver of GPU STM32MP1:
build_kernel gpu -i
- Rebuild the full Android images, in order to recompile all dependencies and take into account new prebuilt images for Linux kernel image and modules:
make -j
4. Getting started[edit source]
4.1. Using ftrace at runtime[edit source]
First of all, you need to enable/activate the ftrace feature from target.
- Once target booted and logged, mount tracefs:
mount -t tracefs nodev /sys/kernel/tracing
Below information is related to the Android™ distribution Need to enable root access rights
adb root adb shell ...
su ... |
- At that step, all the 'ftrace' features take place in the file system directory path /sys/kernel/tracing.
To find out which tracers are available, simply cat the available_tracers file in the tracing directory:
cat /sys/kernel/tracing/available_tracers
function_graph function nop
More tracers can be added by kernel build configurations. Please refer to To go further section.
4.2. Filter option[edit source]
You can get the list of available filter function with the following command:
cat /sys/kernel/tracing/available_filter_functions
4.2.1. Function tracer mode[edit source]
- Start a tracing session
echo 1 > /sys/kernel/tracing/tracing_on
- To enable the function tracer, just write function to the current_tracer file. You can then verify the current value:
echo function > /sys/kernel/tracing/current_tracer cat /sys/kernel/tracing/current_tracer function
cat /sys/kernel/tracing/trace | head -20 # tracer: function # # entries-in-buffer/entries-written: 144045/33695515 #P:2 # # _-----=> irqs-off # / _----=> need-resched # | / _---=> hardirq/softirq # || / _--=> preempt-depth # ||| / delay # TASK-PID CPU# |||| TIMESTAMP FUNCTION # | | | |||| | | date-3591 [001] ...3 3278.796042: memblock_is_map_memory <-pfn_valid date-3591 [001] ...3 3278.796046: unlock_page <-filemap_map_pages date-3591 [001] ...3 3278.796051: alloc_set_pte <-filemap_map_pages date-3591 [001] ...3 3278.796053: add_mm_counter_fast <-alloc_set_pte date-3591 [001] ...3 3278.796055: page_add_file_rmap <-alloc_set_pte date-3591 [001] ...3 3278.796057: __sync_icache_dcache <-alloc_set_pte date-3591 [001] ...3 3278.796059: pfn_valid <-__sync_icache_dcache date-3591 [001] ...3 3278.796061: memblock_is_map_memory <-pfn_valid date-3591 [001] ...3 3278.796064: unlock_page <-filemap_map_pages
- To apply function(s) filter you can set value(s) in /sys/kernel/tracing/set_ftrace_filter, then check for new content of the trace:
# Here we take the example with all uart functions echo "*uart*" > /sys/kernel/tracing/set_ftrace_filter # Clean the existing trace echo > /sys/kernel/tracing/trace # Display new trace content (in that case, please do some actions in the console to get some traces) cat /sys/kernel/tracing/trace | head -20 # tracer: function # # _-----=> irqs-off # / _----=> need-resched # | / _---=> hardirq/softirq # || / _--=> preempt-depth # ||| / delay # TASK-PID CPU# |||| TIMESTAMP FUNCTION # | | | |||| | | sh-343 [000] .... 9313.041827: uart_ioctl <-tty_ioctl sh-343 [000] .... 9313.041855: uart_ioctl <-tty_ioctl sh-343 [000] .... 9313.041866: uart_chars_in_buffer <-tty_wait_until_sent sh-343 [000] .... 9313.041870: uart_wait_until_sent <-tty_wait_until_sent sh-343 [000] .... 9313.041875: uart_set_termios <-tty_set_termios sh-343 [000] .... 9313.041968: uart_write_room <-tty_write_room sh-343 [000] .... 9313.041974: uart_write <-n_tty_write sh-343 [000] d..1 9313.041979: __uart_start <-uart_write sh-343 [000] d..1 9313.041987: uart_write_wakeup <-stm32_transmit_chars sh-343 [000] d.h2 9313.042007: uart_write_wakeup <-stm32_transmit_chars sh-343 [000] d.h2 9313.042022: uart_write_wakeup <-stm32_transmit_chars
- More information about filtering option and configuration is available in the Linux documentation for ftrace[2].
- To empty the trace please refer to the paragraph Erasing trace
- To clear out the filter so that all functions are recorded again:
echo > /sys/kernel/tracing/set_ftrace_filter
4.2.2. Graph function tracer mode[edit source]
Start a tracing session:
echo 1 > /sys/kernel/tracing/tracing_on
To enable the function tracer, just write function_graph into the current_tracer file. You can then verify the current value:
echo function_graph > /sys/kernel/tracing/current_tracer cat /sys/kernel/tracing/current_tracer function_graph
cat /sys/kernel/tracing/trace | head -20 # tracer: function_graph # # CPU DURATION FUNCTION CALLS # | | | | | | | 1) 1.015 us | _spin_lock_irqsave(); 1) 0.476 us | internal_add_timer(); 1) 0.423 us | wake_up_idle_cpu(); 1) 0.461 us | _spin_unlock_irqrestore(); 1) 4.770 us | } 1) 5.725 us | } 1) 0.450 us | mutex_unlock(); 1) + 24.243 us | } 1) 0.483 us | _spin_lock_irq(); 1) 0.517 us | _spin_unlock_irq(); 1) | prepare_to_wait() { 1) 0.468 us | _spin_lock_irqsave(); 1) 0.502 us | _spin_unlock_irqrestore(); 1) 2.411 us | } 1) 0.449 us | kthread_should_stop(); 1) | schedule() {
To apply a graph function(s) filter, you can set value(s) in /sys/kernel/tracing/set_graph_function, then check for the new content of the trace:
# Here we take the example with all uart functions echo "*uart*" > /sys/kernel/tracing/set_graph_function # Clean the existing trace echo > /sys/kernel/tracing/trace
# Display the new trace content (in that case, please do some action in the console to get some traces) cat /sys/kernel/tracing/trace | head -20 # tracer: function_graph # # CPU DURATION FUNCTION CALLS # | | | | | | | 1) | uart_ioctl() { 1) 0.875 us | mutex_lock(); 1) 0.792 us | mutex_unlock(); 1) + 15.542 us | } 1) | uart_ioctl() { 1) 0.583 us | mutex_lock(); 1) 0.584 us | mutex_unlock(); 1) 9.792 us | } 1) | uart_chars_in_buffer() { 1) | _raw_spin_lock_irqsave() { 1) 0.667 us | preempt_count_add(); 1) 5.458 us | } 1) | _raw_spin_unlock_irqrestore() { 1) 0.583 us | preempt_count_sub(); 1) 5.000 us | } 1) + 19.459 us | } 1) 1.541 us | uart_wait_until_sent(); 1) | uart_set_termios() { 1) 0.583 us | mutex_lock(); 1) 0.583 us | mutex_unlock(); 1) + 10.291 us | } 1) | uart_write_room() { 1) | _raw_spin_lock_irqsave() { 1) 0.666 us | preempt_count_add(); 1) 5.333 us | } 1) | _raw_spin_unlock_irqrestore() { 1) 0.583 us | preempt_count_sub(); 1) 5.000 us | } 1) + 19.625 us | } 1) | uart_write() { 1) | _raw_spin_lock_irqsave() { 1) 0.625 us | preempt_count_add(); 1) 5.209 us | } 1) | __uart_start() { 1) | stm32_start_tx() { 1) | stm32_transmit_chars() {
- More information about filtering option and configuration on the Linux documentation for ftrace[2].
- To empty the trace please refer to the paragraph Erasing trace
- To clear out this special filter so that all functions will be recorded again:
echo > /sys/kernel/tracing/set_graph_function
4.3. Buffer size[edit source]
A buffer is allocated for each CPU. For making a trace analysis you can change this buffer size (increase or decrease).
- This is possible to read the given size value per CPU, or the total (value is given in kilobytes):
# Per CPU cat /sys/kernel/tracing/buffer_size_kb 1411 or cat /sys/kernel/tracing/per_cpu/cpuX/buffer_size_kb 1411
# Total for all CPUs: combined size of all the trace buffers
cat /sys/kernel/tracing/buffer_total_size_kb
2822
- To change the value (note that the trace buffers are allocated in pages (blocks of memory that the kernel uses for allocation, usually 4 Kbytes in size))
# Same value for each CPU (here 1000*4096/1024=4000) echo 4000 > /sys/kernel/tracing/buffer_size_kb or # Change buffer size value for a specific CPU X (here 1000*4096/1024=4000) echo 4000 > /sys/kernel/tracing/per_cpu/cpuX/buffer_size_kb
4.4. Using ftrace at boot time[edit source]
You can use ftrace from the kernel boot, which can be very useful to debug the boot issues.
For this, you have to use the kernel command-line parameters:
- ftrace and also ftrace_filter or ftrace_graph_filter if you want to add filter.
4.4.1. With STM32MPU Embedded Software package[edit source]
For instance, to modify the kernel bootargs you can do it in the following ways:
- Mount a boot partition from the Linux kernel console, and then update the extlinux.conf file using the vi editor (see man page[3], or introduction page[4] ). In example:
mount /dev/mmcblk0p4 /boot # As example for SDCard boot on STM32MP15 Evaluation board, otherwise /boot/<bootdevice>_<platform>-<boardId>_extlinux/extlinux.conf vi /boot/mmc0_stm32mp157c-ev1_extlinux/extlinux.conf
Update kernel command-line by adding ftrace parameter:
- - function tracer mode
root=/dev/mmcblk0p5 rootwait rw console=ttyS3,115200 ftrace=function ftrace_filter=*uart*
- - function_graph tracer mode
root=/dev/mmcblk0p5 rootwait rw console=ttyS3,115200 ftrace=function_graph ftrace_graph_filter=*uart*
Save and quit file update, and then reboot the board
or
- Edit the extlinux.conf file from the microSD&trade card (if used as boot device)
- - Insert microSD&trade card on host PC
- - Check for boot partition mounted (i.e /media/$USER/bootfs)
- - Edit the extlinux file corresponding to your setup (i.e
/media/$USER/bootfs/mmc0_stm32mp157c-ev1_extlinux/extlinux.conf
) - - Modify the command-line following your ftrace tracer configuration required (see above)
- - Save modification, then insert the microSD&trade card on your target
- - Boot and check for kernel command-line
4.4.2. With STM32MPU Embedded Software package for Android™[edit source]
For instance, to modify the kernel bootargs you can do it in the following ways which require boot image rebuilt:
- Edit file
device/stm/<STM32Series>/<BoardId>/Boardconfig.mk
- Update kernel command-line by adding ftrace parameter in the BOARD_KERNEL_CMDLINE variable:
- - function tracer mode
... # =========================================================== # # Kernel command line # # =========================================================== # BOARD_KERNEL_CMDLINE := console=ttySTM0,115200 androidboot.console=/dev/ttySTM0 consoleblank=0 earlyprintk BOARD_KERNEL_CMDLINE += skip_initramfs ro rootfstype=ext4 rootwait BOARD_KERNEL_CMDLINE += init=/init firmware_class.path=/vendor/firmware BOARD_KERNEL_CMDLINE += androidboot.hardware=stm BOARD_KERNEL_CMDLINE += ftrace=function ftrace_filter=*uart* ...
- - function_graph tracer mode
... # =========================================================== # # Kernel command line # # =========================================================== # BOARD_KERNEL_CMDLINE := console=ttySTM0,115200 androidboot.console=/dev/ttySTM0 consoleblank=0 earlyprintk BOARD_KERNEL_CMDLINE += skip_initramfs ro rootfstype=ext4 rootwait BOARD_KERNEL_CMDLINE += init=/init firmware_class.path=/vendor/firmware BOARD_KERNEL_CMDLINE += androidboot.hardware=stm BOARD_KERNEL_CMDLINE += ftrace=function_graph ftrace_graph_filter=*uart* ...
- Rebuild and reload the boot image
4.4.3. Checking for trace[edit source]
When booted, to check for the trace, you have to mount the tracefs:
mount -t tracefs nodev /sys/kernel/tracing
Below information is related to the Android™ distribution Need to enable root access rights
adb root adb shell ...
su ... |
Then look at for trace content (i.e. for function trace):
cat /sys/kernel/tracing/trace | head -20 # tracer: function # # _-----=> irqs-off # / _----=> need-resched # | / _---=> hardirq/softirq # || / _--=> preempt-depth # ||| / delay # TASK-PID CPU# |||| TIMESTAMP FUNCTION # | | | |||| | | systemd-1 [000] .... 1.087213: uart_register_driver <-usart_init systemd-1 [000] .... 1.087847: uart_get_rs485_mode <-stm32_serial_probe systemd-1 [000] .... 1.088436: uart_add_one_port <-stm32_serial_probe systemd-1 [000] .... 1.098000: uart_parse_options <-stm32_console_setup systemd-1 [000] .... 1.098007: uart_set_options <-stm32_console_setup systemd-1 [000] .... 1.098014: uart_get_baud_rate <-stm32_set_termios systemd-1 [000] d..1 1.098019: uart_update_timeout <-stm32_set_termios systemd-1 [000] d..1 1.098090: uart_console_write <-stm32_console_write systemd-1 [000] d..1 1.105231: uart_console_write <-stm32_console_write systemd-1 [000] d..1 1.114697: uart_console_write <-stm32_console_write systemd-1 [000] d..1 1.120300: uart_console_write <-stm32_console_write
4.4.4. Capturing an oops (from startup) to the serial console[edit source]
An interesting application to enable ftrace at boot, is to capture the function calls leading up to a panic by placing the following parameters on the kernel command line:
root=/dev/mmcblk0p5 rootwait rw console=ttyS3,115200 ftrace=function ftrace_dump_on_oops
When the oops occurs, the ftrace buffer will be automatically dumped on the console message.
4.5. Erasing trace[edit source]
This is possible to erase content of trace for ftrace with the following command:
echo > /sys/kernel/tracing/trace
5. To go further[edit source]
5.1. Adding print information for ftrace[edit source]
In addition to the printing Linux kernel functions, it is possible to trace the specific debug information with ftrace by using trace_printk function.
It can be used just like printk(), and can also be used in any context (interrupt code, NMI code, and scheduler code).
trace_printk does not output to the console, but writes to the ftrace ring buffer and can be read via the trace file.
To use trace_printk function, you have to include linux/ftrace.h in your source code:
... #include <linux/ftrace.h> ...
Then use trace_printk syntax as printk (see below example):
... trace_printk("%s: %d uart_tx_stopped(port) %i\n", __FUNCTION__, __LINE__, uart_tx_stopped(port)); ...
5.2. Stack Trace[edit source]
Extracted from Kernel documentation for ftrace[2].
Since the kernel has a fixed sized stack, it is important to not waste it in functions. A kernel developer must be aware of what the functions allocate on the stack. If they add too much size, the system can be in danger of a stack overflow, and a corruption will occur, usually leading to a system panic.
There are some tools that check this, usually with interrupts periodically checking the usage. But if you can perform a check at every function call that will become very useful. As ftrace provides a function tracer, it makes it convenient to check the stack size at every function call. This is enabled via the stack tracer.
The Linux kernel configuration option CONFIG_STACK_TRACER enables the ftrace stack tracing functionality.
Symbol: STACK_TRACER
Location:
Kernel Hacking --->
Tracers -->
[*] Trace max stack
To enable it, write a '1' into /proc/sys/kernel/stack_tracer_enabled.
echo 1 > /proc/sys/kernel/stack_tracer_enabled
You can also enable it from the kernel command line to trace the stack size of the kernel during boot up, by adding "stacktrace" to the kernel command line parameter.
root=/dev/mmcblk0p5 rootwait rw console=ttyS3,115200 stacktrace
When booted, to check for the trace, you have to mount first the tracefs, then display the trace content:
mount -t tracefs nodev /sys/kernel/tracing cat /sys/kernel/tracing/stack_max_size 2928 cat /sys/kernel/tracing/stack_trace Depth Size Location (82 entries) ----- ---- -------- 0) 4328 4 __rcu_read_unlock+0x14/0x68 1) 4324 180 select_task_rq_fair+0x8ac/0xb7c 2) 4144 64 try_to_wake_up+0x100/0x3fc 3) 4080 16 wake_up_process+0x20/0x24 4) 4064 24 swake_up_locked.part.0+0x20/0x38 5) 4040 24 swake_up+0x38/0x48 6) 4016 16 rcu_gp_kthread_wake+0x4c/0x50 7) 4000 24 rcu_report_qs_rsp+0x50/0x84 8) 3976 120 rcu_report_qs_rnp+0x258/0x2ec 9) 3856 80 rcu_process_callbacks+0x290/0x43c 10) 3776 96 __do_softirq+0x12c/0x3ec 11) 3680 16 irq_exit+0xd0/0x118 12) 3664 48 __handle_domain_irq+0x90/0xfc 13) 3616 40 gic_handle_irq+0x5c/0xa0 14) 3576 68 __irq_svc+0x6c/0xa8 15) 3508 28 unwind_get_byte+0x20/0x74 16) 3480 160 unwind_frame+0x1a8/0x6b0 17) 3320 32 walk_stackframe+0x34/0x40 18) 3288 56 __save_stack_trace+0xa4/0xa8 19) 3232 16 save_stack_trace+0x30/0x34 20) 3216 72 create_object+0x120/0x278 21) 3144 40 kmemleak_alloc+0x8c/0xd4 22) 3104 64 kmem_cache_alloc+0x184/0x2f0 23) 3040 64 __kernfs_new_node+0x58/0x15c 24) 2976 24 kernfs_new_node+0x2c/0x48 25) 2952 24 __kernfs_create_file+0x28/0xb8 26) 2928 56 sysfs_add_file_mode_ns+0xc4/0x1a0 27) 2872 24 sysfs_create_file_ns+0x4c/0x58 28) 2848 56 kobject_add_internal+0x174/0x358 29) 2792 40 kobject_add+0x50/0x98 30) 2752 32 irq_sysfs_add+0x44/0x60 31) 2720 72 __irq_alloc_descs+0x174/0x234 32) 2648 48 irq_domain_alloc_descs+0x64/0xe4 33) 2600 56 irq_create_mapping+0x108/0x1fc 34) 2544 56 irq_create_fwspec_mapping+0x140/0x318 35) 2488 88 irq_create_of_mapping+0x5c/0x64 36) 2400 168 of_irq_get+0x68/0x78 37) 2232 24 stpmu1_regulator_parse_dt+0x68/0x80 38) 2208 96 regulator_register+0x218/0x970 39) 2112 32 devm_regulator_register+0x54/0x84 40) 2080 136 stpmu1_regulator_probe+0x350/0x5f4 41) 1944 32 platform_drv_probe+0x60/0xbc 42) 1912 64 driver_probe_device+0x2f4/0x488 43) 1848 32 __device_attach_driver+0xac/0x14c 44) 1816 40 bus_for_each_drv+0x54/0xa4 45) 1776 40 __device_attach+0xc0/0x150 46) 1736 16 device_initial_probe+0x1c/0x20 47) 1720 32 bus_probe_device+0x94/0x9c 48) 1688 64 device_add+0x3c0/0x5d0 49) 1624 16 of_device_add+0x44/0x4c 50) 1608 40 of_platform_device_create_pdata+0x84/0xb4 51) 1568 104 of_platform_bus_create+0x160/0x2f8 52) 1464 56 of_platform_populate+0x9c/0x134 53) 1408 32 stpmu1_probe+0x6c/0xac 54) 1376 40 i2c_device_probe+0x290/0x2dc 55) 1336 64 driver_probe_device+0x2f4/0x488 56) 1272 32 __device_attach_driver+0xac/0x14c 57) 1240 40 bus_for_each_drv+0x54/0xa4 58) 1200 40 __device_attach+0xc0/0x150 59) 1160 16 device_initial_probe+0x1c/0x20 60) 1144 32 bus_probe_device+0x94/0x9c 61) 1112 64 device_add+0x3c0/0x5d0 62) 1048 24 device_register+0x24/0x28 63) 1024 48 i2c_new_device+0x14c/0x2f4 64) 976 96 of_i2c_register_device+0x134/0x1dc 65) 880 40 of_i2c_register_devices+0x8c/0x100 66) 840 48 i2c_register_adapter+0x184/0x404 67) 792 48 i2c_add_adapter+0xa4/0x138 68) 744 160 stm32f7_i2c_probe+0x954/0xd08 69) 584 32 platform_drv_probe+0x60/0xbc 70) 552 64 driver_probe_device+0x2f4/0x488 71) 488 32 __driver_attach+0x110/0x12c 72) 456 40 bus_for_each_dev+0x5c/0xac 73) 416 16 driver_attach+0x2c/0x30 74) 400 48 bus_add_driver+0x1d0/0x274 75) 352 24 driver_register+0x88/0x104 76) 328 16 __platform_driver_register+0x50/0x58 77) 312 16 stm32f7_i2c_driver_init+0x24/0x28 78) 296 112 do_one_initcall+0x54/0x178 79) 184 72 kernel_init_freeable+0x1dc/0x274 80) 112 24 kernel_init+0x18/0x124 81) 88 88 ret_from_fork+0x14/0x24
5.3. More tracers[edit source]
More tracers are available for ftrace. Please refer to the Kernel documentation for ftrace[2].
Tracer name | Descriptipn |
---|---|
blk | Block tracer. The tracer used by the blktrace user application |
hwlat | Hardware Latency tracer. It is used to detect if the hardware produces any latency |
irqsoff | Traces the areas that disable interrupts and saves the trace with the longest max latency |
preemptoff | Similar to irqsoff but traces and records the amount of time for which preemption is disabled |
preemptirqsoff | Similar to irqsoff and preemptoff, but traces and records the largest time for which irqs and/or preemption is disabled |
wakeup | Traces and records the max latency that it takes for the highest priority task to get scheduled after it has been woken up |
wakeup_rt | Traces and records the max latency that it takes for just RT tasks (as the current "wakeup" does) |
wakeup_dl | Traces and records the max latency that it takes for a SCHED_DEADLINE task to be woken (as the "wakeup" and "wakeup_rt" does) |
mmiotrace | A special tracer that is used to trace binary module. It traces all the calls that a module makes to the hardware |
branch | This tracer can be configured when tracing likely/unlikely calls within the kernel |
nop | This is the "trace nothing" tracer |
5.4. Complementary tools[edit source]
While the debugfs interface is rather simple, it can also be awkward to work with. Some tools are proposed to simplify the user experience with ftrace.
- trace-cmd is a command-line tool that works and interacts with ftrace instead of echoing commands into specific files and reading the result from another file. It proposes a high level user command interface to ease the ftrace usage.
- Associated to trace-cmd, kernelshark tool proposes a trace viewer useful for analysing the traces.
- LTTng is an open source tracing framework for Linux partially based on ftrace, which also proposes a high level user interface through command line. We associate Trace Compass on Host PC side to a log viewer.
6. References[edit source]
- Useful external links
Document link | Document Type | Description |
---|---|---|
ftrace (kernel.org docs) | Standard | Documentation from Linux kernel sources |
Debugging the kernel using Ftrace - part1 | User Guide | http://lwn.net |
Debugging the kernel using Ftrace - part2 | User Guide | http://lwn.net |
Using the TRACE_EVENT() macro (with CREATE_TRACE_POINTS) | Training | http://lwn.net |
Load perf analysis using ftrace | User Guide | Linaro |