1. Article purpose[edit source]
The purpose of this article is to:
- briefly introduce the DSI peripheral and its main features
- indicate the level of security supported by this hardware block
- explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components
- explain, when necessary, how to configure the DSI peripheral.
2. Peripheral overview[edit source]
The DSI peripheral implements all the protocol functions defined in the MIPI® Display Serial Interface (MIPI® DSI) specification. It provides an interface to communicate with a DSI-compliant display. The MIPI® DSI is part of a group of communication protocols defined by the MIPI® Alliance [1].
2.1. Features[edit source]
Refer to the STM32MP15 reference manuals for the complete list of features.
Note that even if some MIPI DSI modes are supported by the DSI internal peripheral, in practice:
- software frameworks like U-Boot or Linux® kernel does not support all the possible modes.
- hardware integration constraints like the clock possible values or the pll configurations make difficult to use all possible modes.
Please consider the following recommandations when selecting a MIPI DSI panel or bridge for your project:
- Pixel data transmission
- in DSI command mode: not supported in U-Boot and in Linux® kernel. Please consider the DSI video mode instead.
- in DSI video mode:
- in burst mode: supported
- non-burst mode with sync events or pulses: supported but there are clock constraints to consider [2].
- Command transmission (initialization sequence, backlight...)
2.2. Security support[edit source]
The DSI is a non-secure peripheral.
3. Peripheral usage and associated software[edit source]
3.1. Boot time[edit source]
The DSI is used at boot time for displaying a splash screen thanks to the U-Boot framework [3].
3.2. Runtime[edit source]
3.2.1. Overview[edit source]
The DSI internal peripheral is allocated to the Arm® Cortex®-A7 non-secure core to be controlled in Linux® by the Linux DRM/KMS framework.
Chapter Peripheral assignment describes which peripheral instance can be assigned to which context.
3.2.2. Software frameworks[edit source]
Internal peripherals software table template
| Visual | DSI | | DRM/KMS framework | | |- |}
3.2.3. Peripheral configuration[edit source]
The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the STM32CubeMX tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article or for Linux® in the DSI device tree configuration article.
3.2.4. Peripheral assignment[edit source]
Internal peripherals assignment table template
| rowspan="1" | Visual | rowspan="1" | DSI | DSI | | ☐ | | |-
|}
4. How to go further[edit source]
Refer to the STM32 DSI application note (AN4860) [2] for a detailed description of the DSI peripheral and applicable use-cases.
Even if this application note is related to STM32 microcontrollers, it also applies to STM32 MPUs.
5. References[edit source]
- ↑ https://www.mipi.org MIPI® Alliance
- ↑ 2.0 2.1 2.2 2.3 DSI host on STM32 MCUs Application Note (AN4860)
- ↑ U-Boot framework