The table below contains some typical issues related to the DRM/KMS framework, as well as solutions or debugging methods.
If your issue is not listed, refer to the articles in the DRM/KMS or troubleshooting grids categories.
Symptom | Resolution |
---|---|
./myQtApplication Could not queue DRM page flip! (Permission denied) Could not queue DRM page flip! (Permission denied) |
The psplash-drm userland splash screen is running and is then the DRM master, avoiding other DRM applications to access to DRM/KMS. Please stop this psplash-drm application with the command below before running your use case: psplash-drm-quit Note: You may need to enter "export QT_QPA_EGLFS_ALWAYS_SET_MODE=1" before running your Qt application. For further information, refer to the Qt documentation. |
echo 32 > /sys/class/backlight/5a000000.dsi.0/brightness sh: write error: No such device or address |
On this board, the panel backlight is related to a MIPI® DSI panel. This backlight can be modified only if the panel is already powered on. That is probably not the case here. |
I/TC: Resumed E/TC:0 tzc_it_handler:79 TZC permission failure E/TC:0 dump_fail_filter:417 Overrun violation on filter 0 E/TC:0 dump_fail_filter:420 Permission violation on filter 0 E/TC:0 dump_fail_filter:425 Violation @0xdce1ff80, non-secure unprivileged read, AXI ID 403 E/TC:0 Panic at core/arch/arm/plat-stm32mp1/plat_tzc400.c:84 <tzc_it_handler> E/TC:0 TEE load address @ 0xde000000 |
This trace indicates that the TZC internal peripheral is detecting a "permission violation" made by the master whose AXI ID is 0x403. It corresponds to the LTDC internal peripheral (LTDC NSAID=0b0011, please refer to the STM32 reference manuals for details).
|