This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This article lists documents that apply to the STM32 MPU EcosystemRelease of the STM32MP15x lines . Those documents are generally referenced into other wiki pages.
All the resources for the STM32MP1 Series are located in the STM32MP1 Series web page.
Reference | Name | Link | |
---|---|---|---|
Application notes | |||
AN5031 | Getting started with STM32MP15 Series hardware development | AN5031.pdf | |
AN5109 | STM32MP15x lines using low-power modes | AN5109.pdf | |
AN5122 | STM32MP1 Series DDR memory routing guidelines | AN5122.pdf | |
AN5253 | Migration of microcontroller applications from STM32F4x9 lines to STM32MP151, STM32MP153 and STM32MP157 lines microprocessor | AN5253.pdf | |
AN5256 | STM32MP151, STM32MP153 and STM32MP157 discrete power supply hardware integration | AN5256.pdf | |
AN5260 | STM32MP151/153/157 MPU lines and STPMIC1B integration on a battery powered application | AN5260.pdf | |
AN5284 | STM32MP1 series system power consumption | AN5284.pdf | |
Datasheets[1] | |||
DS12505 | STM32MP157C/F datasheet (secure) |
DS12505.pdf | |
DS12504 | STM32MP157A/D datasheet (basic) |
DS12504.pdf | |
DS12503 | STM32MP153C/F datasheet (secure) |
DS12503.pdf | |
DS12502 | STM32MP153A/D datasheet (basic) |
DS12502.pdf | |
DS12501 | STM32MP151C/F datasheet (secure) |
DS12501.pdf | |
DS12500 | STM32MP151A/D datasheet (basic) |
DS12500.pdf | |
Errata sheets | |||
ES0438 | STM32MP15xx device errata | ES0438.pdf | |
Reference manuals[1] | |||
RM0436 | STM32MP157 reference manual (STM32MP157xxx advanced Arm®-based 32-bit MPUs) |
RM0436.pdf | |
RM0442 | STM32MP153 reference manual (STM32MP153xxx advanced Arm®-based 32-bit MPUs) |
RM0442.pdf | |
RM0441 | STM32MP151 reference manual (STM32MP151xxx advanced Arm®-based 32-bit MPUs) |
RM0441.pdf | |
Boards schematics | |||
MB1262 schematics | STM32MP157C-EV1 motherboard schematics MB1262-C01 board schematic (Evaluation board) |
MB1262-C01.pdf | |
MB1263 schematics | STM32MP157F-EV1 daughterboard schematics MB1263-C04 board schematic (Evaluation board) |
MB1263-C04.pdf | |
MB1230 schematics | DSI 720p LCD display daughterboard schematics MB1230-C02 board schematic (Evaluation board) |
MB1230-C02.pdf | |
MB1379 schematics | Camera daughterboard schematics MB1379-A01 board schematic (Evaluation board) |
MB1379-A01.pdf | |
MB1272 schematics | STM32MP157x-DKx motherboard schematics MB1272-DK2-C02 board schematic (Discovery kit) |
MB1272-C02.pdf | |
STM32MP157x-DKx motherboard schematics MB1272-DK2-C03 board schematic (Discovery kit) |
MB1272-C03.pdf | ||
MB1407 schematics | STM32MP157x-DKx daughterboard schematics MB1407-LCD-C01 board schematic (Discovery kit) |
MB1407-C01.pdf | |
STM32MP157x-DKx daughterboard schematics MB1407-LCD-C02 board schematic (Discovery kit) |
MB1407-C02.pdf | ||
Boards user manuals | |||
UM2534 | STM32MP157A-DK1 and STM32MP157C-DK2 Discovery kits user manual | UM2534.pdf | |
UM2535 | STM32MP157C-EV1 and STM32MP157A-EV1 Evaluation boards user manual | UM2535.pdf | |
UM2637 | STM32MP157D-DK1 and STM32MP157F-DK2 Discovery kits user manual | UM2637.pdf | |
UM2648 | STM32MP157F-EV1 and STM32MP157D-EV1 Evaluation boards user manual | UM2648.pdf | |
Tools user manuals |
- ↑ 1.0 1.1 The part numbers are specified in STM32MP15 microprocessor part numbers