This article explains step-by-step how to configure, create, and populate the serial NAND partitions with the right size, in order to boot from a serial NAND flash memory device (UBI format).
1. Introduction[edit source]
STM32MP157x-EV1 boards can boot from different storage devices (such as eMMC, SD card, parallel NAND flash memory or NOR flash memory).
Other external storage devices, present, for example, on the expansion board connected to STM32MP157x-EV1 board, can be chosen to boot from. In order to achieve this, some parameters in Yocto recipes must be modified to generate a functional image.
For NAND flash memory devices, UBIFS is the only filesystem supported by OpenSTLinux platform. This article explains step-by-step how to configure, create, and populate the serial NAND partitions with the right size, in order to boot from a serial NAND flash memory device (UBI format).
For demonstration purposes, this article takes the example of a serial NAND flash memory device, but it can be transposed to any NAND device.
To help you to understand this complex article, it is recommended to open, read, and analyze also the file available in the following OpenSTLinux distribution directory conf/machine/include.
The first step is to calculate the right size of serial NAND partitions. Then, based on these results, the UBIFS volume is created and populated.
2. How to calculate the size of serial NAND flash memory partitions[edit source]
This chapter aims at describing how to configure the serial NAND flash memory UBI partitioning to enable the board to boot from it.
Several partitions are defined for STM32MP157x-EV1 boards. The list can be found in the Flash partitions article.
In the whole article, the serial NAND flash memory, MT29F2G01ABA, is taken as an example.
This memory device has a size of 256 Mbytes. Stored partitions should be sized as shown in the table below. FBBL1, SSBL1, and SSBL2 sizes already take into account the default OpenSTLinux constraints, and are defined in a Linux® layer. The user can fine-tune these sizes to better fit his/her product, in st-machine-common-stm32mp.inc file:
Partition | Type | Content | Size |
---|---|---|---|
FSBL1 | raw | fsbl binaries | 512 Kbytes |
FSBL2 | raw | fsbl binaries | 512 Kbytes |
metadata1 | raw | metadata binaries | 512 Kbytes |
metadata2 | raw | metadata binaries | 512 Kbytes |
fip-a1 | raw | FIP binary | 4 Mbytes |
fip-a2 | raw | FIP binary | 4 Mbytes |
fip-b1 | raw | FIP binary | 4 Mbytes |
fip-b2 | raw | FIP binary | 4 Mbytes |
UBI | ubifs | multi volume UBI | UBI size (in Mbytes) |
The memory storage device stores all the boot stages as well as the UBI filesystem.
Boot stages include FSBL (first stage bootloader) and SSBL (second stage bootloader). The SSBL can be included into the FIP and is duplicated on the memory device.
The UBI size corresponding to this memory device is:
UBI size = SPI NAND size - (FSBL1 + FSBL2 + metada1 + metada2 + fip-a1 + fip-a2 + fip-b1 + fip-b2) UBI size for the example given = 256 Mbytes - (512 + 512 + 512 + 512 + 1024 * ( 4 + 4 + 4 +4) ) = 238 Mbytes
The following software parts must be stored in the multivolume UBI:
- uboot_config,
- uboot_config_r,
- bootfs,
- vendorfs,
- rootfs
- userfs.
Volume | Type | Content | Size |
---|---|---|---|
uboot_config | UBI | empty | 256 Kbytes |
uboot_config_r | UBI | empty | 256 Kbytes |
boot | ubifs | bootfs | 64 Mbytes |
vendorfs | ubifs | vendorfs | 16 Mbytes |
rootfs | ubifs | rootfs | Maximum available space |
userfs | ubifs | userfs | 16 Mbytes |
To take into account the small storage capacity of this memory device, the size of the userfs partition must be reduced from 128 Mbytes (default value in OpenSTLinux) to 16 Mbytes, in order to free more space for the rootfs partition.
To generate a UBI filesystem, some parameters must be set according to the storage device. The next chapters explain how to calculate these parameters.
2.1. Storage device characteristics[edit source]
In the serial NAND flash memory MT29F2G01ABA datasheet, the memory sizes are defined as follows:
- Memory device size: 256 Mbytes
- 2048 blocks
- Block size: 128 Kbytes
- Page size: 2048 bytes
2.2. Preamble : Variable naming[edit source]
The STM32MP157x-EV1 provided layers support several kinds of storage devices. Some share the same partition configuration regarding the size and partition type (for example eMMC and SD card), while others are different (for example parallel NAND flash memory devices). To be able to define and build everything at one time, the variables can be overloaded with a suffix.
It has been arbitrarily decided to use the following taxonomy: suffix :<memory device type>_<page size in Kbytes>_<block size expressed in Kbytes> .
In the chapters below, all the MT29F2G01ABA variables are named :spinand_2_128, for example EXTRA_UBIFS_SIZE:spinand_2_128.
2.3. Calculating the maximum size of the roofs partition[edit source]
The UBI is made of four partitions (bootfs, vendorfs, rootfs, userfs), two u-boot configuration parameters storage area (u-boot_config, u-boot_config_r), and some UBI overhead. The UBI overhead corresponds to some extra memory space, reserved to NAND flash memory driver, and which purpose is to handle the bad blocks.
In addition, for each UBIFS partition, this serial NAND flash memory uses several "extra blocks". The experience shows that each UBIFS can require an additional block. After booting the board, the final partition size is smaller than expected.
To generate the UBI layer, the exact size of each partition must be known. This means that, contrary to SD-card management, the rootfs size must be defined accurately to prepare NAND memory devices.
The maximal rootfs size can be calculated using the following formula: Max rootfs size = Multivolume UBI - (uboot_config + uboot_config_r + boots + vendorfs + userfs + UBI Overhead + FilesystemNumber * EXTRA_UBIFS_SIZE) where FilesystemNumber = 4 EXTRA_UBIFS_SIZE = size of all extra blocks
Below an explanation on how to calculate EXTRA_UBIFS_SIZE and the UBI overhead.
2.3.1. Defining EXTRA_UBIFS_SIZE value[edit source]
Generally speaking, when the UBI filesystem is generated, its size does not match the expected one, and it is smaller than expected. The size difference is almost the same on all partitions (such as userfs, rootfs).
To obtain the expected size for each filesystem (userfs, rootfs, ...), some extra blocks must be added to this expected size.
The number of extra blocks can be empirically determined.
The way to proceed is to define no extra blocks, generate the TSV, and flash it. Check the size of the filesystem, then restart to obtain the right filesystem size. See example below:
In st-machine-common-stm32mp.inc, add or modify the EXTRA_UBIFS_SIZE parameter and set it to 0:
EXTRA_UBIFS_SIZE:spinand_2_128 = "0"
Then generate the image and flash it.
Once the system has started, mount the partitions and compare their size with the requested size.
The Bootfs partition size is set in st-machine-common-stm32mp.inc to 64 Mbytes (67,108,864 bytes).
- bootfs partition
The Bootfs partition requested size is set in st-machine-common-stm32mp.inc to 64 Mbytes (67,108,864 bytes).
mkdir boot; mount -t ubifs ubi0:boot boot [ 308.695504] UBIFS (ubi0:2): Mounting in unauthenticated mode [ 308.700230] UBIFS (ubi0:2): background thread "ubifs_bgt0_2" started, PID 493 [ 308.723561] UBIFS (ubi0:2): start fixing up free space [ 320.387422] UBIFS (ubi0:2): free space fixup complete [ 320.404941] UBIFS (ubi0:2): UBIFS: mounted UBI device 0, volume 2, name "boot" [ 320.410797] UBIFS (ubi0:2): LEB size: 126976 bytes (124 Kbytes), min./max. I/O unit sizes: 2048 bytes/2048 bytes [ 320.420778] UBIFS (ubi0:2): FS size: 65773568 bytes (62 Mbytes, 518 LEBs), journal size 9023488 bytes (8 Mbytes, 72 LEBs) [ 320.431222] UBIFS (ubi0:2): reserved for root: 0 bytes (0 Kbyte) [ 320.437149] UBIFS (ubi0:2): media format: w4/r0 (latest is w5/r0), UUID B9AD3E8C-464F-4AD7-A9EA-C5BCB2AF0C4E, small LPT model
The above log shows that the booths partition size is only 65,773,568 bytes bytes. Additional space must be added to the bootfs partition size. This extra space is called "extra blocks" because it is defined as a number of blocks.
The formula to compute the number of extra blocks is:
extra blocks = (expected size in bytes - real size in bytes)/ memory block size in bytes extra blocks for the eg = (67,108,864 bytes - 65,773,568 bytes)/ (128*1024) = 10.1875
- vendorfs partition
The vendorfs partition requested size is set in st-machine-common-stm32mp.inc to 16 Mbytes (16,777,216 bytes).
mkdir vendorfs; mount -t ubifs ubi0:vendorfs vendorfs [ 496.605692] UBIFS (ubi0:3): Mounting in unauthenticated mode [ 496.610389] UBIFS (ubi0:3): background thread "ubifs_bgt0_3" started, PID 518 [ 496.627244] UBIFS (ubi0:3): start fixing up free space [ 497.105173] UBIFS (ubi0:3): free space fixup complete [ 497.122778] UBIFS (ubi0:3): UBIFS: mounted UBI device 0, volume 3, name "vendorfs" [ 497.129033] UBIFS (ubi0:3): LEB size: 126976 bytes (124 Kbytes), min./max. I/O unit sizes: 2048 bytes/2048 bytes [ 497.139010] UBIFS (ubi0:3): FS size: 15491072 bytes (14 Mbytes, 122 LEBs), journal size 9023488 bytes (8 Mbytes, 72 LEBs) [ 497.149456] UBIFS (ubi0:3): reserved for root: 0 bytes (0 Kbyte) [ 497.155237] UBIFS (ubi0:3): media format: w4/r0 (latest is w5/r0), UUID A506F102-49C4-413C-9ECA-484E04F311D8, small LPT model
The above log shows that the vendorfs partition size is only 15,491,072 bytes . Additional space must be added to the vendorfs partition size. This extra space is called "extra blocks" because it is defined as a number of blocks.
The formula to compute the number of extra blocks is:
extra blocks = (expected size in bytes - real size in bytes)/ memory block size in bytes extra blocks for the eg = (16,777,216 bytes - 15,491,072 bytes)/ (128*1024) = 9.8125
The same computation can be done on the rootfs partition to ensure that the number of extra blocks is correct.
Regarding the userfs partition, the number of extra blocks is more difficult to determine since the partition is extended when the board boots.
The EXTRA_UBIFS_SIZE parameter is common to all partitions and must be an integer. The EXTRA_UBIFS_SIZE must consequently be rounded to the smallest integer superior to the highest value between 9.81 and 10.19. As a result, for each partition, 11 extra blocks must be added:
Then, the parameter EXTRA_UBIFS_SIZE:spinand_2_128 is equal to 11 extrablocks multiplied by the size of a block (128 Kbytes). For OpenSTLinux distribution, the EXTRA_UBIFS_SIZE is then overloaded by EXTRA_UBIFS_SIZE:spinand_2_128
EXTRA_UBIFS_SIZE = ExtraBlockNumber * block size = 11 * 128 Kbytes = "1408"
This parameter can be defined in file st-machine-common-stm32mp.inc
EXTRA_UBIFS_SIZE:spinand_2_128 = "1408"
2.3.2. Calculating the UBI overhead size[edit source]
According to Linux MTD documentation[1], the UBI overhead is defined by the foliowng formula:
UBI overhead = (B - BB + 4) * SP + O * (P - B - 4) with * W - total number of physical erase blocks on the flash memory chip (NB: the entire chip, not the MTD partition); * P - total number of physical erase blocks on the MTD partition; * SP - physical erase block size; * SL - logical erase block size; * BB - number of bad blocks on the MTD partition; * BR - number of PEBs reserved for bad PEB handling (it is 20 * W/1024 for NAND by default, and 0 for NOR and other flash memory types, which do not have bad PEBs); * B - MAX(BR,BB); * O - the overhead related to storing EC and VID headers in bytes, that is O = SP - SL.
The UBI overhead corresponding to the NAND flash memory described in this article is (20*2048/1024 + 4) * 128 Kbytes + (128 Kbytes - 124 Kbytes) * (238 Mbytes/256 Kbytes - 20*2048/1024 - 4) = 9264 Kbytes
2.3.1. Calculating the maximum rootfs size[edit source]
As already explained above, the formula to calculate the maximal rootfs size is the following:
Max rootfs size = Multivolume UBI - (uboot_config + uboot_config_r + bootfs + vendorfs + userfs + UBI Overhead + PartitionsNumber * ExtraBlockNumber * Block size )
The maximum rootfs size corresponding to the NAND flash memory described in this article is 130000 Kbytes
In Yocto, the partition size is a expressed in Kbytes, which means that the previously calculated size must be divided by 1024, and only the integer part has to be kept. Then multiply the value by 1024:
rootfs size = trunc(Max rootfs size/ 1024)*1024
For the MT29F2G01ABA flash memory: trunc(130000 / 1024)*1024 = 129024 . So, in the machine configuration, STM32MP_ROOTFS_SIZE can be written like this:
STM32MP_ROOTFS_SIZE:spinand_2_128 ?= "129024"
Do not forget to specify the size of the userfs in the configuration files.
STM32MP_USERFS_SIZE:spinand_2_128 ?= "16384"
2.3.2. Configuring the partition sizes into Yocto layer[edit source]
The default values of all the partition sizes are defined in st-machine-common-stm32mp.inc:
STM32MP_BOOTFS_SIZE ?= "65536" STM32MP_USERFS_SIZE ?= "129024" STM32MP_VENDORFS_SIZE ?= "16384"
The userfs size for the MT29F2G01ABA can be set in the same file: STM32MP_USERFS_SIZE:spinand_2_128 ?= "16384"
This default parameter (STM32MP_USERFS_SIZE ) is overloaded by this new parameter STM32MP_USERFS_SIZE:spinand_2_128.
3. Creating the MultiUBI volume[edit source]
The OpenSTLinux image generated by ST embeds several UBIFS partitions. This is called the multiubi in ST Yocto configuration files. Only one UBI file can be downloaded into the board. This file must contain all volumes (uboot_config, uboot_config_r, boot, rootfs, vendorfs, userfs).
3.1. Generating automatically UBI and multiUBI volumes[edit source]
The UBI volume consists of a set of ubifs partitions and some binary files. The ubifs partitions used for creating the UBI volume are defined in conf/machine/include/st-machine-common-stm32mp.inc.
Ubifs partitions are generated in files that must be generated by the command "mkfs.ubifs" before creating the UBI volume.
The UBI volume is generated by using the ubinize command. This tool is a community development. Refer to manpage[2] for details.
The ubinize and "mkfs.ubifs" commands are executed by Yocto during the image generation process. The machine must be configured before (see chapter #How to calculate the size of serial NAND flash memory partitions. The following declarations must be added as follows in the configuration file (in st-machine-common-stm32mp.inc):
UBINIZE_ARGS:spinand_2_128 = "--min-io-size <page size> --peb-size <block size>" MKUBIFS_ARGS:spinand_2_128 = "--min-io-size <page size> --leb-size <LEBSize> --max-leb-cnt <BlockSize> --space-fixup" where BlockSize defined in NAND datasheet and LEBSize as explained below.
LEBSize value: UBI uses subpages to reduce flash memory space overhead. This overhead is reduced only if subpages can be used. The MT29F2G01ABA does not have subpages: UBI puts the VID header (volume identifier header) at a physical offset of 2048 (value defined in standard UBI[2]) and the LEB size consequently becomes 124 Kbytes (128 Kbytes minus one NAND page to store the EC header (erase counter header) and minus another NAND page for the VID header).
For the MT29F2G01ABA:
UBINIZE_ARGS:spinand_2_128 = "--min-io-size 2048 --peb-size 128 Kbytes" MKUBIFS_ARGS:spinand_2_128 = "--min-io-size 2048 --leb-size 126976 --max-leb-cnt 2048 --space-fixup"
4. How to improve the boot sequence for NAND memory device[edit source]
During the boot process, TF-A parses the flash memory device to find bootstage binaries. To avoid parsing the whole flash memory device, a default flash offset (also known as MTD offset) is defined, depending on the flash memory type and boot scheme.
- FIP
#ifndef STM32MP_NAND_FIP_OFFSET #define STM32MP_NAND_FIP_OFFSET U(0x00200000) #endif
- Legacy
#ifndef STM32MP_NAND_BASE_OFFSET #define STM32MP_NAND_BASE_OFFSET U(0x00200000) #endif
These default values may be not suitable for the flash memory, resulting in a timeout during the boot. To avoid the timeout, it is possible to specify the start offset.
To know the offset value, generate the tsv and retrieve the offset value for the first FIP binary.
#Opt Id Name Type IP Offset Binary - 0x01 fsbl1-boot Binary none 0x0 arm-trusted-firmware/tf-a-stm32mp157f-ev1-usb.stm32 - 0x03 fip-boot Binary none 0x0 fip/fip-stm32mp157f-ev1-trusted.bin P 0x04 fsbl1 Binary(2) nand0 0x00000000 arm-trusted-firmware/tf-a-stm32mp157f-ev1-nand.stm32 P 0x05 fip Binary nand0 0x00200000 fip/fip-stm32mp157f-ev1-trusted.bin P 0x06 fip2 Binary nand0 0x00600000 fip/fip-stm32mp157f-ev1-trusted.bin P 0x10 ubifs System nand0 0x00A00000 st-image-core-stm32mp-valid-stm32mp1_nand_4_256_multivolume.ubi
Then add this value to your machine configuration
TF_A_MTD_START_OFFSET_SPINAND = "0x00200000"
If you use the SDK to build TF-A, add STM32MP_FORCE_MTD_START_OFFSET=0x00200000 in the command line.
5. References[edit source]