This article explains how to experiment with ONNX Runtime [1] applications for image classification based on the MobileNet v1 model using TensorFlow Lite Python runtime.
1. Description[edit source]
The image classification[2] neural network model allows identification of the subject represented by an image. It classifies an image into various classes.
The application enables three main features :
- A camera streaming preview implemented using Gstreamer
- A NN inference based on the camera (or test data pictures) inputs is being ran by the TensorFlow Lite[3] interpreter
- A user interface implemented using Python GTK.
The performances depend on the number of CPUs available. The camera preview is limited to one CPU core where the TensorFlow Lite[3] interpreter is configured to use the maximum of the available resources.
The model used with this application is the MobileNet v1 downloaded from the Tensorflow Lite Hub[4].
2. Installation[edit source]
2.1. Install from the OpenSTLinux AI package repository[edit source]
After having configured the AI OpenSTLinux package you can install the X-LINUX-AI components for this application:
apt-get install tflite-cv-apps-image-classification-python
And restart the demo launcher:
- For OpenSTLinux distribution with a version lower than 4.0 use
systemctl restart weston@root
- For other OpenSTLinux distribution use :
systemctl restart weston-launch
2.2. Source code location[edit source]
The label_tfl.py Python script is available:
- in the Openembedded OpenSTLinux Distribution with X-LINUX-AI Expansion Package:
- <Distribution Package installation directory>/layers/meta-st/meta-st-stm32mpu-ai/recipes-samples/tflite-cv-apps/files/image-classification/python/label_tfl.py
- on the target:
- /usr/local/demo-ai/computer-vision/tflite-image-classification/python/label_tfl.py
- on GitHub:
3. How to use the application[edit source]
3.1. Launching via the demo launcher[edit source]
3.2. Executing with the command line[edit source]
The Python script label_tfl.py application is located in the userfs partition:
/usr/local/demo-ai/computer-vision/tflite-image-classification/python/label_tfl.py
It accepts the following input parameters:
usage: label_tfl.py [-h] [-i IMAGE] [-v VIDEO_DEVICE] [--frame_width FRAME_WIDTH] [--frame_height FRAME_HEIGHT] [--framerate FRAMERATE] [-m MODEL_FILE] [-l LABEL_FILE] [-e EXT_DELEGATE] [-p {std,max}] [--edgetpu] [--input_mean INPUT_MEAN] [--input_std INPUT_STD] [--validation] [--num_threads NUM_THREADS] options: -h, --help show this help message and exit -i IMAGE, --image IMAGE image directory with image to be classified -v VIDEO_DEVICE, --video_device VIDEO_DEVICE video device (default /dev/video0) --frame_width FRAME_WIDTH width of the camera frame (default is 320) --frame_height FRAME_HEIGHT height of the camera frame (default is 240) --framerate FRAMERATE framerate of the camera (default is 15fps) -m MODEL_FILE, --model_file MODEL_FILE .tflite model to be executed -l LABEL_FILE, --label_file LABEL_FILE name of file containing labels -e EXT_DELEGATE, --ext_delegate EXT_DELEGATE external_delegate_library path -p {std,max}, --perf {std,max} [EdgeTPU ONLY] Select the performance of the Coral EdgeTPU --edgetpu enable Coral EdgeTPU acceleration --input_mean INPUT_MEAN input mean --input_std INPUT_STD input standard deviation --validation enable the validation mode --num_threads NUM_THREADS Select the number of threads used by tflite interpreter to run inference
3.3. Testing with MobileNet V1[edit source]
The model used for test is the mobilenet_v1_0.5_128_quant.tflite downloaded from Tensorflow Lite Hub[4]
To ease launching of the Python script, two shell scripts are available:
- launch image classification based on camera frame inputs
/usr/local/demo-ai/computer-vision/tflite-image-classification/python/launch_python_label_tfl_mobilenet.sh
- launch image classification based on the pictures located in /usr/local/demo-ai/computer-vision/models/mobilenet/testdata directory:
/usr/local/demo-ai/computer-vision/tflite-image-classification/python/launch_python_label_tfl_mobilenet_testdata.sh
4. References[edit source]
- ↑ ONNX Runtime
- ↑ TFLite image classification overview
- ↑ 3.0 3.1 Cite error: Invalid
<ref>
tag; no text was provided for refs namedtensorflowlite_url
- ↑ 4.0 4.1 TFLite Hub
- ↑ Coral Edge TPU
- ↑ Wiki article image classification on EdgeTPU with TFlite python runtime