This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This page is a candidate for renaming (move). The requested new name is: How to transfer files to Discovery kit using Tera Term on Windows PC . The supplied reason is: Balance the verb complements better . -- Registered User (-) 09:38, 16 November 2022 (CET). Wiki maintainers: remember to update the pages that link this page before renaming (moving) it. |
The article is written as an extension to the article X-NUCLEO-NFC05A1 expansion board and X-NUCLEO-NFC06A1 expansion board. The purpose of this article is to specifically help users with steps to transfer any file from a Windows® PC to the STM32MP157C-DK2 Discovery kit using "Tera Term"[Ex1 1]. Download and install Tera Term on your Windows® PC and follow the steps listed below.
- Plug the power cable to power-up the STM32MP157C-DK2 .
- Connect the STM32MP157C-DK2 Discovery kit to your PC via a USB Micro-B cable through CN11.
- Check the Virtual COM port number visible in the device manager. For example, in the snapshot below, the COM port number is 14.
- Open Tera Term on your PC and select the COM port (as found in step 3 above). The baud rate must be 115200 bauds. The virtual terminal (remote access) is displayed as shown in the snapshot below.
- To transfer a file from the host PC to STM32MP157C-DK2 ,click on the File menu in the top-left corner of the Tera Term window and go to [File]>[Transfer]>[ZMODEM]>[Send]. Refer to the snapshot below.
- Select the file to be transferred from the pop-up window (see an example in the snapshot below) and click on the Open tab.
- A progress bar shows the file transfer status as shown in the snapshot below
Cite error: <ref>
tags exist for a group named "Ex1", but no corresponding <references group="Ex1"/>
tag was found