1. Article purpose[edit source]
This article explains how to configure the RNG using the device tree mechanism (DT), relying on the binding documentation, which is the description of the required and optional device-tree properties.
The peripheral can be assigned to different contexts and software components, depending on the final product needs. Refer to How to assign an internal peripheral to a runtime context article for guidelines on such configuration.
2. DT binding documentation[edit source]
The device tree binding documents are stored either in the given applicable components listed below, or in the Linux® kernel repository:
- TF-A BL2, OP-TEE, Linux® Kernel:
- RNG device tree bindings : Documentation/devicetree/bindings/rng/st,stm32-rng.yaml
3. DT configuration[edit source]
This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device-tree file organization.
STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.
3.1. DT configuration (STM32/SoC level)[edit source]
The RNG node is located in the device tree file for the software components, supporting the peripheral and listed in the above DT binding documentation paragraph.
It is only included on SoC supporting secure boot.
3.2. DT configuration (board level)[edit source]
This chapter explains how to enable and configure the RNG DT nodes for a board.
The peripheral configuration must be done in the specific board device tree files (board dts file).
RNG runs on two different clocks:
- The AHB bus clock to access registers
- A dedicated RNG clock connected to internal random blocks
Depending on the clock source selected for the RNG clocks, the RNG dedicated clock must be higher than AHB clock / 32 if clock error detection is enabled.
3.3. DT configuration examples[edit source]
&rng {
status = "okay";
clock-error-detect; // Enable the clock error management
};
4. How to configure the DT using STM32CubeMX[edit source]
The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
STM32CubeMX might not support all the properties described in the DT binding files listed in the above DT binding documentation paragraph. In such cases, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties; They are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.
5. References[edit source]
Refer to the following links for additional information: