This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. STM32DDRFW-UTIL overview[edit source]
This article describes STM32DDRFW-UTIL, an official STMicroelectronics firmware package for DDR configuration and test on STM32MP1 Series.
1.1. Applicability[edit source]
The STM32DDRFW-UTIL applies to STM32MP13x lines and STM32MP15x lines
.
1.2. Package overview[edit source]
STM32DDRFW-UTIL firmware is a software package containing multiple STM32CubeIDE projects applicable for all STM32 MPU products with a DDR which includes:
- BSP, CMSIS and HAL drivers for all applicable STM32MPxxx series
- DDR_Tool full source code with:
- Common directory with general purpose content
- Tool directory with tool core and tests
- STM32CubeIDE Projects for all ST supported boards
- Binaries for all supported ST boards with BootROM image header to be programmed directly into SDCARD or loaded via STM32CubeProgramer without using STM32CubeIDE tool.
- README.md document for help
1.3. README.md[edit source]
The README.md, included in the package, is a complete document that describes:
- the Software architecture and design of STM32DDRFW-UTIL.
- how to use the STM32DDRFW-UTIL firmware package for DDR configuration and test on STM32MP1 Series MPUs.
2. How to get STM32DDRFW-UTIL[edit source]
Refer to the following link to find STM32DDRFW-UTIL firmware package.