1. Article purpose[edit source]
The purpose of this article is to explain how to configure the analog-to-digital converter ADC internal peripheral using the device tree mechanism which provides a hardware description of the ADC peripheral, an in particular:
- how to configure the ADC peripheral
- how to configure the board, e.g. the ADC voltage reference regulator, channels, pins and sampling time.
The device tree to configure depends on the context/component to which the ADC peripheral is assigned:
- For boot time:
- U-Boot: in that case, the peripheral driver is used in this component.
- For runtime:
- Linux® OS: in that case, peripheral driver is registered to the IIO framework.
To assign the peripheral to another execution context, refer to How to assign an internal peripheral to a runtime context article for guidelines on peripheral assignment .
2. DT bindings documentation[edit source]
Whatever the context/component, the binding documents are stored in each applicable components:
- For boot time
- U-Boot:
- For runtime
3. DT configuration[edit source]
This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device tree file split.
The STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.
![](/stm32mpu-ecosystem-v4/nsfr_img_auth.php/7/74/ADC_DT_configuration.png)
3.1. DT configuration (STM32/SoC level)[edit source]
On STM32MP13x lines The ADC nodes are declared in
stm32mp131.dtsi[1] and in
stm32mp133.dtsi[2].
On STM32MP15x lines The ADC nodes are declared in stm32mp151.dtsi[3].
- DT root node ('adc') describes the ADC hardware block parameters such as register areas, clocks and interrupts.
- DT child nodes ('adc1' and/or 'adc2') describe ADC1 and/or ADC2 independently.
adc: adc@address { compatible = "st,stm32mp1-adc-core"; ... /* common resources in 'adc' root node. */ adc1: adc@0 { compatible = "st,stm32mp1-adc"; ... /* private resources in 'adc1' child node. */ }; adc2: adc@100 { compatible = "st,stm32mp1-adc"; ... /* private resources in 'adc2' child node. */ }; };
3.2. DT configuration (board level)[edit source]
Follow the sequences described in the below chapters to configure and enable the ADC on your board.
The objective of this chapter is to explain how to enable and configure the ADC internal peripheral DT nodes for a board. This board DT is overloaded on top of the SoC DT. It is usually composed of several DT files: at least one "board" dts file, that includes the "SoC" dtsi file, plus one or several other dts files.
3.2.1. Common resources for all ADCs[edit source]
The DT root node ('adc') must be filled in:
- Enable the ADC block by setting status = "okay".
- Configure the pins in use via pinctrl, through pinctrl-0 and pinctrl-names.
- Configure the analog supply voltage regulator[4] by setting vdda-supply = <&your_vdda_regulator>.
- Configure the analog reference voltage regulator[4] by setting vref-supply = <&your_vref_regulator>.
The DT child nodes ('adc1' and/or 'adc2') must be filled in with ADC block properties and channels properties.
3.2.2. Resources dedicated to an ADC block[edit source]
3.2.2.1. ADC block properties[edit source]
- Enable ADC block by setting status = "okay".
- Set ADC block resolution by setting assigned-resolution-bits = <12> (optional).
3.2.2.2. Channel properties (for ecosystem release ≥ v3.1.0 )[edit source]
Each channel is described by a dedicated DT sub node, filled in with properties documented in Generic IIO bindings for ADC channels[6].
- Define channel index 'x' by setting reg = <x>.
- Identifiy the channel by setting its name with label = "xxx" (optional).
Reserved label "vrefint", "vddcore" and "vbat" allow to identify internal channels. - Enable differential channel pair (<vinp vinn>) by setting diff-channels = <x y> (optional).
- Set the minimum sampling time st,min-sample-time-nsecs by setting st,min-sample-time-nsecs = <10000> (optional).
3.2.2.3. Legacy channel properties (for ecosystem release ≤ v3.0.0 )[edit source]
These properties are deprecated, but are still supported for backward compatibility. The properties introduced in v3.1.0 should be used instead, whenever possible.
- Enable single-ended channel(s) (<vinp...>) by setting st,adc-channels = <0 1 2...>.
- Enable differential channel(s) pairs (<vinp vinn>, ...) by setting st,adc-diff-channels = <1 0>, <2 6>, ....
- Set the minimum sampling time [7] for each or all channels by setting st,min-sample-time-nsecs = <10000> (optional).
3.3. DT configuration example[edit source]
The example below shows how to configure ADC1:
- Input pin: use Pinctrl device tree configuration to configure PF12 as analog input.
- Analog supply: it is provided by one of the PMIC LDO regulators.
- Voltage reference: it is provided by the VREFBUF internal regulator.
- Input channel: configure ADC1_IN6 (e.g on PF12).
- Sampling time: the minimum sampling time is 10 µs.
# part of pin-controller dt node adc1_in6_pins_a: adc1-in6 { pins { pinmux = <STM32_PINMUX('F', 12, ANALOG)>; /* configure 'PF12' as ANALOG */ }; };
3.3.1. For ecosystem release ≥ v3.1.0[edit source]
&adc { /* ADC1 & ADC2 common resources */ pinctrl-names = "default"; pinctrl-0 = <&adc1_in6_pins_a>; /* Use PF12 pin as ANALOG */ vdda-supply = <&vdda>; /* Example to supply vdda pin by using a PMIC regulator vref-supply = <&vrefbuf>; /* Example to use VREFBUF (It needs to be enabled as well) */ status = "okay"; /* Enable ADC12 block */ adc1: adc@0 { /* private resources for ADC1 */ status = "okay"; /* Enable ADC1 */ channel@6 { reg = <6>; /* ADC1 in6 channel is used */ st,min-sample-time-nsec = <10000>; /* 10µs sampling time */ }; }; adc2: adc@100 { /* private resources for ADC2 */ ... }; };
3.3.2. For ecosystem release ≤ v3.0.0[edit source]
&adc { /* ADC1 & ADC2 common resources */ pinctrl-names = "default"; pinctrl-0 = <&adc1_in6_pins_a>; /* Use PF12 pin as ANALOG */ vdda-supply = <&vdda>; /* Example to supply vdda pin by using a PMIC regulator vref-supply = <&vrefbuf>; /* Example to use VREFBUF (It needs to be enabled as well) */ status = "okay"; /* Enable ADC12 block */ adc1: adc@0 { /* private resources for ADC1 */ st,adc-channels = <6>; /* ADC1 in6 channel is used */ st,min-sample-time-nsecs = <10000>; /* 10µs sampling time */ status = "okay"; /* Enable ADC1 */ }; adc2: adc@100 { /* private resources for ADC2 */ ... }; };
4. How to configure the DT using STM32CubeMX[edit source]
The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.
5. References[edit source]
For additional information, refer to the following links:
- ↑ STM32MP131 device tree file
- ↑ STM32MP133 device tree file
- ↑ STM32MP151 device tree file
- ↑ 4.0 4.1 4.2 Regulator overview
- ↑ VREFBUF internal peripheral
- ↑ Documentation/devicetree/bindings/iio/adc/adc.yaml , Generic IIO bindings for ADC channels
- ↑ How to get the best ADC accuracy in STM32, by STMicroelectronics