This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Overview[edit source]
media-ctl is a V4L2 utility[1] allowing to setup and configure the camera subsystem subdevices. It is based on Media Controller Linux kernel interface[2].
2. Usage[edit source]
media-ctl --help
media-ctl [options] -d, --device dev Media device name (default: /dev/media0) If <dev> starts with a digit, then /dev/media<dev> is used. If <dev> doesn't exist, then find a media device that reports a bus info string equal to <dev>. -e, --entity name Print the device name associated with the given entity -V, --set-v4l2 v4l2 Comma-separated list of formats to setup --get-v4l2 pad Print the active format on a given pad --get-dv pad Print detected and current DV timings on a given pad --set-dv pad Configure DV timings on a given pad -h, --help Show verbose help and exit -i, --interactive Modify links interactively -l, --links links Comma-separated list of link descriptors to setup --known-mbus-fmts List known media bus formats and their numeric values -p, --print-topology Print the device topology. If an entity is specified through the -e option, print information for that entity only. --print-dot Print the device topology as a dot graph -r, --reset Reset all links to inactive -v, --verbose Be verbose Links and formats are defined as links = link { ',' link } ; link = pad '->' pad '[' flags ']' ; pad = entity ':' pad-number ; entity = entity-number | ( '"' entity-name '"' ) ; v4l2 = pad '[' v4l2-properties ']' ; v4l2-properties = v4l2-property { ',' v4l2-property } ; v4l2-property = v4l2-mbusfmt | v4l2-crop | v4l2-interval | v4l2-compose | v4l2-interval ; v4l2-mbusfmt = 'fmt:' fcc '/' size ; { 'field:' v4l2-field ; } { 'colorspace:' v4l2-colorspace ; } { 'xfer:' v4l2-xfer-func ; } { 'ycbcr-enc:' v4l2-ycbcr-enc-func ; } { 'quantization:' v4l2-quant ; } v4l2-crop = 'crop:' rectangle ; v4l2-compose = 'compose:' rectangle ; v4l2-interval = '@' numerator '/' denominator ; rectangle = '(' left ',' top, ')' '/' size ; size = width 'x' height ; where the fields are entity-number Entity numeric identifier entity-name Entity name (string) pad-number Pad numeric identifier flags Link flags (0: inactive, 1: active) fcc Format FourCC width Image width in pixels height Image height in pixels numerator Frame interval numerator denominator Frame interval denominator v4l2-field One of the following: any none top bottom interlaced seq-tb seq-bt alternate interlaced-tb interlaced-bt v4l2-colorspace One of the following: default smpte170m smpte240m rec709 unknown 470m 470bg jpeg srgb oprgb bt2020 raw dcip3 v4l2-xfer-func One of the following: default 709 srgb oprgb smpte240m none dcip3 smpte2084 v4l2-quant One of the following: default full-range lim-range
3. Examples[edit source]
Refer to V4L2 camera subsystem setup for examples of usage.
4. References[edit source]