1. Debug with console[edit source]
See U-Boot Documentation or doc/README.log for U-Boot logging details.
CONFIG_LOG is enable in OpenSTLinux.
By default, the traces are available on the U-Boot console which use stdout-path
defined in the chosen
node of the Linux kernel device tree as described in the Linux kernel binding[1].
See page How to configure U-Boot for your board for configuration details.
The ST boards use the default logging configuration:
- CONFIG_LOG_DEFAULT_LEVEL = CONFIG_LOG_MAX_LEVEL = 6 (LOGL_INFO), the 'debug' macros used by U-Boot (log_debug(), debug(), pr_debug()...) are removed in the U-Boot binary.
- CONFIG_LOGF_FILE, CONFIG_LOGF_LINE, CONFIG_LOGF_FUNC are not activated: not debug information in log messages by default.
To activate all the debug traces in U-Boot you need to set the default logging level - e.g. set CONFIG_LOG_DEFAULT_LEVEL to 7 (LOGL_DEBUG), with a major impact on U-Boot size.
When the traces are present in U-Boot, you can change the default trace level with CONFIG_LOG_DEFAULT_LEVEL or you can use the log
command (CONFIG_CMD_LOG) to dynamically configure and filter the output:
log level 7 log format all
1.1. Activate debug trace on one file[edit source]
To turn on this debug logging just in one file, you can define LOG_DEBUG for this file
- add define before any include in the <file>.c file
#define LOG_DEBUG
- with a Makefile
CFLAGS_<file>.o+= -DLOG_DEBUG
1.2. Debug before console[edit source]
If U-Boot fails before the console configuration (in the first stage of U-Boot execution), trace is not available.
In this case, you need to:
- debug with GDB (see the next chapter)
or,
- activate the debug UART feature:
- add in defconfig of U-Boot configuration
- CONFIG_DEBUG_UART
- CONFIG_DEBUG_UART_STM32
- adapt the function board_debug_uart_init(): that configures the required resources (pad, clock) before initialization by the U-Boot driver.
This function needs to be adapted for your board.
- add in defconfig of U-Boot configuration
2. Debug with GDB[edit source]
With OpenSTLinux, you can directly use GDB script Setup.gdb:
Or for manual GDB connection, you need to:
- get the elf files for U-Boot =
u-boot
available in the build directory - connect GDB to the target
- reset with attach the target with the gdb "monitor reset halt" command:
execution is stopped in ROM code or at the beginning of FSBL execution. - load the symbols of the binary to be debugged with commands available in next chapter:
#Load U-Boot symbol - start execution with the "continue" command
2.1. Load U-Boot symbol[edit source]
With U-Boot relocation, symbols are more difficult to load.
See https://www.denx.de/wiki/DULG/DebuggingUBoot
If you connect GDB on running target, you can load the debug symbols:
- Before relocation with "symbol-file" command:
symbol-file u-boot
- After relocation with "add-symbol-file" command to relocate the symbol with the code offset = gd->relocaddr:
symbol-file u-boot --> only for "gd_t" definition set $offset = ((gd_t *)$r9)->relocaddr --> get relocation offset symbol-file --> clear previous symbol add-symbol-file u-boot $offset
The following GDB example script automatically loads the U-Boot symbol before and after relocation for a programmed board, after "monitor reset halt" command:
thbreak *0xC0100000 commands > symbol-file u-boot > thbreak relocate_code > commands > print "RELOCATE U-Boot..." > set $offset = ((gd_t *)$r9)->relocaddr > print $offset > symbol-file > add-symbol-file u-boot $offset > thbreak boot_jump_linux > continue > end > continue > end
This script uses a temporary hardware breakpoint "thbreak" to load the symbol when U-Boot code is loaded in DDR by FSBL = TF-A at the U-Boot entry point, CONFIG_SYS_TEXT_BASE =
It allows the symbol to be loaded only when code is executed to avoid DDR access before DDR initialization.
3. References[edit source]
- ↑ Documentation/devicetree/bindings/chosen.txt the Linux kernel binding for chosen node