1. Article purpose[edit source]
The purpose of this article is to explain how to secure an STM32 MPU-based platform thanks to several hardware mechanisms, and to briefly introduce the software components responsible for the secure configuration.
2. Firewall[edit source]
MPU firewalls comprise access filters for MPU peripherals and subsystems memory mapped interfaces, internal RAMs/ROMs and external memory (DDR). Depending on the assignment, an MPU interface can be dedicated or shared between several hardware execution context(s).
2.1. STM32MP1 firewall[edit source]
- ETZPC:
- assigns access rights to MPU peripherals from Cortex-A7 contexts (secure or normal) and Cortex-M4 context.
- assigns access rights to internal ROM/RAM from Cortex-A7 and Cortex-M4.
- TZC: assigns access rights to DDR regions.
- RCC: can restrict the access of some of its registers to the secure execution context.
- PWR: can restrict the access of some of its registers to the secure execution context.
- BSEC: The OTP memory can be fused to restrict the access to some of its content to the secure execution context.
- RTC: This MPU interface can restrict some of its interface registers to the secure execution context.
- GPIO: GPIO bank Z can be configured to restrict some GPIO configuration to the secure execution context.
- TAMP: can restrict the access of some of its registers to the secure execution context.
- EXTI: can restrict the access of some of its registers to the secure execution context.
- GIC: can restrict the access of some of its registers to the secure execution context.
- MDMA: can configure MDMA interrupt execution context.
3. Secure debug[edit source]
The STM32 MPU offers the possibility to manage the platform debug configuration.
It is indeed possible to enable/disable independently secure and non-secure debug accesses.
3.1. STM32MP1 secure debug[edit source]
Debug accesses are controlled through BSEC peripheral.
By default, the STM32 MPU is started by the ROM code with both secure and non-secure debug enabled.
When the trusted boot is enabled, the ROM code disables debug accesses and relies on secure OS to configure them.
When a FSBL debug is required, a dedicated wrapper exists (that can be also signed) to open the debug.
4. Secure and non-secure worlds[edit source]
Thanks to Arm® TrustZone, some portions of the executing code can be assigned to a non-secure world or to a secure world.
The secure world offers an isolated context that guarantee code and data integrity up to the hardware support. The secure world can be used to host a Trusted Execution Environment (TEE) that executes in parallel with the rich OS and provides secure services.
The firmware and more generally software executing in secure world implicitly use the TrustZone(r) NS signal/bit to be granted access to sensitive resources. These resources can be DDR locations, SoC peripheral interfaces or SoC internal resources such as clocks, debug facilities, and more.
4.1. TF-A SP_MIN runtime services[edit source]
The TF-A configuration supports the installation of a minimal runtime secure service provider and peripheral access control with firewall. This runtime firewall is built from TF-A BL32 SP_MIN image.
Run time services provided by TF-A includes not restricted to, PSCI controls, SCMI resources, some SiP & OEM SMCCC services for power states transition and other platform facilities.
4.2. OP-TEE OS runtime services[edit source]
The OP-TEE is recommended by STMicroelectronics as it is an open source TEE solution. The package provides additional secure services to the platform since it can host core secure services and run trusted applications. OP-TEE provides the same level of services as TF-A listed above: PSCI, SCMI, SiP & OEM SMCCC. OP-TEE provides other high level services, such as running trusted applications and possibly generic services used by standard non-secure components such as random number generation.
5. Security frameworks[edit source]
The platform non-secure world accesses to specific resources using generic frameworks. These operations are used to managed overall systems and must be implemented inside the TEE.
These accesses are using the SMC Calling convention [1]
Identifier | Name | Description |
---|---|---|
0x84000000-0x8400001F | PSCI 32-bit calls | 32-bit Power Secure Control Interface |
0x82000000-0x8200FF00 | SiP Service Calls | Interfaces to SoC implementation-specific services |
5.1. PSCI[edit source]
PSCI[2] manages the power state of the CPU and the overall system. This framework is an Arm® generic implementation targeting CPU related power management services among which secondary CPUs boot up, dynamic addition and removal of CPUs, CPU idle management and system shutdown and reset.
5.1.1. STM32MP1 PSCI support[edit source]
Both TF-A SP_MIN and OP-TEE implement PSCI v1.1 [3] and offer standard services for:
- Core idle management
- Boot up for secondary boot core
- Dynamic addition and removal of cores
- System shutdown and reset
5.2. SCMI[edit source]
The SCMI[4] specification defines a standard to access resources for power, performance and system management. This framework is an Arm® generic implementation.
SCMI protocols can be used to create device interfaces for external resource that are controlled by a SCMI server implementation. Targeted devices are of, not limited to:
- Power domain management
- Performance management
- Clock management
- Sensor management
- Reset controller management
The SCMI specification does not specify the SMC IDs to use. It relies on specific OEM IDs.
5.2.1. STM32MP1 SCMI support[edit source]
See the specific article on SCMI overview. It presents SCMI used by the secure world (TF-A SP_MIN, OP-TEE) to expose system resources, as input source clocks and PLL output clocks, reset controllers to non-secure world (U-Boot bootloader, Linux kernel).
5.3. Platform SiP and OEM SMCCC services[edit source]
5.3.1. STM32MP1[edit source]
The STM32MP1 embeds SiP and OEM SMCCC services for non-secure world to access low-power transition facilities, clock calibration facilities, BSEC OTP access, possibly also some test facilities. Both TF-A and OP-TEE implement the same level of services aside possible test facilities.
Identifier | Name | Description |
---|---|---|
0x82001000 | RCC | Access restricted to CIER/CIFR registers |
0x82001001 | PWR | Access restricted to CR3/WKUPCR/MPUWKUPENR registers |
0x82001002 | RCC Calibration | Secure services to start a HSI or CSI calibration |
0x82001003 | BSEC | Secure service to access OTP (read/write/programmation) |
0x82001008 | PD_DOMAIN | Access to program the power domain for low-power management |
0x82001009 | RCC OPP | Access to program CPU frequency |
0x82002000 | SCMI_AGENT0 | Access to SCMI services Channel 0 |
0x82002001 | SCMI_AGENT1 | Access to SCMI services Channel 1 (MCKPROT Resources) |
6. Security peripherals[edit source]
6.1. Cryptographic hardware acceleration[edit source]
The STM32 MPU embeds multiple peripherals for cryptographic acceleration:
6.2. Trusted platform module (TPM)[edit source]
The STM32 MPU can be associated to an external trusted platform module (TPM).
It provides secret data storage capabilities as well as cryptographic capabilities allowing to use them.
6.3. Tamper event detection[edit source]
The STM32 MPU embeds internal and external tampers detections mechanisms. They can be used to detect physical attack, out-of-spec voltage, etc. A tamper detection will result in the automatic clearing of sensitive data in the system: it is a key feature for security product.
6.3.1. STM32MP1[edit source]
The tamper configuration is described in STM32MP15 Tamper configuration.
7. Secure Secret Provisioning[edit source]
The STM32 MPU allows secrets to be provisioned in BSEC fuses in a secure way. This is the Secure Secret Provisioning (SSP) feature.
This feature is a secure process which runs between the software programmer (including a HSM), the ROM code and a customized TF-A BL2. The security relies on the chip attestation and a package encryption exchange between the programmer and the STM32 MPU.
This feature is fully describes in the AN5510: Overview of the secure secret provisioning (SSP) on STM32MP1 Series.
7.1. Fuses provisioning in STM32MP1[edit source]
The build process for the TF-A SSP firmware is described here.
8. References[edit source]