1. Article purpose[edit source]
The purpose of this article is to:
- briefly introduce the SPI peripheral and its main features
- indicate the level of security supported by this hardware block
- explain how each instance can be allocated to the runtime contexts and linked to the corresponding software components
- explain, when necessary, how to configure the SPI peripheral and for some of them the I2S features.
2. Peripheral overview[edit source]
The SPI peripheral can be used to communicate with an external devices using the SPI (Serial Peripheral Interface).
A subset of the SPI instances supports the I2S audio protocol. These SPI/I2S peripherals can alternatively be used in audio applications, when they are configured as an I2S interface. Refer to peripheral assignment chapter to check I2S feature support for each SPI instance.
2.1. Features[edit source]
2.1.1. SPI main features[edit source]
- Full-duplex, half-duplex and simplex synchronous modes.
- Slave and master modes.
2.1.2. I2S main features[edit source]
Only available for SPI supporting I2S mode.
- Full-duplex or simplex modes.
- Slave and master modes.
- Four audio protocols supported.
2.1.3. Specific features[edit source]
Some of the SPI peripheral characteristics depend on I2S support, as summarized in following table:
SPI modes/features | I2S supported | I2S not supported |
---|---|---|
Rx & TxFIFO size (N) [x 8-bit] | 16 | 8 |
Maximum configurable data size [bits] | 32 | 16 |
Refer to STM32MP13 reference manuals or STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to see which features are implemented.
2.2. Security support[edit source]
2.2.1. On STM32MP13x lines
[edit source]
There are five SPI instances:
- SPI4 and SPI5 are secure peripheral (under ETZPC control)
- The other SPI instances are non-secure peripherals
2.2.2. On STM32MP15x lines
[edit source]
There are six I2C instances:
- SPI6 is a secure peripheral (under ETZPC control)
- The other SPI instances are non-secure peripherals
3. Peripheral usage and associated software[edit source]
3.1. Boot time[edit source]
The SPI is not used at boot time.
3.2. Runtime[edit source]
3.2.1. Overview[edit source]
The secure instances can be allocated to:
- the Arm® Cortex®-A7 secure core. Notice that the SPI OP-TEE driver is not available in OpenSTLinux distribution yet.
All the SPI instances can be allocated to:
- the Arm® Cortex®-A7 non-secure core to be controlled in Linux® by:
- the SPI framework for SPI configured in SPI mode
- the ALSA framework for SPI configured in I2S mode
- the Cortex-M4 to be controlled in STM32Cube MPU Package by STM32Cube SPI driver
Chapter Peripheral assignment describes which peripheral instance can be assigned to which context.
3.2.2. Software frameworks[edit source]
Internal peripherals software table template
| Low speed interface | SPI | OP-TEE SPI driver | Linux SPI framework | STM32Cube SPI driver | SPI configured in SPI mode
The OP-TEE SPI driver is not yet available |- | Audio | SPI | | Linux ALSA framework | STM32Cube SPI driver | SPI configured in I2S mode
Only for SPI supporting I2S feature |- |}
3.2.3. Peripheral configuration[edit source]
The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration by itself can be done via STM32CubeMX tool for all internal peripheral, then it can manually be completed (especially for external peripherals) according to the information given in the corresponding software framework article.
When the Arm® Cortex®-A7 core operates in non-secure access mode, the SPI is controlled by the Linux kernel framework.
- SPI mode:
Refer to SPI framework to check how to drive SPI through Linux kernel.
- I2S mode:
Refer to I2S Linux driver to drive the SPI through Linux kernel ALSA framework. Refer to Soundcard configuration to configure it through the Linux kernel device tree[1].
3.2.4. Peripheral assignment[edit source]
Internal peripherals assignment table template
| rowspan="6" | Low speed interface
or
audio | rowspan="6" | SPI | SPI2S1 | | ☐ | ☐ | Assignment (single choice) |- | SPI2S2 | | ☐ | ☐ | Assignment (single choice) |- | SPI2S3 | | ☐ | ☐ | Assignment (single choice) |- | SPI4 | | ☐ | ☐ | Assignment (single choice) |- | SPI5 | | ☐ | ☐ | Assignment (single choice) |- | SPI6 | ☐ | ☐ | | Assignment (single choice) |-
|}
4. References[edit source]