STM32MP13 TAMP internal peripheral

Revision as of 09:08, 13 October 2021 by Registered User
Applicable for STM32MP13x lines

Warning white.png Warning
Not yet updated for STM32MP13

1. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the TAMP peripheral and its main features
  • indicate the level of security supported by this hardware block
  • explain how it can be allocated to the three runtime contexts and linked to the corresponding software components
  • explain, when necessary, how to configure the TAMP peripheral.

2. Peripheral overview[edit source]

The TAMP peripheral is used to prevent any attempt by an attacker to perform an unauthorized physical or electronic action against the device. It also includes the backup registers that remain powered-on when the platform is switched off.

Info white.png Information
It is important to notice that the backup registers and the BKPSRAM internal memory can be erased when a tamper detection occurs in TAMP internal peripheral

2.1. Features[edit source]

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to see which features are implemented.

2.2. Security support[edit source]

The TAMP is a secure peripheral. The access to some backup registers can be opened to the non-secure world via a direct configuration in TAMP, in secure mode.

3. Peripheral usage and associated software[edit source]

3.1. Boot time[edit source]

The TAMP is used at boot time to share data between the ROM code, FSBL and SSBL: see backup registers for further information.

3.2. Runtime[edit source]

3.2.1. Overview[edit source]

TAMP is seen as a system peripheral, that can be used by the Arm® Cortex®-A7 secure context with OP-TEE or the Arm® Cortex®-A7 non-secure context with Linux.

3.2.2. Software frameworks[edit source]

Internal peripherals software table template

| Security
| TAMP
| OP-TEE
| Linux syscon framework[1]
|
|
|-
|}


For the Linux kernel configuration, sysconf part, please refer to TAMP device tree configuration.
For the secure configuration, please refer to TAMP device tree configuration and Tamper configuration.

3.2.3. Peripheral configuration[edit source]

The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the STM32CubeMX tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article.

3.2.4. Peripheral assignment[edit source]

Internal peripherals assignment table template

| rowspan="1" | Security
| rowspan="1" | TAMP
| TAMP
| 
| 
|
|
|-
|}

4. How to go further[edit source]

5. References[edit source]