1. Article purpose[edit source]
The purpose of this article is to explain how to configure the timer (TIM)[1] when the peripheral is assigned to Linux® OS:
- Configuring the timer peripheral to enable PWM, trigger or quadrature encoder.
- Configuring the board, e.g. TIM pins.
The configuration is performed using the device tree mechanism[2].
It is used by the TIM Linux driver that registers relevant information in PWM, IIO and counter frameworks.
If the peripheral is assigned to another execution context, refer to How to assign an internal peripheral to a runtime context article for guidelines on peripheral assignment and configuration.
2. DT bindings documentation[edit source]
The TIM internal peripheral[1] is a multifunction device (MFD).
- st,stm32-timers deals with core resources. (e.g. registers, clock, DMAs)
Each function is represented by a separate compatible string:
- st,stm32-pwm deals with PWM resources. (e.g. PWM input/output pins)
- st,stm32-timer-trigger deals with trigger resources (e.g. trigger output connected to other STM32 internal peripherals)
Each function is represented by a separate DT binding document:
- STM32 TIM MFD device tree bindings[3] document deals with core resources (e.g. registers, clock, DMAs)
- st,stm32-timer-counter deals with quadrature encoder resources and external events counter.
- STM32 TIM PWM device tree bindings[4] document deals with PWM resources (e.g. PWM input/output pins)
- st,stm32-timer-timer deals with clock sources.
- STM32 TIM IIO trigger device tree bindings[5] document deals with other internal peripheral triggering resources
The required and optional configuration properties of these function are documented in STM32 TIM MFD device tree bindings[6]
- STM32 TIM quadrature encoder device tree bindings[7] document deals with quadrature encoder resources
3. DT configuration[edit source]
This hardware description is a combination of both STM32 microprocessor and board device tree files. Refer to Device tree for more explanations about device tree file split.
The STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.
3.1. DT configuration (STM32 level)[edit source]
TIM nodes are declared in stm32mp151.dtsi[8].
DT root node (e.g. timers1...) and DT child nodes describe the TIM features such as:
- PWM
- trigger and quadrature encoder
They also describe hardware parameters such as registers address, clock and DMA.
timers1: timer@address { /* timer common resources */ compatible = "st,stm32-timers"; ... pwm { /* PWM*/ compatible = "st,stm32-pwm"; }; timer@0 { compatible = "st,stm32h7-timer-trigger"; /* trigger identifier (e.g. 0 for TIM1 triggers, 1 for TIM2... */ reg = <0>; }; counter { compatible = "st,stm32-timer-counter"; }; };
3.2. DT configuration (board level)[edit source]
This part is used to configure and enable the TIM hardware used on the board:
- Enabling DT root node for the TIM instances in use (e.g timers1...) by setting status = "okay";
- Enabling DT child node(s) for the feature(s) in use (PWM input/output, trigger and quadrature encoder) by setting status = "okay";
- Configuring pins in use via pinctrl through pinctrl-0, pinctrl-1 and pinctrl-names.
To enable PWM capture on the board (optional), DMA must be configured:
- Enable DMA channel(s) corresponding to the PWM input(s) by setting dmas = <...>, <...>; and matching dma-names = "ch1", "ch3";.
When PWM capture isn't used, it's recommended to disable DMA channels by default, to spare them for other usage:
- Disable DMA channels by setting /delete-property/dmas and /delete-property/dma-names
3.3. DT configuration examples[edit source]
3.3.1. TIM configured in PWM mode[edit source]
The example below shows how to configure TIM1 channel 1 to act as:
- PWM output on PE9, e.g. TIM1_CH1 (See pinctrl device tree configuration and GPIO internal peripheral)
- PWM device tree provider (e.g. TIM1_CH1) used by a device tree consumer (e.g. like "pwm-leds"[9]).
/* select TIM1_CH1 alternate function 1 on 'PE9' */ pwm1_pins_a: pwm1-0 { pins { pinmux = <STM32_PINMUX('E', 9, AF1)>; bias-pull-down; drive-push-pull; slew-rate = <0>; }; }; /* configure 'PE9' as analog input in low-power mode */ pwm1_sleep_pins_a: pwm1-sleep-0 { pins { pinmux = <STM32_PINMUX('E', 9, ANALOG)>; }; };
/* PWM DT provider on TIM1: "pwm1" */ &timers1 { status = "okay"; /* spare all DMA channels since they are not needed for PWM output */ /delete-property/dmas; /delete-property/dma-names; /* define pwm1 label */ pwm1: pwm { /* configure PWM pins on TIM1_CH1 */ pinctrl-0 = <&pwm1_pins_a>; pinctrl-1 = <&pwm1_sleep_pins_a>; pinctrl-names = "default", "sleep"; /* enable PWM on TIM1 */ status = "okay"; }; };
- PWM DT user example
/ { ... /* PWM DT user on TIM1_CH1: "pwm1", example with "pwm-leds"[9] */ pwmleds { compatible = "pwm-leds"; example { label = "stm32-pwm-leds-example"; /* Use pwm1 channel 0 (e.g. TIM1_CH1) */ /* period in nanoseconds (500000), normal polarity (0) */ pwms = <&pwm1 0 500000 0>; max-brightness = <127>; }; }; };
3.3.2. TIM configured in PWM mode and trigger source[edit source]
The example below shows how to configure TIM1 channel 1 to act as:
- PWM output on PE9, e.g. TIM1_CH1 (See pinctrl device tree configuration and GPIO internal peripheral)
- trigger source (synchronous with PWM) for other internal peripheral such as STM32 ADC
/* select TIM1_CH1 alternate function 1 on 'PE9' */ pwm1_pins_a: pwm1-0 { pins { pinmux = <STM32_PINMUX('E', 9, AF1)>; bias-pull-down; drive-push-pull; slew-rate = <0>; }; }; /* configure 'PE9' as analog input in low-power mode */ pwm1_sleep_pins_a: pwm1-sleep-0 { pins { pinmux = <STM32_PINMUX('E', 9, ANALOG)>; }; };
&timers1 { status = "okay"; /* spare all DMA channels since they are not needed for PWM output */ /delete-property/dmas; /delete-property/dma-names; pwm { /* configure PWM on TIM1_CH1 */ pinctrl-0 = <&pwm1_pins_a>; pinctrl-1 = <&pwm1_sleep_pins_a>; pinctrl-names = "default", "sleep"; /* enable PWM on TIM1 */ status = "okay"; }; timer@0 { /* enable trigger on TIM1 */ status = "okay"; }; };
3.3.3. TIM configured in PWM input capture mode[edit source]
The example below shows how to configure TIM1 channel 1 in PWM input capture mode (e.g. period and duty cycle):
- Configure PWM input on PE9, e.g. TIM1_CH1 (See pinctrl device tree configuration and GPIO internal peripheral)
/* select TIM1_CH1 alternate function 1 on 'PE9' */ pwm1_in_pins_a: pwm1-in-0 { pins { pinmux = <STM32_PINMUX('E', 9, AF1)>; bias-disable; }; }; /* configure 'PE9' as analog input in low-power mode */ pwm1_in_sleep_pins_a: pwm1-in-sleep-0 { pins { pinmux = <STM32_PINMUX('E', 9, ANALOG)>; }; };
A DMA channel is required and must be configured depending on the PWM input channel:
- Select DMA channel 1, "ch1", to capture PWM input channel 1 and/or 2
- Select DMA channel 3, "ch3", to capture PWM input channel 3 and/or 4
- Select both "ch1" and "ch3" dmas to enable capture on all PWM input channels
&timers1 { status = "okay"; /* Enable DMA "ch1" for PWM input on TIM1_CH1 */ dmas = <&dmamux1 11 0x400 0x5>; dma-names = "ch1"; pwm { /* configure PWM input pins, e.g. TIM1_CH1 */ pinctrl-0 = <&pwm1_in_pins_a>; pinctrl-1 = <&pwm1_in_sleep_pins_a>; pinctrl-names = "default", "sleep"; /* enable PWM on TIM1 */ status = "okay"; }; };
3.3.4. TIM configured as quadrature encoder interface[edit source]
The example below shows how to configure TIM1 to interface with a quadrature encoder:
- Configure PE9 and PE11 as encoder input pins, e.g. TIM1_CH1, TIM1_CH2 (see pinctrl device tree configuration and GPIO internal peripheral)
tim1_in_pins_a: tim1-in-pins-0 { pins { pinmux = <STM32_PINMUX('E', 9, AF1)>, /* TIM1_CH1 */ <STM32_PINMUX('E', 11, AF1)>; /* TIM1_CH2 */ bias-disable; }; }; tim1_in_pins_sleep_a: tim1-in-pins-sleep-0 { pins { pinmux = <STM32_PINMUX('E', 9, ANALOG)>, /* TIM1_CH1 */ <STM32_PINMUX('E', 11, ANALOG)>; /* TIM1_CH2 */ }; };
&timers1 { status = "okay"; /delete-property/dmas; /* spare all DMA channels since they are not required for quadrature encoder interface */ /delete-property/dma-names; counter { pinctrl-0 = <&tim1_in_pins_a>; /* configure TIM1_CH1 and TIM1_CH2 as encoder input pins */ pinctrl-1 = <&tim1_in_pins_sleep_a>; pinctrl-names = "default", "sleep"; status = "okay"; /* enable Encoder interface mode on TIM1 */ }; };
4. How to configure the DT using STM32CubeMX[edit source]
The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.
5. References[edit source]
Please refer to the following links for additional information:
- ↑ 1.0 1.1 TIM internal peripheral
- ↑ Device tree
- ↑ Documentation/devicetree/bindings/mfd/stm32-timers.txt , STM32 TIM MFD device tree bindings
- ↑ Documentation/devicetree/bindings/pwm/pwm-stm32.txt , STM32 TIM PWM device tree bindings
- ↑ Documentation/devicetree/bindings/iio/timer/stm32-timer-trigger.txt , STM32 TIM trigger device tree bindings
- ↑ Documentation/devicetree/bindings/mfd/mfd/st,stm32-timers.yaml
- ↑ Documentation/devicetree/bindings/counter/stm32-timer-cnt.txt , STM32 TIM quadrature encoder device tree bindings
- ↑ 8.0 8.1 stm32mp151.dtsi , STM32.dtsi file
- ↑ 9.0 9.1 Documentation/devicetree/bindings/leds/leds-pwm.txt , PWM LEDs device tree bindings