This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This article provides guidelines to setup environment for developing and debugging User Space application within STM32CubeIDE version 1.4 or 1.5.
1. Prerequisites[edit source]
Minimum hardware:
- STM32MP15x-based board
- Linux console
- Ethernet (or Ethernet over USB) for connection to Linux CA7
Minimum software:
- STM32CubeIDE 1.4.2 installed
- STM32MP15 project created
- Yocto SDk installed thanks to "Setup OpenSTLinux" CA7 contextual menu
2. Create User Space project[edit source]
Open new C Project wizard: File -> New -> Project... C Project. In first window choose OpenSTLinux SDK, then Next & Finish.