1. Article purpose[edit source]
The purpose of this article is to explain how to configure the WLAN when the peripheral (or peripheral associated to the framework) is assigned to Linux® OS.
The configuration is performed using the device tree mechanism that provides a hardware description of the WLAN peripheral connected on SDIO bus.
The purpose of this article is to explain Cypress WLAN/BT companion chip[1] device tree node
2. DT bindings documentation[edit source]
The WLAN[2] tree bindings are composed by :
- SDIO link configuration[3]
- WLAN device configuration[4]
3. DT configuration[edit source]
This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device tree file split.
3.1. DT configuration (STM32 level)[edit source]
The companion chip uses the SDIO link so the DT is based on the SDMMC peripheral node which is located in stm32mp151.dtsi
- This is a set of properties that may not vary for given STM32 device, such as: registers address, clock, reset.
The SDMMC DT configuration is explained at SDMMC device tree configuration
This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user. |
3.2. DT configuration (board level)[edit source]
Part of the device tree is used to describe the WLAN hardware used on a given board. The DT node ("sdmmc2") must be filled in:
- mmc-pwrseq: phandle to the MMC power sequence node
&sdmmc2 { ... arm,primecell-periphid = <0x10153180>; ... non-removable; st,neg-edge; bus-width = <4>; vmmc-supply = <&v3v3>; mmc-pwrseq = <&wifi_pwrseq>; /* phandle to the MMC power sequence node */ ... brcmf: bcrmf@1 { /* node of WLAN companion chip */ reg = <1>; compatible = "brcm,bcm4329-fmac"; } }
4. References[edit source]