CRYP device tree configuration

Revision as of 22:01, 1 November 2021 by Registered User (Update)

1. Article purpose[edit source]

The purpose of this article is to explain how to configure the CRYP[1] .

The configuration is performed using the device tree mechanism[2].

The Device tree provides a hardware description of the CRYP[1].

2. DT bindings documentation[edit source]

The CRYP [1] is represented by the STM32 CRYP device tree bindings[3].

3. DT configuration[edit source]

This hardware description is a combination of STM32 microprocessor and board device tree files. See Device tree for explanations on device tree file split.

The STM32CubeMX can be used to generate the board device tree. Refer to #How_to_configure_the_DT_using_STM32CubeMX for more details.

3.1. DT configuration (STM32 level)[edit source]

The CRYP[1] node is located in the SoC device tree file.

3.2. DT configuration (board level)[edit source]

Board level device tree is used to enable the CRYP[1].

4. How to configure the DT using STM32CubeMX[edit source]

The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.

5. References[edit source]

Please refer to the following links for additional information: