How to configure flash memory for TF-A BL2

Revision as of 12:12, 22 April 2020 by Registered User (Example table updated)

1. Article purpose[edit source]

This article explains how to configure the TF-A MTD frameworks:

  • SPI NOR
  • SPI NAND
  • SPI MEM
  • FMC NAND

These frameworks represents the memory access organisation.

These frameworks use two different configurations:

If the peripheral is assigned to another execution context, refer to How to assign an internal peripheral to a runtime context article for guidelines on peripheral assignment and configuration.

2. Framework overview[edit source]

BL2 MTD v2.0.0.png

2.1. Components description[edit source]

  • IO_Storage

The IO storage provides an abstraction layer to access storage devices.

  • Boot device configuration

The Boot device configuration is a platform specific ad-dons to manage Flash memory settings.

  • MTD core

The MTD core provides an abstraction layer for raw Flash memories.

  • Raw NAND subsystem

The Raw NAND protocol is used in the MTD subsystem for interfacing NAND Flash memories.

  • SPI-MEM subsystem

The SPI-MEM protocol is used in the MTD subsystem for interfacing all kinds of SPI memories (NORs, NANDs)

  • SPI-NAND subsystem

The SPI-NAND protocol is used in the MTD subsystem for interfacing SPI NAND Flash memories.

  • SPI-NOR subsystem

The SPI-NOR protocol is used in the MTD subsystem for interfacing SPI NOR Flash memories.

  • FMC driver / FMC (Hardware)

Please refer to the FMC internal peripheral.

  • QUADSPI driver / QUADSPI (Hardware)

Please refer to the QUADSPI internal peripheral.

3. DT configuration[edit source]

This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device tree file split.

Pinctrl device tree configuration (and optionally to Pinctrl overview) must be added in #DT configuration (board level).

STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.

4. Raw NAND flash memory[edit source]

4.1. Raw NAND DT configuration[edit source]

For the DT bindings, refers to FMC_device_tree_configuration.

For the DT configuration (STM32 level), refers to FMC DT Configuration at STM32 level.

For the DT configuration (board level), refers to FMC DT Configuration at board level.

Warning white.png Warning
Only the required device used to load images must be declared as a child node

4.2. Raw NAND device configuration[edit source]

Raw NAND access will use th raw NAND framework. Some additional parameters are required by the raw NAND framework to address the memory:

  • Page size
  • Block size
  • Blocks number in device
  • NAND width (8 or 16 bits)
  • ECC : Supported algorithm (BCH8/BCH4/Hamming are available). The default ECC framework configuration is no error correction.

Some memories are ONFI[1] compliant. In that case, required parameters can be directly read from the parameter description table.

For the others, user must properly fill out OTP configuration.

4.2.1. Raw NAND examples[edit source]

  • Raw Nand ONFI with ECC override (Default from parameter table is BCH4, force to BCH8).
OTP Word 9 : 0x18000
Use OTP Page size Block size Block numbers (N * 256) Width ECC
0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 1 1 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0


  • 8bit NAND with 4KB paged / 256KB erase size / 1024MB size, ECC BCH4
OTP Word 9 : 0xA0808000
Use OTP Page size Block size Block numbers (N * 256) Width ECC
1 0 1 0 0 0 0 0 1 0 0 0 0 0 0 0 1 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0


  • 16bit NAND with 2KB paged / 512KB erase size / 2048MB size, with On die ECC
OTP Word 9 : 0x91060000
Use OTP Page size Block size Block numbers (N * 256) Width ECC
1 0 0 1 0 0 0 1 0 0 0 0 0 1 1 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0


5. SPI NAND flash memory[edit source]

5.1. SPI NAND DT configuration[edit source]

For the DT bindings, refers to the QUADSPI_device_tree_configuration.

For the DT configuration (STM32 level), refers to QUADSPI DT Configuration at STM32 level.

For the DT configuration (board level), refers to QUADSPI DT Configuration at board level.

Warning white.png Warning
Only the required device used to load images must be declared as a child node

5.2. SPI NAND device configuration[edit source]

SPI NAND and SPI MEM frameworks are used to address such memories.

5.2.1. SPI NAND framework[edit source]

SPI NAND framework requires additional parameters:

  • Page size
  • Block size
  • Blocks number in device
  • Plane number

These parameters must be properly filled out by user in OTP configuration.

5.2.2. SPI MEM framework[edit source]

SPI MEM framework is used to send commands. By default, the generic read command used is the legacy command:
0x03 with 1 line command, 1 line address, 1 data bus width (1_1_1). It is possible to override this read command to improve performance access to the memory using platform configuration.

5.2.3. SPI NAND example[edit source]

  • SPI NAND with 2KB paged / 256KB erase size / 1024MB size, 2 Planes
OTP Word 9 : 0x88804000
Use OTP Page size Block size Block numbers (N * 256) Not Used Not Used 2 Planes
1 0 0 0 1 0 0 0 1 0 0 0 0 0 0 0 0 1 0 0 0 0 0 0 0 0 0 0 0 0 0 0


  • Update read command to use command 0x6B (1_1_4) defined in platform file[2]
device->spi_read_cache_op.cmd.opcode = SPI_NAND_OP_READ_FROM_CACHE_4X;
device->spi_read_cache_op.cmd.buswidth = SPI_MEM_BUSWIDTH_1_LINE;
device->spi_read_cache_op.addr.nbytes = 2U;
device->spi_read_cache_op.addr.buswidth = SPI_MEM_BUSWIDTH_1_LINE;
device->spi_read_cache_op.dummy.nbytes = 1U;
device->spi_read_cache_op.dummy.buswidth = SPI_MEM_BUSWIDTH_1_LINE;
device->spi_read_cache_op.data.buswidth = SPI_MEM_BUSWIDTH_4_LINE;
device->spi_read_cache_op.data.dir = SPI_MEM_DATA_IN;

6. SPI NOR flash memory[edit source]

6.1. SPI NOR DT configuration[edit source]

For the DT bindings, refers to the QUADSPI_device_tree_configuration.

For the DT configuration (STM32 level), refers to QUADSPI DT Configuration at STM32 level.

For the DT configuration (board level), refers to QUADSPI DT Configuration at board level.

Warning white.png Warning
Only the required device used to load images must be declared as a child node

6.2. SPI NOR device configuration[edit source]

SPI NOR and SPI MEM frameworks are used to address such memories.

6.2.1. SPI NOR framework[edit source]

SPI NOR framework requires additional parameters:

  • Device size

These parameters need to be defined in the platform configuration file<ref_name="boot_device">.

6.2.2. SPI MEM framework[edit source]

SPI MEM framework is used to send commands. By default, the generic read command used is the legacy command:
0x03 with 1 line command, 1 line address, 1 data bus width (1_1_1). It is possible to override this read command to improve performance access to the memory using platform configuration.

6.2.3. SPI NOR example[edit source]

  • SPI NOR 64MB size
	device->size = SZ_64M;                                --> Device size
  • Update read command to use command 0x6B (1_1_4) define in platform file[2]
	device->read_op.cmd.opcode = SPI_NOR_OP_READ_1_1_4;
	device->read_op.cmd.buswidth = SPI_MEM_BUSWIDTH_1_LINE;
	device->read_op.addr.nbytes = 3U;
	device->read_op.addr.buswidth = SPI_MEM_BUSWIDTH_1_LINE;
	device->read_op.dummy.nbytes = 1U;
	device->read_op.dummy.buswidth = SPI_MEM_BUSWIDTH_1_LINE;
	device->read_op.data.buswidth = SPI_MEM_BUSWIDTH_4_LINE;
	device->read_op.data.dir = SPI_MEM_DATA_IN;

7. How to configure the DT using STM32CubeMX[edit source]

The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.

8. References[edit source]

Please refer to the following links for additional information: