This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Purpose[edit source]
This article proposes some guidelines in order to determine the best low power strategy for your STM32MP15 product.
2. STM32MP15 main power supplies and low power modes[edit source]
For a good understanding of this article, it is important to understand the perimeter of the two STM32MP15 main power supplies:
- VDD supplies I/Os and system analog such as reset, power management, oscillators and PLLs. VDD is present as far as the STM32MP15 is not in OFF or VBAT mode. For a given system, its voltage is fixed and chosen in the range from 1.8 V to 3.3 V supported by the STM32MP1 Series.
- VDDcore supplies the digital core domain and must be present after VDD on start up. Its voltage varies depending on the system state:
- 1.2 V typical in Run and (LP-)Stop modes
- 0.9 V typical in LPLV-Stop mode
- OFF in Standby mode
For more information, please refer to the PWR chapter of the STM32MP15 Reference Manual.
3. STM32MP15 low power modes overview[edit source]
When the system does not need to run for a while, various actions can be taken to reduce its power consumption:
- Stop the clocks: this corresponds to the Stop mode and the external regulator can even be allowed to switch in low power mode in order to reduce its power consumption: this is the LP-Stop mode.
- Reduce the supply voltage
4. STM32MP15 low power modes overview[edit source]
For each supported low power mode (described in the AN5109), the figure below shows:
- The peripherals that can be used as wake up sources (in grey boxes)
- The STM32MP15 typical power consumption (on the left)
- The system wake up times in various configurations (on the right)
![STM32MP15 low power modes](/stm32mpu-ecosystem-v4/nsfr_img_auth.php/c/ce/STM32MP15_low_power_modes.png)