Revision as of 10:51, 20 November 2019 by Registered User
This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or
pending task to finish installation of
Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.
This category groups together all articles and subcategories related to the hardware components used on the STM32 MPU boards, and for which additional software information is needed.
An internal peripheral (a.k.a. hardware block ) is embedded inside a STM32 MPU microprocessor device, whereas a hardware component is outside the microprocessor, but delivered with an STM32 MPU board. It is either soldered on a STM32 MPU board (e.g. the Cirrus cs42l51 audio codec for the STM32MP157x_DKx Discovery kits), or plugged into a STM32MPU board via a hardware port (such as the OmniVision OV5640 camera sensor for the STM32MP157C-EV1 Evaluation board).
A hardware component is natively managed by the STM32MPU Embedded Software distributions.
|
|
This category groups together all articles and subcategories related to the hardware components used on the STM32 MPU boards, and for which additional software information is needed.
It is either soldered on a STM32 MPU board (e.g. the Cirrus cs42l51 audio codec for the STM32MP157x_DKx Discovery kits), or plugged into a STM32MPU board via a hardware port (such as the OmniVision OV5640 camera sensor for the STM32MP157C-EV1 Evaluation board).
A hardware component is natively managed by the STM32MPU Embedded Software distributions.
|
Be careful not to confuse a hardware component with ainternal peripheral (a.k.a. hardware block ) which is embedded inside a STM32 MPU microprocessor device.
|
Subcategories
This category has the following 6 subcategories, out of 6 total.