RETRAM internal memory

Revision as of 16:51, 15 February 2019 by Registered User


Template:ArticleMainWriter Template:ArticleApprovedVersion


1. Peripheral overview[edit source]

The RETRAM internal memory is 64 Kbytes wide and is physically near to the Arm® Cortex®-M4 for optimized performance from the core. It is located in the VSW power domain, allowing it to be supplied during Standby low power mode, and to retain retention firmware that can be executed very quickly by the Cortex-M4 on wake up from Standby mode.

1.1. Features[edit source]

Refer to STM32MP15 reference manuals for the complete feature list, and to the software components introduced below to see which features are actually implemented.

1.2. Security support[edit source]

The RETRAM is a secure peripheral (under ETZPC control).

2. Peripheral usage and associated software[edit source]

2.1. Boot time[edit source]

Linux® remoteproc framework (running on the Cortex-A7) loads the Cortex-M4 firmware to the RETRAM, starting at address 0x00000000. At least, it must load the part of the firmware containing the vector table, since the Cortex-M4 reset entry point is address 0x00000004. The rest of the firmware code is loaded into the MCU SRAM. The overall memory mapping is shown in the platform memory mapping section.

2.2. Runtime[edit source]

2.2.1. Overview[edit source]

The Cortex-M4 vector table is mapped from address 0x00000000 (so to the RETRAM) at reset, but it can be remapped by software to any other location by means of the vector table offset register (VTOR). Beyond the reset entry point (0x00000004), the exception table also contains the software entries table used by the NVIC to branch the software execution to the right interrupt service routine.

While going to Standby low power mode, the RETRAM can remain supplied, so it can preserve a (small) Cortex-M4 piece of retention firmware that is executed on wake up when the ROM code (running on Cortex-A7) restarts the Cortex-M4.
All these constraints make the RETRAM the minimum (and default) choice for Cortex-M4 firmware.

RETRAM can be allocated to:

  • the Cortex-A7 secure to be used under OP-TEE.

or

or

  • the Cortex-M4 for use with the STM32Cube MPU Package, either for runtime firmware that ca be mapped in both RETRAM and MCU SRAM, or for retention firmware that only fits into the RETRAM, but could have some data in MCU SRAM (keeping in mind that these data are lost while entering Standby low power mode).

2.2.2. Software frameworks[edit source]

Internal peripherals software table template

| Core/RAM
| RETRAM
| OP-TEE overview
| Linux reserved memory
| STM32Cube
|
|-
|}

2.2.3. Peripheral configuration[edit source]

The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the STM32CubeMX tool for all internal peripherals, and then manually completed (especially for external peripherals), according to the information given in the corresponding software framework article.

2.2.4. Peripheral assignment[edit source]

Internal peripherals assignment table template

| rowspan="1" | Core/RAM
| rowspan="1" | RETRAM
| RETRAM
| 
| 
| 
| Assignment (single choice)
|-
|}