Registered User mNo edit summary |
Registered User mNo edit summary |
||
Line 35: | Line 35: | ||
| [[GPU internal peripheral | GPU]] | | [[GPU internal peripheral | GPU]] | ||
| | | | ||
| OpenGL®ES framework | |||
| | | | ||
| | | |
Latest revision as of 18:20, 12 June 2023
1. Article purpose[edit source]
The purpose of this article is to:
- briefly introduce the GPU peripheral and its main features
- indicate the level of security supported by this hardware block
- explain how each instance can be allocated to the runtime contexts and linked to the corresponding software components
- explain, when necessary, how to configure the GPU peripheral.
2. Peripheral overview[edit source]
The GPU peripheral is a dedicated graphics processing unit. It accelerates numerous 3D graphics applications such as graphical user interface (GUI), menu display or animations. It works together with an optimized software stack designed for industry-standard APIs and supporting AndroidTM and Linux® embedded development platforms.
2.1. Features[edit source]
Refer to the STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to see which features are implemented.
2.2. Security support[edit source]
The GPU is a non-secure peripheral.
3. Peripheral usage and associated software[edit source]
3.1. Boot time[edit source]
The GPU is not used at boot time.
3.2. Runtime[edit source]
3.2.1. Overview[edit source]
The GPU internal peripheral is allocated to the Arm® Cortex®-A7 non-secure core running the Linux® userland.
Chapter Peripheral assignment describes which peripheral instance can be assigned to which context.
3.2.2. Software frameworks[edit source]
Domain | Peripheral | Software components | Comment | ||
---|---|---|---|---|---|
OP-TEE | Linux | STM32Cube | |||
Visual | GPU | OpenGL®ES framework |
3.2.3. Peripheral configuration[edit source]
The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the STM32CubeMX tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article, and in the GPU device tree configuration article for Linux®.
3.2.4. Peripheral assignment[edit source]
Click on the right to expand the legend...
Domain | Peripheral | Runtime allocation | Comment | |||
---|---|---|---|---|---|---|
Instance | Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) |
Cortex-M4 (STM32Cube) | |||
Visual | GPU | GPU | ☐ |
4. How to go further[edit source]
Please go through the articles belonging to the GPU category.
5. References[edit source]