This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User mNo edit summary |
Registered User m (Addition of GC2145 information) |
||
Line 14: | Line 14: | ||
{{:STM32MP15_internal_peripherals_software_table_template}} | {{:STM32MP15_internal_peripherals_software_table_template}} | ||
| Visual | | Visual | ||
| [[#OmniVision_OV5640 | OmniVision OV5640]] | | [[#OmniVision_OV5640 | OmniVision OV5640]] [[#GalaxyCore_GC2145 | GalaxyCore GC2145]] | ||
| | | | ||
| [[V4L2 camera overview | V4L2 camera framework]] | | [[V4L2 camera overview | V4L2 camera framework]] | ||
| | | | ||
| Camera | | Camera sensors | ||
|} | |} | ||
Line 30: | Line 30: | ||
Sources: {{CodeSource | Linux kernel | drivers/media/i2c/ov5640.c}} | Sources: {{CodeSource | Linux kernel | drivers/media/i2c/ov5640.c}} | ||
== GalaxyCore GC2145 == | |||
The GalaxyCore GC2145 camera sensor supports both parallel and MIPI<sup>®</sup> CSI-2 interfaces. | |||
For details and the datasheet please contact GalaxyCore. | |||
===Linux driver=== | |||
Sources: {{CodeSource | Linux kernel | drivers/media/i2c/gc2145.c}} | |||
<noinclude> | <noinclude> |
Latest revision as of 09:49, 12 April 2023
1. Article purpose[edit source]
The purpose of this article is to:
- List the camera sensors hardware components that might be integrated in the different boards.
- Link these components to the corresponding software framework(s).
- Point to the appropriate component datasheets.
- Explain, when necessary, how to configure these components.
2. Software frameworks[edit source]
Domain | Peripheral | Software components | Comment | ||
---|---|---|---|---|---|
OP-TEE | Linux | STM32Cube | |||
Visual | OmniVision OV5640 GalaxyCore GC2145 | V4L2 camera framework | Camera sensors |
3. OmniVision OV5640[edit source]
The OmniVision OV5640 camera sensor supports both parallel and MIPI® CSI-2 interfaces.
For details and the datasheet please contact the OV5640 provider.
3.1. Linux driver[edit source]
Bindings: Documentation/devicetree/bindings/media/i2c/ov5640.txt
Sources: drivers/media/i2c/ov5640.c
4. GalaxyCore GC2145[edit source]
The GalaxyCore GC2145 camera sensor supports both parallel and MIPI® CSI-2 interfaces.
For details and the datasheet please contact GalaxyCore.
4.1. Linux driver[edit source]
Sources: drivers/media/i2c/gc2145.c